A hydrostatic pressure test is used as a proof of strength and leak tightness of containers and pipelines that hold liquids and gases. The procedure and documentation of such a test can be increased in efficiency by …
Read moreValve actuators: Pressure switch combines control and alarm function
Jing Lyu | ApplicationsHydraulic valve actuators require pressure switches for safe operation. In control cabinets, usually two of these measuring instruments are installed. One switch is used to control the pump for the hydraulic pressure, …
Read moreWIKA has inaugurated a new factory in Kazakhstan
Stefan Schneider | WIKA insightWIKA has put into operation a new factory in Kazakhstan. The factory is located in Atyrau at the Caspian Sea. It took the team responsible for the location only six months from the planning to the start of production …
Read moreIgnition protection type Ex i for pressure measuring instruments with battery operation
Jing Lyu | PressureWhich ignition protection type is suitable for battery-operated pressure measuring instruments, which are increasingly being used in combination with a radio unit? WIKA has clearly answered this question for its …
Read moreLevel limit switches: innovation meets all-rounder
Andreas Krüger | Know-howIn the world of industrial process measurement, precise level measurements are of vital importance. Level limit switches play a crucial role here to ensure that liquids in a tank are optimally controlled and monitored. …
Read morePressure transducer: Digitally connected with EtherCAT®
Fabian Mayer | PressurePressure transducers with EtherCAT ® as the communication protocol continue the digitalisation of the semiconductor industry at the transmitter level. In future, in every production plant, dozens of pressure measuring …
Read moreWIKA initiatives for global sustainability
Stefan Schneider | WIKA insightAs a globally active company, WIKA strives for sustainability worldwide. All locations contribute to this at different levels. Environmental protection, climate protection, the support for people within as well as …
Read moreInterface measurement with two floats
Andreas Krüger | Know-howOne speaks of an interface measurement when two different liquids in a tank or container are measured independently of one another. Such an interface measurement is always useful when the liquids are not miscible with …
Read more