Bimetal or gas-actuated – the question of the suitable dial thermometer for the respective process can only be answered in a case without comparison: Only gas-actuated thermometers can be combined with a capillary. In In the reaction to a temperature …
All posts by Christoph Strebel
Selection criteria for dial thermometers (2): process temperature
Christoph Strebel | Know-howWhich dial thermometer is suitable for which process? Whether a bimetal or a gas-actuated thermometer is used depends on several factors - for example, on the process temperature. Bimetal thermometers are generally designed for scale ranges of -70 °C to +600 …
Selection criteria for mechanical Thermometers (1): Response time
Christoph Strebel | Know-howSelecting suitable mechanical thermometers for a process is not a quick task. Bimetal thermometers or gas-actuated thermometers - the decision on the type of thermometer alone depends on several factors. One of the most important selection criteria is the response time …