Submersible pressure transmitters as well known as level probes are intended to be used in immersion applications, thus they are immersed completely into the medium and, therefore, must withstand the properties of the media at all times. Both in water and …
Hydrostatic level measurement
The design of a submersible pressure transmitter / level probe – Part 2
Enrico Bossart | Know-howIn my last article, the design of a submersible pressure transmitter / level probe - Part 1, I was explaining the design of a submersible pressure transmitter, beginning with the measuring cell and its electronics. Specifically with respect to the media resistance …
The design of a submersible pressure transmitter / level probe – Part 1
Enrico Bossart | LevelA submersible pressure transmitter or level probe is a hydrostatic pressure sensor, specifically developed for the purpose of level measurement. Submersible pressure transmitters, such as the WIKA model LH-20 , are level sensors with special characteristics and …
Hydrostatic level measurement in closed geometries – calculation of the filling height
Enrico Bossart | LevelIn a previous blog post, I explained the calculation of the filling height in open geometries and vessels . Unlike open vessels, the calculation of level in closed geometries, such as gas-tight tanks or pressurised vessels, requires a compensation of the pressure of …
Hydrostatic level measurement in open geometries and vessels – calculation of the filling height
Enrico Bossart | LevelIn my last blog post, I introduced the way in which hydrostatic level measurement works . The hydrostatic pressure is used to determine the level through the measurement of the liquid column and is directly proportional to the filling height, as well as to the density …