Millions of cubic metres of liquids or gases flow through the pipes of industrial processes every day. In order to be able to transport, control and monitor these correctly, the flow rate must be calculated beforehand. The flow rate, also called volume flow, is a …
Applications
Pressure monitoring for mobile tanks in pharmaceutical processes
Jing Lyu | ApplicationsPressure monitoring in mobile tanks is an important measuring task in the pharmaceutical industry. Among other things, it enables users to check whether the containers are leak-tight during transport. In the case of active ingredients, this is an absolute necessity. …
Safe pressure measurement in chlorine production
Jing Lyu | ApplicationsPressure measurement plays a central role in chlorine production, which is a safety-critical process. This is due to the fact that chlorine is highly reactive and can therefore easily trigger explosions in combination with organic substances. So it is important to …
Pressure switch for safe operation of food silos
Jing Lyu | ApplicationsPressure switches in food silos make a significant contribution to detecting overpressure in good time and safely preventing it. A manufacturer of such elevated vessels uses the model MA mechanical pressure switch for this task. One special property tipped the scales …
Level monitoring in milk tanks using a process transmitter
Jing Lyu | ApplicationsLevel monitoring using a process transmitter with a flush diaphragm is an option for applications in the food industry. It is highly accurate and at the same time suitable for aseptic tanks. A manufacturer of dairy products (milk, cream and yoghurt), for example, uses …