The invention of the pump itself was a major breakthrough for mankind. It significantly simplified the supply of drinking water. With growing demands for a stable water supply, largely free from pressure fluctuations, and at the same time increasing demands on the …
Applications
SIL pressure switch: Safety in tyre manufacturing
Jing Lyu | ApplicationsNumerous industrial processes have an inherently high risk potential. Special pressure switches support the safety of people and the environment. Example: the vulcanisation of tyres for motor vehicles. To monitor this process, leading manufacturers use the model MW …
Safe filter monitoring with differential pressure gauges
Jing Lyu | ApplicationsFilter monitoring is a core task of differential pressure gauges - the differential pressure increases as soon as the filter becomes clogged. The measuring instruments thus signal when the filter needs to be cleaned or replaced. The efficiency of such a solution can be …
Natural gas: On-site calibration optimised at the metering skid
Jing Lyu | ApplicationsOn-site calibration of measuring instruments is often very time-consuming and expensive. This is especially true for applications with several measurands. One example of this is the metering skid, a system for the custody transfer measurement of the amount of natural …
Measurement technology in compressors
Roland Sachs | ApplicationsThe measurement technology used in compressors is tending to increase more and more. And for good reason. The balancing act between increased compressed air demands and reduced energy consumption also depends, to a large extent, on the intelligent use of measuring …