The high requirements placed on pesticides and their production are also reflected in the pressure measurement in the process. A WIKA customer has therefore supplemented the electronic instrumentation for pressure monitoring with a mechanical backup. For this …
All posts by Jing Lyu
Pressure switch in hydrogen-powered train ensures safety
Jing Lyu | ApplicationsIn a newly developed hydrogen train for local transport, a pressure switch from WIKA plays a crucial role. Within the scope of pressure monitoring, it performs the central safety function in the H2 supply system during the journey. The benefits of hydrogen in rail …
Plastics production: Safe pressure measurement up to 330 °C
Jing Lyu | ApplicationsPressure measurement in the production of PBAT, a biodegradable plastic, faces a special challenge: Temperatures of up to 330 °C prevail in the process. For a PBAT producer, therefore, WIKA has designed a model IPT-20 process transmitter with a flush diaphragm seal …
Lasting accuracy for diaphragm seal systems for vacuum process
Jing Lyu | ApplicationsA diaphragm seal system in a vacuum process must master a major challenge – it must deliver a reliable measuring result, even when the pressure drops and the temperature rises at the same time. The example of a chemical company producing phthalic anhydride (PA) shows …
Pressure monitoring in the pharmaceutical industry with a universal instrument
Jing Lyu | ApplicationsPressure monitoring in the pharmaceutical industry is a demanding task with a wide variety of requirements. However, a corresponding diversification in instrumentation does not have to be an inevitable consequence. This is demonstrated by the use of a universal process …