In practice, RoHS-compliant is often equated with "lead-free". However, this is a widespread mistake. The RoHS directive 2002/95/EC aims to minimize the use of hazardous substances (including, among others, lead), but it does not completely exclude a small percentage. …
All posts by Sabine Mai
Level measurement in ground water
Sabine Mai | LevelThe recovery of drinking water from ground water has top priority in many countries. In Germany, this method has a share of about 70 per cent in the water supply. The water drawn from depths of several hundred of meters below the earth’s surface is normally in …
What are front flush diaphragm pressure connections used for?
Sabine Mai | GeneralFront flush diaphragm pressure connections are required whenever the pressure channel of a standard pressure sensor may become clogged or damaged in use. This problem is encountered, for example, with crystalline, viscous, aggressive, adhering or abrasive media. …
What exactly is a level probe / submersible pressure transmitter?
Sabine Mai | LevelThe submersible pressure transmitter, sometimes also referred to as a level probe, is a special type of pressure sensor used for level measurements in e.g. tanks, wells, shafts and bore holes. For level measurements, the level probe is submersed directly into the …
Pressure sensor principles – a comparison
Sabine Mai | PressureThere is no “ideal” sensor principle. Of particularly great importance and widespread use are resistive sensor technologies, due to their reliability. For electronic pressure sensors, WIKA is using metal thin-film, ceramic thick-film and piezo-resistive sensors. …