{"id":50644,"date":"2023-04-27T06:34:09","date_gmt":"2023-04-27T04:34:09","guid":{"rendered":"https:\/\/blog.wika.com\/en\/?p=50644"},"modified":"2025-05-19T11:41:19","modified_gmt":"2025-05-19T09:41:19","slug":"pressure-monitoring-in-uht-plant-without-risk-of-contamination","status":"publish","type":"post","link":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/","title":{"rendered":"Pressure monitoring in UHT plant without risk of contamination"},"content":{"rendered":"<p><strong>Companies in the food industry use electronic pressure transmitters to monitor the pressure in a UHT plant. In order to optimise its process reliability, a manufacturer of dairy products has now upgraded its system to utilise the WIKA DMSU21SA pressure transmitter with integrated diaphragm monitoring. The previously installed measuring assembly leaked due to damage to the diaphragm, leading to consequent contamination of the product.<\/strong><\/p>\n<p>\u201cUltra-high-temperature\u201d (UHT) processes are used to destroy unwanted microorganisms and at the same time to preserve the physico-chemical properties of the respective product \u2013 here milk \u2013 in order to increase the shelf life of the food. The UHT plant mentioned works with indirect heating via a heat exchanger. In this way, a large part of the thermal energy can be recovered and the process can be operated cost-effectively.<\/p>\n<h2>Pressure monitoring in UHT plant using flush-mounted pressure transmitter<\/h2>\n<p>Temperature, flow and pressure instrumentation is required to control heat transfer. In view of temperatures up to +135 \u00b0C and other challenging conditions, such as aggressive cleaning agents, flush pressure transmitters are used for pressure monitoring in UHT plant. Their diaphragms withstand normal process conditions over a long period of time without restriction.<\/p>\n<p>However, continuous stress, caused, for example, by 24-hour operation in the production of dairy products, temperature changes, cleaning processes and subsequent steaming, can wear and damage even such a solid diaphragm, for example as a result of violent pressure surges (\u201cwater hammer effect\u201d). The crack or perforation can allow pressure transmission fluid to seep into the process. Conversely, product gets behind the diaphragm, remains there and forms a new source of germs.<\/p>\n<h2>Significant losses after contamination of the product<\/h2>\n<p>The damage initially remains undetected because the sensor continues to function and measure. The contamination it has caused can have serious consequences. Because the product is no longer pure, the affected batch must often be destroyed once the damage has been detected. The processing of milk usually involves large quantities, 20,000 litres and more. Such an incident also causes a production downtime of several hours, plus the effort for cleaning and sterilisation and then the disposal of the contaminated product.<\/p>\n<h2>The DMSU21SA provides protection against contamination and immediate notification of any damage<\/h2>\n\n      <div class=\"wp-caption alignright\" style=\"max-width:396px;\"><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/en\/wp-content\/blogs.dir\/18\/files\/2023\/04\/textbild_dms21sa.jpg\" alt=\"Digitalised safety with pressure monitoring in a UHT plant.\" \/><p class=\"wp-caption-text\">The DMSU21SA process transmitter with integrated diaphragm monitoring is EHEDG-approved (EL Class I) and 3-A marked and can be supplied with all common sterile connections.<\/p><\/div>\n    \n<p>With the manufacturer mentioned above, the leak occurred at a measuring location directly at the heat exchanger. The company did not hesitate and exchanged all instruments in the process for WIKA DMSU21SA pressure transmitters with integrated diaphragm monitoring. The measuring system works with a welded double diaphragm, the space between which is evacuated.<\/p>\n<p>If the diaphragm on the process side is damaged, the vacuum is released and the monitoring instrument (pressure switch) emits an alarm signal. The manufacturer is informed about the incident at the same time and can initiate countermeasures immediately. The second diaphragm keeps the process securely sealed until the damage has been repaired.<\/p>\n<p>The instrument replacement is also made without much effort. This is because the DMSU21SA can be commissioned without any problems, based on the plug-and-play principle. The measuring system communicates via the HART<sup>\u00ae<\/sup> protocol and can therefore also be integrated into digitalised structures.<\/p>\n<p><strong>Note<\/strong><br \/>\nFurther details on the DMSU21SA can be found in our blog post \u201c<a href=\"https:\/\/blog.wika.com\/en\/products\/pressure-products\/diaphragm-seal-system-with-diaphragm-monitoring-also-digital\/\">Diaphragm seal system with diaphragm monitoring \u2013 also digital<\/a>\u201d and on the <a href=\"https:\/\/www.wika.com\/en-en\/dmsu21sa.WIKA\" rel=\"external\" target=\"_blank\">WIKA website<\/a>. There you will also find information on other <a href=\"https:\/\/www.wika.com\/en-en\/food_and_beverages.WIKA\" rel=\"external\" target=\"_blank\">measurement solutions for the food industry<\/a>. If you have any questions, your <a href=\"https:\/\/www.wika.com\/en-en\/contact.WIKA\" rel=\"external\" target=\"_blank\">contact<\/a> will gladly help you.<\/p>\n<p><strong>Also read our posts<\/strong><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/applications\/lasting-accuracy-for-diaphragm-seal-systems-for-vacuum-process\/\">Lasting accuracy for diaphragm seal systems for vacuum process<\/a><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/knowhow\/diaphragm-seal-systems-with-tri-clamp-connection-are-novaseptic-compatible\/\">Diaphragm seal systems with TRI-CLAMP\u00ae connection are NovAseptic\u00ae-compatible<\/a><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/products\/hygienic-pressure-gauge-ip68-with-cleaning-from-the-outside\/\">Hygienic pressure gauge: IP68 when cleaning from the outside<\/a><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/products\/temperature-products\/hygienic-m12-coupler-connector-for-thermometer-connection-head\/\">Hygienic M12 coupler connector for thermometer connection head<\/a><\/p>\n\n      <div class=\"wp-caption alignright\" style=\"max-width:396px;\"><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/en\/files\/2023\/07\/buyersguide_en-co-388x218.jpg\" alt=\"Women worker in drinking water plant clean hygiene uniform monitor control pressure gauge water purity process.\" \/><p class=\"wp-caption-text\">Pressure measurement technology for the food and beverage industry<\/p><\/div>\n    \n<p><strong>Your free buyer\u2019s guide<br \/>\n<\/strong><span>Precision in the food and beverage industry: Our guide provides practical information on what to look for when selecting pressure measurement solutions. Download your free\u00a0<\/span><a href=\"https:\/\/www.wika.com\/en-en\/buyers_guide_pressure_measurement_technology_for_the_food_and_beverage_industry.WIKA\" target=\"_blank\" rel=\"noopener external\">buyer\u2019s guide \u201cPressure measurement technology for the food and beverage industry\u201d<\/a><span>\u00a0now.<\/span><\/p>\n<p>&nbsp;<\/p>\n","protected":false},"excerpt":{"rendered":"<p>Companies in the food industry use electronic pressure transmitters to monitor the pressure in a UHT plant. In order to optimise its process reliability, a manufacturer of dairy products has now upgraded its system to utilise the WIKA DMSU21SA pressure transmitter with integrated diaphragm monitoring. The previously installed measuring assembly leaked due to damage to [&hellip;]<\/p>\n","protected":false},"author":134,"featured_media":50677,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"_acf_changed":false,"footnotes":""},"categories":[232],"tags":[273,737,284,274,575,726,721],"class_list":["post-50644","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-applications","tag-cleaning","tag-foodbeverages","tag-measuring-point","tag-operating-conditions","tag-pressure-measurement-device","tag-pressure-transmitters","tag-process-safety"],"acf":[],"yoast_head":"<!-- This site is optimized with the Yoast SEO plugin v27.6 - https:\/\/yoast.com\/product\/yoast-seo-wordpress\/ -->\n<title>Pressure monitoring in UHT plant without risk of contamination - WIKA blog<\/title>\n<meta name=\"description\" content=\"A manufacturer switched to WIKA pressure transmitters with diaphragm monitoring for process-reliable pressure monitoring in its UHT system.\" \/>\n<meta name=\"robots\" content=\"index, follow, max-snippet:-1, max-image-preview:large, max-video-preview:-1\" \/>\n<link rel=\"canonical\" href=\"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/\" \/>\n<meta property=\"og:locale\" content=\"en_GB\" \/>\n<meta property=\"og:type\" content=\"article\" \/>\n<meta property=\"og:title\" content=\"Pressure monitoring in UHT plant without risk of contamination - WIKA blog\" \/>\n<meta property=\"og:description\" content=\"A manufacturer switched to WIKA pressure transmitters with diaphragm monitoring for process-reliable pressure monitoring in its UHT system.\" \/>\n<meta property=\"og:url\" content=\"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/\" \/>\n<meta property=\"og:site_name\" content=\"WIKA blog\" \/>\n<meta property=\"og:image\" content=\"https:\/\/blog.wika.com\/en\/files\/2023\/05\/beitragsbild_uht-anlage-838x471-2.jpg\" \/>\n\t<meta property=\"og:image:width\" content=\"838\" \/>\n\t<meta property=\"og:image:height\" content=\"471\" \/>\n\t<meta property=\"og:image:type\" content=\"image\/jpeg\" \/>\n<meta name=\"author\" content=\"Jing Lyu\" \/>\n<meta name=\"twitter:label1\" content=\"Written by\" \/>\n\t<meta name=\"twitter:data1\" content=\"Jing Lyu\" \/>\n\t<meta name=\"twitter:label2\" content=\"Estimated reading time\" \/>\n\t<meta name=\"twitter:data2\" content=\"4 minutes\" \/>\n<script type=\"application\/ld+json\" class=\"yoast-schema-graph\">{\"@context\":\"https:\\\/\\\/schema.org\",\"@graph\":[{\"@type\":\"Article\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\\\/#article\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\\\/\"},\"author\":{\"name\":\"Jing Lyu\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/8710ec58b46c9dcd86997cf055ce6411\"},\"headline\":\"Pressure monitoring in UHT plant without risk of contamination\",\"datePublished\":\"2023-04-27T04:34:09+00:00\",\"dateModified\":\"2025-05-19T09:41:19+00:00\",\"mainEntityOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\\\/\"},\"wordCount\":707,\"commentCount\":0,\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2023\\\/05\\\/beitragsbild_uht-anlage-838x471-2.jpg\",\"keywords\":[\"Cleaning\",\"Food\\\/Beverages\",\"Measuring point\",\"Operating conditions\",\"Pressure measurement device\",\"Pressure transmitters\",\"Process safety\"],\"articleSection\":[\"Applications\"],\"inLanguage\":\"en-GB\"},{\"@type\":\"WebPage\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\\\/\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\\\/\",\"name\":\"Pressure monitoring in UHT plant without risk of contamination - WIKA blog\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\"},\"primaryImageOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\\\/#primaryimage\"},\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2023\\\/05\\\/beitragsbild_uht-anlage-838x471-2.jpg\",\"datePublished\":\"2023-04-27T04:34:09+00:00\",\"dateModified\":\"2025-05-19T09:41:19+00:00\",\"author\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/8710ec58b46c9dcd86997cf055ce6411\"},\"description\":\"A manufacturer switched to WIKA pressure transmitters with diaphragm monitoring for process-reliable pressure monitoring in its UHT system.\",\"breadcrumb\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\\\/#breadcrumb\"},\"inLanguage\":\"en-GB\",\"potentialAction\":[{\"@type\":\"ReadAction\",\"target\":[\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\\\/\"]}]},{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\\\/#primaryimage\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2023\\\/05\\\/beitragsbild_uht-anlage-838x471-2.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2023\\\/05\\\/beitragsbild_uht-anlage-838x471-2.jpg\",\"width\":838,\"height\":471,\"caption\":\"Tubular Aseptic UHT Pasteurizer with Vacuum Deaerator\"},{\"@type\":\"BreadcrumbList\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\\\/#breadcrumb\",\"itemListElement\":[{\"@type\":\"ListItem\",\"position\":1,\"name\":\"Home\",\"item\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\"},{\"@type\":\"ListItem\",\"position\":2,\"name\":\"Pressure monitoring in UHT plant without risk of contamination\"}]},{\"@type\":\"WebSite\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\",\"name\":\"WIKA blog\",\"description\":\"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.\",\"potentialAction\":[{\"@type\":\"SearchAction\",\"target\":{\"@type\":\"EntryPoint\",\"urlTemplate\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/?s={search_term_string}\"},\"query-input\":{\"@type\":\"PropertyValueSpecification\",\"valueRequired\":true,\"valueName\":\"search_term_string\"}}],\"inLanguage\":\"en-GB\"},{\"@type\":\"Person\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/8710ec58b46c9dcd86997cf055ce6411\",\"name\":\"Jing Lyu\",\"image\":{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2016\\\/05\\\/jing-lu-140x140.jpg\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2016\\\/05\\\/jing-lu-140x140.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2016\\\/05\\\/jing-lu-140x140.jpg\",\"caption\":\"Jing Lyu\"},\"description\":\"Since October 2015, I have been working at WIKA and am currently employed as a Content Marketing Manager. I am particularly interested in new customer solutions, innovative technologies, and forward-looking developments in measurement and sensor technology. With my articles, I aim to explain technical relationships in a simple and understandable way, provide guidance, and answer common questions in a practical manner \u2013 enabling users to quickly find the solutions that truly help them move forward.\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/author\\\/lujing\\\/\"}]}<\/script>\n<!-- \/ Yoast SEO plugin. -->","yoast_head_json":{"title":"Pressure monitoring in UHT plant without risk of contamination - WIKA blog","description":"A manufacturer switched to WIKA pressure transmitters with diaphragm monitoring for process-reliable pressure monitoring in its UHT system.","robots":{"index":"index","follow":"follow","max-snippet":"max-snippet:-1","max-image-preview":"max-image-preview:large","max-video-preview":"max-video-preview:-1"},"canonical":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/","og_locale":"en_GB","og_type":"article","og_title":"Pressure monitoring in UHT plant without risk of contamination - WIKA blog","og_description":"A manufacturer switched to WIKA pressure transmitters with diaphragm monitoring for process-reliable pressure monitoring in its UHT system.","og_url":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/","og_site_name":"WIKA blog","og_image":[{"width":838,"height":471,"url":"https:\/\/blog.wika.com\/en\/files\/2023\/05\/beitragsbild_uht-anlage-838x471-2.jpg","type":"image\/jpeg"}],"author":"Jing Lyu","twitter_misc":{"Written by":"Jing Lyu","Estimated reading time":"4 minutes"},"schema":{"@context":"https:\/\/schema.org","@graph":[{"@type":"Article","@id":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/#article","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/"},"author":{"name":"Jing Lyu","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/8710ec58b46c9dcd86997cf055ce6411"},"headline":"Pressure monitoring in UHT plant without risk of contamination","datePublished":"2023-04-27T04:34:09+00:00","dateModified":"2025-05-19T09:41:19+00:00","mainEntityOfPage":{"@id":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/"},"wordCount":707,"commentCount":0,"image":{"@id":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2023\/05\/beitragsbild_uht-anlage-838x471-2.jpg","keywords":["Cleaning","Food\/Beverages","Measuring point","Operating conditions","Pressure measurement device","Pressure transmitters","Process safety"],"articleSection":["Applications"],"inLanguage":"en-GB"},{"@type":"WebPage","@id":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/","url":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/","name":"Pressure monitoring in UHT plant without risk of contamination - WIKA blog","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/#website"},"primaryImageOfPage":{"@id":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/#primaryimage"},"image":{"@id":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2023\/05\/beitragsbild_uht-anlage-838x471-2.jpg","datePublished":"2023-04-27T04:34:09+00:00","dateModified":"2025-05-19T09:41:19+00:00","author":{"@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/8710ec58b46c9dcd86997cf055ce6411"},"description":"A manufacturer switched to WIKA pressure transmitters with diaphragm monitoring for process-reliable pressure monitoring in its UHT system.","breadcrumb":{"@id":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/#breadcrumb"},"inLanguage":"en-GB","potentialAction":[{"@type":"ReadAction","target":["https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/"]}]},{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/#primaryimage","url":"https:\/\/blog.wika.com\/en\/files\/2023\/05\/beitragsbild_uht-anlage-838x471-2.jpg","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2023\/05\/beitragsbild_uht-anlage-838x471-2.jpg","width":838,"height":471,"caption":"Tubular Aseptic UHT Pasteurizer with Vacuum Deaerator"},{"@type":"BreadcrumbList","@id":"https:\/\/blog.wika.com\/en\/applications\/pressure-monitoring-in-uht-plant-without-risk-of-contamination\/#breadcrumb","itemListElement":[{"@type":"ListItem","position":1,"name":"Home","item":"https:\/\/blog.wika.com\/en\/"},{"@type":"ListItem","position":2,"name":"Pressure monitoring in UHT plant without risk of contamination"}]},{"@type":"WebSite","@id":"https:\/\/blog.wika.com\/en\/#website","url":"https:\/\/blog.wika.com\/en\/","name":"WIKA blog","description":"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.","potentialAction":[{"@type":"SearchAction","target":{"@type":"EntryPoint","urlTemplate":"https:\/\/blog.wika.com\/en\/?s={search_term_string}"},"query-input":{"@type":"PropertyValueSpecification","valueRequired":true,"valueName":"search_term_string"}}],"inLanguage":"en-GB"},{"@type":"Person","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/8710ec58b46c9dcd86997cf055ce6411","name":"Jing Lyu","image":{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/files\/2016\/05\/jing-lu-140x140.jpg","url":"https:\/\/blog.wika.com\/en\/files\/2016\/05\/jing-lu-140x140.jpg","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2016\/05\/jing-lu-140x140.jpg","caption":"Jing Lyu"},"description":"Since October 2015, I have been working at WIKA and am currently employed as a Content Marketing Manager. I am particularly interested in new customer solutions, innovative technologies, and forward-looking developments in measurement and sensor technology. With my articles, I aim to explain technical relationships in a simple and understandable way, provide guidance, and answer common questions in a practical manner \u2013 enabling users to quickly find the solutions that truly help them move forward.","url":"https:\/\/blog.wika.com\/en\/author\/lujing\/"}]}},"_links":{"self":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/50644","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/users\/134"}],"replies":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/comments?post=50644"}],"version-history":[{"count":8,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/50644\/revisions"}],"predecessor-version":[{"id":51883,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/50644\/revisions\/51883"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media\/50677"}],"wp:attachment":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media?parent=50644"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/categories?post=50644"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/tags?post=50644"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}