{"id":51015,"date":"2023-11-23T09:00:16","date_gmt":"2023-11-23T08:00:16","guid":{"rendered":"https:\/\/blog.wika.com\/en\/?p=51015"},"modified":"2024-07-10T10:49:09","modified_gmt":"2024-07-10T08:49:09","slug":"advantages-of-in-situ-calibration-using-the-example-of-pressure-switches","status":"publish","type":"post","link":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/","title":{"rendered":"Advantages of in-situ calibration using the example of pressure switches"},"content":{"rendered":"<p><strong>In-situ calibration of measuring instruments is carried out in numerous industrial processes. The advantages are obvious: The instruments remain installed, so the process does not have to be opened. In this way, plant operators reduce the time and costs involved in testing. At the same time, they rule out potential errors when reinstalling the instruments following their calibration in the laboratory. A prerequisite for in-situ calibration is usually the setting up of the measuring location with appropriate instrumentation valves, as shown below, using an example of pressure switch measuring locations in an incineration plant for liquid waste.<\/strong><\/p>\n<p>The operator of the plant is a company that specialises in the disposal of contaminated residues from the chemical industry. In its incineration plant for liquid waste, 46 pressure switches perform central monitoring tasks. This primarily involves maintaining the energy supply for the incineration process. If the pressure required for this falls below the defined limit value, the measuring instruments trigger a process stop. This is because, with an insufficient supply of natural gas, air and steam, for example, the plant cannot incinerate the substances fed into it properly. In such a case, the operator must therefore immediately determine the cause of the insufficient pressure. A blocked pipe or a technical defect would be typical examples.<\/p>\n<h2>46 pressure switches require a considerable amount of testing<\/h2>\n<p>The pressure switches are calibrated once a year during the regular system shutdown. Previously, the company had the instruments disassembled for this purpose. This meant that they were first electrically disconnected and then disassembled. The pressure switches were then sent to the company&#8217;s own test laboratory and, after successful calibration and any necessary adjustments, returned to the plant for installation. Given the number of 46 pressure switches, the testing process required a considerable amount of time and effort, which was further exacerbated by the confined installation environment.<\/p>\n<p>The company was looking for an alternative and, in collaboration with WIKA, implemented the possibility of in-situ calibration. It is based on two instrumentation valve models from WIKA, to which the pressure switches were screwed and connected to the process. Depending on the installation situation, these are the compact model IVM monoflange and the model IV2 valve block, both in block-and-bleed version. As the measuring points in question are safety-relevant, the company opted for valve variants with a removable handle: they prevent unintentional adjustment of the valves and thus impairment or even decommissioning of the attached measuring device.<\/p>\n<h2>In-situ calibration increases system availability<\/h2>\n<p>For in-situ calibration, the operator first closes the block valve. This isolates the pressure supply to the switches from the process. This is followed by venting via the bleed port. This is also the interface for the calibrator and the pump for generating the test pressure. The switch point is approached three times with the mobile test instrument and adjusted if necessary. Calibration is therefore completed in a much shorter time, which increases plant availability. At the same time, the entire loop from the pressure switch to the control room is tested in one go. This also provides the operator with information on the deviation of the entire active chain in the electrical loop, including the display, alarm or switching action.<\/p>\n<p>However, a measuring location for in-situ calibration offers yet another advantage: If a fault is suspected between the regular calibration intervals, the switching functions and limit values of individual pressure switches can also be checked while the process is running.<\/p>\n<h2>Valves fulfil high demands on safety and service life<\/h2>\n<p>The instrumentation valves from WIKA, selected for in-situ calibration, fulfil the customer&#8217;s requirements for safety and service life of process components. The upper bodies of models IV2 and IVM have a blow-out proof valve spindle and a non-rotating spindle tip with metal seat for low-wear operation. A low torque ensures smooth and precise valve adjustment, even at high pressures. Both valves are also available in a version to prevent fugitive emissions, in accordance with ISO 15848-1 and TA-Luft (VDI 2440).<\/p>\n\n      <div class=\"wp-caption alignright\" style=\"max-width:846px;\"><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/en\/files\/2023\/11\/textbild_kalibrieren-in-situ_fw_beide-838x291.jpg\" alt=\"The attachment of instrumentation valves to pressure switches in block-and-bleed version enables in-situ calibration; on the left with valve block and on the right with mono flange.\" \/><p class=\"wp-caption-text\">Before \u2013 after: Pressure switch measuring locations in conventional design (left illustration) and with WIKA instrumentation valves for in-situ calibration (right illustration), in this case with model IV2 valve block and model IVM mono flange (right).<\/p><\/div>\n    \n<p>&nbsp;<\/p>\n<p>&nbsp;<\/p>\n<p>&nbsp;<\/p>\n<p>&nbsp;<\/p>\n<p><strong><\/p>\n<p>Note<br \/>\n<\/strong>On the WIKA website you will find further information on the <a href=\"https:\/\/www.wika.com\/en-en\/ivm.WIKA\" rel=\"external\" target=\"_blank\">IVM<\/a> and <a href=\"https:\/\/www.wika.com\/en-en\/iv2.WIKA\" rel=\"external\" target=\"_blank\">IV2<\/a>\u00a0instrumentation valves as well as an overview of other <a href=\"https:\/\/www.wika.com\/en-en\/valves_and_protective_devices.WIKA\" rel=\"external\" target=\"_blank\">valves and protective devices<\/a>. There, you can also find out about WIKA&#8217;s measurement solutions for the <a href=\"https:\/\/www.wika.com\/en-en\/chemical_industry.WIKA\" rel=\"external\" target=\"_blank\">chemical industry<\/a> in general and specifically for the prevention of <a href=\"https:\/\/www.wika.com\/en-en\/fugitive_emissions.WIKA\" rel=\"external\" target=\"_blank\">fugitive emissions<\/a>. For the on-site calibration of pressure measuring instruments, we also feature the CPH7000 portable process calibrator, the <a href=\"https:\/\/www.wika.com\/en-en\/cpp30.WIKA\" rel=\"external\" target=\"_blank\">CPP30<\/a> hand test pump and the <a href=\"https:\/\/www.wika.com\/en-en\/cpg1500.WIKA\" rel=\"external\" target=\"_blank\">CPG1500<\/a> precision digital pressure gauge on the website.<\/p>\n<p>In addition, WIKA offers a customer-specific assembly with measuring instrument for all valves. Such \u201cinstrument hook-ups\u201d are delivered ready for operation and leak tested.<\/p>\n<p>If you have any questions, your <a href=\"https:\/\/www.wika.com\/en-en\/contact.WIKA\" rel=\"external\" target=\"_blank\">contact<\/a> will gladly help you.<\/p>\n<p><strong>Also read our posts<\/strong><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/knowhow\/avoid-fugitive-emissions-through-prevention\/\">Avoiding fugitive emissions through prevention<\/a><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/knowhow\/play-it-safe-with-double-block-bleed\/\">Play it safe with double block &amp; bleed<\/a><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/knowhow\/how-does-a-monoflange-work\/\">How does a monoflange work?<\/a><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/knowhow\/combination-of-pressure-measuring-instrument-with-accessories\/\">Combination of pressure measuring instrument with accessories: Instrument hook-up instead of own assembly<\/a><\/p>\n","protected":false},"excerpt":{"rendered":"<p>In-situ calibration of measuring instruments is carried out in numerous industrial processes. The advantages are obvious: The instruments remain installed, so the process does not have to be opened. In this way, plant operators reduce the time and costs involved in testing. At the same time, they rule out potential errors when reinstalling the instruments [&hellip;]<\/p>\n","protected":false},"author":134,"featured_media":51018,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"_acf_changed":false,"footnotes":""},"categories":[232],"tags":[517,286,284,563,79,721,462],"class_list":["post-51015","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-applications","tag-calibration","tag-chemical","tag-measuring-point","tag-pressure","tag-pressure-switch","tag-process-safety","tag-valves-and-controllers"],"acf":[],"yoast_head":"<!-- This site is optimized with the Yoast SEO plugin v27.6 - https:\/\/yoast.com\/product\/yoast-seo-wordpress\/ -->\n<title>Advantages of in-situ calibration using the example of pressure switches - WIKA blog<\/title>\n<meta name=\"description\" content=\"The testing effort can be reduced with in-situ calibration. This is shown by the example of pressure switches in an incineration plant.\" \/>\n<meta name=\"robots\" content=\"index, follow, max-snippet:-1, max-image-preview:large, max-video-preview:-1\" \/>\n<link rel=\"canonical\" href=\"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/\" \/>\n<meta property=\"og:locale\" content=\"en_GB\" \/>\n<meta property=\"og:type\" content=\"article\" \/>\n<meta property=\"og:title\" content=\"Advantages of in-situ calibration using the example of pressure switches - WIKA blog\" \/>\n<meta property=\"og:description\" content=\"The testing effort can be reduced with in-situ calibration. This is shown by the example of pressure switches in an incineration plant.\" \/>\n<meta property=\"og:url\" content=\"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/\" \/>\n<meta property=\"og:site_name\" content=\"WIKA blog\" \/>\n<meta property=\"og:image\" content=\"https:\/\/blog.wika.com\/en\/files\/2023\/11\/beitragsbild_kalibrieren-in-situ.jpg\" \/>\n\t<meta property=\"og:image:width\" content=\"838\" \/>\n\t<meta property=\"og:image:height\" content=\"471\" \/>\n\t<meta property=\"og:image:type\" content=\"image\/jpeg\" \/>\n<meta name=\"author\" content=\"Jing Lyu\" \/>\n<meta name=\"twitter:label1\" content=\"Written by\" \/>\n\t<meta name=\"twitter:data1\" content=\"Jing Lyu\" \/>\n\t<meta name=\"twitter:label2\" content=\"Estimated reading time\" \/>\n\t<meta name=\"twitter:data2\" content=\"5 minutes\" \/>\n<script type=\"application\/ld+json\" class=\"yoast-schema-graph\">{\"@context\":\"https:\\\/\\\/schema.org\",\"@graph\":[{\"@type\":\"Article\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\\\/#article\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\\\/\"},\"author\":{\"name\":\"Jing Lyu\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/8710ec58b46c9dcd86997cf055ce6411\"},\"headline\":\"Advantages of in-situ calibration using the example of pressure switches\",\"datePublished\":\"2023-11-23T08:00:16+00:00\",\"dateModified\":\"2024-07-10T08:49:09+00:00\",\"mainEntityOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\\\/\"},\"wordCount\":870,\"commentCount\":0,\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2023\\\/11\\\/beitragsbild_kalibrieren-in-situ.jpg\",\"keywords\":[\"Calibration\",\"Chemical\",\"Measuring point\",\"Pressure\",\"Pressure switch\",\"Process safety\",\"Valves &amp; Controllers\"],\"articleSection\":[\"Applications\"],\"inLanguage\":\"en-GB\"},{\"@type\":\"WebPage\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\\\/\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\\\/\",\"name\":\"Advantages of in-situ calibration using the example of pressure switches - WIKA blog\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\"},\"primaryImageOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\\\/#primaryimage\"},\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2023\\\/11\\\/beitragsbild_kalibrieren-in-situ.jpg\",\"datePublished\":\"2023-11-23T08:00:16+00:00\",\"dateModified\":\"2024-07-10T08:49:09+00:00\",\"author\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/8710ec58b46c9dcd86997cf055ce6411\"},\"description\":\"The testing effort can be reduced with in-situ calibration. This is shown by the example of pressure switches in an incineration plant.\",\"breadcrumb\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\\\/#breadcrumb\"},\"inLanguage\":\"en-GB\",\"potentialAction\":[{\"@type\":\"ReadAction\",\"target\":[\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\\\/\"]}]},{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\\\/#primaryimage\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2023\\\/11\\\/beitragsbild_kalibrieren-in-situ.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2023\\\/11\\\/beitragsbild_kalibrieren-in-situ.jpg\",\"width\":838,\"height\":471,\"caption\":\"The testing effort can be reduced with in-situ calibration.\"},{\"@type\":\"BreadcrumbList\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\\\/#breadcrumb\",\"itemListElement\":[{\"@type\":\"ListItem\",\"position\":1,\"name\":\"Home\",\"item\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\"},{\"@type\":\"ListItem\",\"position\":2,\"name\":\"Advantages of in-situ calibration using the example of pressure switches\"}]},{\"@type\":\"WebSite\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\",\"name\":\"WIKA blog\",\"description\":\"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.\",\"potentialAction\":[{\"@type\":\"SearchAction\",\"target\":{\"@type\":\"EntryPoint\",\"urlTemplate\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/?s={search_term_string}\"},\"query-input\":{\"@type\":\"PropertyValueSpecification\",\"valueRequired\":true,\"valueName\":\"search_term_string\"}}],\"inLanguage\":\"en-GB\"},{\"@type\":\"Person\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/8710ec58b46c9dcd86997cf055ce6411\",\"name\":\"Jing Lyu\",\"image\":{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2016\\\/05\\\/jing-lu-140x140.jpg\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2016\\\/05\\\/jing-lu-140x140.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2016\\\/05\\\/jing-lu-140x140.jpg\",\"caption\":\"Jing Lyu\"},\"description\":\"Since October 2015, I have been working at WIKA and am currently employed as a Content Marketing Manager. I am particularly interested in new customer solutions, innovative technologies, and forward-looking developments in measurement and sensor technology. With my articles, I aim to explain technical relationships in a simple and understandable way, provide guidance, and answer common questions in a practical manner \u2013 enabling users to quickly find the solutions that truly help them move forward.\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/author\\\/lujing\\\/\"}]}<\/script>\n<!-- \/ Yoast SEO plugin. -->","yoast_head_json":{"title":"Advantages of in-situ calibration using the example of pressure switches - WIKA blog","description":"The testing effort can be reduced with in-situ calibration. This is shown by the example of pressure switches in an incineration plant.","robots":{"index":"index","follow":"follow","max-snippet":"max-snippet:-1","max-image-preview":"max-image-preview:large","max-video-preview":"max-video-preview:-1"},"canonical":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/","og_locale":"en_GB","og_type":"article","og_title":"Advantages of in-situ calibration using the example of pressure switches - WIKA blog","og_description":"The testing effort can be reduced with in-situ calibration. This is shown by the example of pressure switches in an incineration plant.","og_url":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/","og_site_name":"WIKA blog","og_image":[{"width":838,"height":471,"url":"https:\/\/blog.wika.com\/en\/files\/2023\/11\/beitragsbild_kalibrieren-in-situ.jpg","type":"image\/jpeg"}],"author":"Jing Lyu","twitter_misc":{"Written by":"Jing Lyu","Estimated reading time":"5 minutes"},"schema":{"@context":"https:\/\/schema.org","@graph":[{"@type":"Article","@id":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/#article","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/"},"author":{"name":"Jing Lyu","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/8710ec58b46c9dcd86997cf055ce6411"},"headline":"Advantages of in-situ calibration using the example of pressure switches","datePublished":"2023-11-23T08:00:16+00:00","dateModified":"2024-07-10T08:49:09+00:00","mainEntityOfPage":{"@id":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/"},"wordCount":870,"commentCount":0,"image":{"@id":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2023\/11\/beitragsbild_kalibrieren-in-situ.jpg","keywords":["Calibration","Chemical","Measuring point","Pressure","Pressure switch","Process safety","Valves &amp; Controllers"],"articleSection":["Applications"],"inLanguage":"en-GB"},{"@type":"WebPage","@id":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/","url":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/","name":"Advantages of in-situ calibration using the example of pressure switches - WIKA blog","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/#website"},"primaryImageOfPage":{"@id":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/#primaryimage"},"image":{"@id":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2023\/11\/beitragsbild_kalibrieren-in-situ.jpg","datePublished":"2023-11-23T08:00:16+00:00","dateModified":"2024-07-10T08:49:09+00:00","author":{"@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/8710ec58b46c9dcd86997cf055ce6411"},"description":"The testing effort can be reduced with in-situ calibration. This is shown by the example of pressure switches in an incineration plant.","breadcrumb":{"@id":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/#breadcrumb"},"inLanguage":"en-GB","potentialAction":[{"@type":"ReadAction","target":["https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/"]}]},{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/#primaryimage","url":"https:\/\/blog.wika.com\/en\/files\/2023\/11\/beitragsbild_kalibrieren-in-situ.jpg","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2023\/11\/beitragsbild_kalibrieren-in-situ.jpg","width":838,"height":471,"caption":"The testing effort can be reduced with in-situ calibration."},{"@type":"BreadcrumbList","@id":"https:\/\/blog.wika.com\/en\/applications\/advantages-of-in-situ-calibration-using-the-example-of-pressure-switches\/#breadcrumb","itemListElement":[{"@type":"ListItem","position":1,"name":"Home","item":"https:\/\/blog.wika.com\/en\/"},{"@type":"ListItem","position":2,"name":"Advantages of in-situ calibration using the example of pressure switches"}]},{"@type":"WebSite","@id":"https:\/\/blog.wika.com\/en\/#website","url":"https:\/\/blog.wika.com\/en\/","name":"WIKA blog","description":"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.","potentialAction":[{"@type":"SearchAction","target":{"@type":"EntryPoint","urlTemplate":"https:\/\/blog.wika.com\/en\/?s={search_term_string}"},"query-input":{"@type":"PropertyValueSpecification","valueRequired":true,"valueName":"search_term_string"}}],"inLanguage":"en-GB"},{"@type":"Person","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/8710ec58b46c9dcd86997cf055ce6411","name":"Jing Lyu","image":{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/files\/2016\/05\/jing-lu-140x140.jpg","url":"https:\/\/blog.wika.com\/en\/files\/2016\/05\/jing-lu-140x140.jpg","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2016\/05\/jing-lu-140x140.jpg","caption":"Jing Lyu"},"description":"Since October 2015, I have been working at WIKA and am currently employed as a Content Marketing Manager. I am particularly interested in new customer solutions, innovative technologies, and forward-looking developments in measurement and sensor technology. With my articles, I aim to explain technical relationships in a simple and understandable way, provide guidance, and answer common questions in a practical manner \u2013 enabling users to quickly find the solutions that truly help them move forward.","url":"https:\/\/blog.wika.com\/en\/author\/lujing\/"}]}},"_links":{"self":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/51015","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/users\/134"}],"replies":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/comments?post=51015"}],"version-history":[{"count":9,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/51015\/revisions"}],"predecessor-version":[{"id":51413,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/51015\/revisions\/51413"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media\/51018"}],"wp:attachment":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media?parent=51015"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/categories?post=51015"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/tags?post=51015"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}