{"id":51502,"date":"2024-09-05T11:21:14","date_gmt":"2024-09-05T09:21:14","guid":{"rendered":"https:\/\/blog.wika.com\/en\/?p=51502"},"modified":"2026-05-04T12:08:45","modified_gmt":"2026-05-04T10:08:45","slug":"temperature-transmitter-t38-doesnt-give-drift-a-chance","status":"publish","type":"post","link":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/","title":{"rendered":"Temperature transmitter T38 doesn\u2019t give drift a chance"},"content":{"rendered":"<p><strong>For plant operators a permanent temperature sensor\u2019s drift tends to be a pain in the neck. This defect usually becomes apparent at a following calibration \u2013 in other words: too late! Until then it might have caused a false temperature measurement and compromised the process in the end. <\/strong><\/p>\n<p>WIKA\u2019s newly developed temperature transmitter T38 now enables the user to prevent this kind of defect from happening. Its prominent feature is the unique True Drift Detection (TDD). Connected with a specific WIKA thermometer, it continuously monitors the complete measuring range for critical deviation. The technology works for measuring ranges from -50 \u00b0C up to +500 \u00b0C. This combination provides a comprehensive self-monitoring of the sensor, making it fit perfectly into digitalised processes.<\/p>\n<h2>True Drift Detection: Demand-driven interventions instead of fixed recurring checks<\/h2>\n<p>Resistance thermometers are widely used to monitor process temperatures. Although generally robust, a persistent above-average stress causes the sensor to drift, induced for instance by high temperatures, heavy temperature fluctuations or humidity. While processing the sensor signal, the read-out unit of temperature transmitter T38 will immediately detect any critical deviation of the resistance characteristic. It has implemented a smart algorithm in order to check and compare the values measured by the matched sensor and the reference element. The defect is then reported via HART<sup>\u00ae<\/sup> communication protocol or on the current loop.<\/p>\n<p>The plant operator is able to react in due time. Such condition monitoring leads to immediate, demand-driven interventions. Otherwise, a drift would not be detected until the next recurring check based on a defined maintenance plan. Thus, TDD makes processes more reliable and safer.<\/p>\n<h2>Probe with integrated reference: Easy upgrade of measuring locations<\/h2>\n<p>For TDD, the temperature transmitter has to be combined with an appropriate WIKA thermometer. The probe design is based on the proven temperature measurement principle with a platinum resistor (RTD) in accordance with IEC\/EN 60751. The reference element is installed parallel to the RTD in the probe tip and perfectly matched for optimal measuring and monitoring results. The sensor has a resistance characteristic conforming to the standard, and the instrument always indicates the currently measured value. The reference element and its signal are prevented from averaging or distorting the measured value by the underlying concept of the TDD technology. Since the probe has identical geometry to conventional solutions, existing measuring locations can be upgraded easily.<\/p>\n<h2>Temperature transmitter T38: Distinct versatility and uncomplicated installation<\/h2>\n<p>The temperature transmitter T38 offers distinct versatility for all branches of the process industry. It\u2019s available as head or rail-mounted version. The head version can also be supplemented with a clip-on display for on-site readout. Besides the TDD thermometer, the transmitter supports all common sensor types, which can be connected and measured as single or dual sensors. A wide choice of measuring ranges is provided accordingly.<\/p>\n<p>The upshot for users is a temperature measuring system tailor-made for their particular application, which is ready to use straight away. It can be integrated into the process according to the plug-and-play principle. Any altering of configuration can be easily and flawlessly accomplished via HART<sup>\u00ae<\/sup> protocol.<\/p>\n<h2>T38 with SIL 2 and new Ex d field housing: Solution for use in hazardous areas<\/h2>\n<p>Concerning safety applications, the temperature transmitter T38 is first class. Both instrument models have SIL 2 certification in accordance with IEC 61508 and are approved for use in hazardous areas. A mineral-insulated metal-sheathed cable, which was specially developed for True Drift Detection, supports the resilience of the entire thermometer. Furthermore, the transmitter can be combined with the new Ex d field housing, model PIH\/PIR, showing a distinct resistance to extreme temperatures, humidity, mechanical stress and the effects of salt water.<\/p>\n<p>Another safety feature is added by the special trapezoidal terminal design of the head-mounted version of the T38. Its very large clamping area and an access from the outside enables error-free connection of both the probe and the current loop.<\/p>\n<h2>Conclusion<\/h2>\n<p>WIKA\u2019s T38 marks a new generation of temperature transmitters, supporting plant operators to increase the efficiency and safety of their processes. It offers:<\/p>\n<ul>\n<li>Comprehensive condition monitoring due to the True Drift Detection over a measuring range from -50 \u00b0C to +500 \u00b0C<\/li>\n<li>Suitability for all branches of the process industry, especially for safety applications and digitalised processes<\/li>\n<li>Easy and error-free installation, including the upgrade of existing measuring locations<\/li>\n<\/ul>\n<p><strong>Note<\/strong><br \/>\nFor more and detailed information about the temperature transmitter T38, please have a look on the <a href=\"https:\/\/www.wika.com\/en-en\/lp_t38_temperature_transmitter.WIKA\" rel=\"external\" target=\"_blank\">WIKA website<\/a>. There you will also find an overview of other measurement solutions for the process industry. Should you have any further questions, your <a href=\"https:\/\/www.wika.com\/en-en\/contact.WIKA\" rel=\"external\" target=\"_blank\">contact<\/a> will gladly help you.<\/p>\n<p><strong>Also read our posts<\/strong><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/knowhow\/ice-cold-electrical-thermometers-in-low-ambient-temperatures\/\"><span data-contrast=\"none\">Ice cold \u2013 Electrical thermometers in low ambient temperatures<\/span><\/a><span data-ccp-props=\"{&quot;201341983&quot;:0,&quot;335559739&quot;:160,&quot;335559740&quot;:259}\">\u00a0<br \/>\n<\/span><a href=\"https:\/\/blog.wika.com\/en\/products\/temperature-products\/application-of-sapphire-thermocouples-in-gasification-reactors\/\"><span data-contrast=\"none\">Application of sapphire thermocouples in gasification reactors<\/span><\/a><span data-ccp-props=\"{&quot;201341983&quot;:0,&quot;335559739&quot;:160,&quot;335559740&quot;:259}\">\u00a0<br \/>\n<\/span><a href=\"https:\/\/blog.wika.com\/en\/knowhow\/measuring-the-response-times-of-electrical-thermometers\/\"><span data-contrast=\"none\">Measuring the response times of electrical thermometers<\/span><\/a><span data-ccp-props=\"{&quot;201341983&quot;:0,&quot;335559739&quot;:160,&quot;335559740&quot;:259}\">\u00a0<br \/>\n<\/span><a href=\"https:\/\/blog.wika.com\/en\/knowhow\/temperature-calibration-with-reference-probes-dry-well-calibrators-and-baths\/\"><span data-contrast=\"none\">Temperature calibration with reference probes, dry-well calibrators and baths<\/span><\/a><span data-ccp-props=\"{&quot;201341983&quot;:0,&quot;335559739&quot;:160,&quot;335559740&quot;:259}\">\u00a0<\/span><\/p>\n","protected":false},"excerpt":{"rendered":"<p>For plant operators a permanent temperature sensor\u2019s drift tends to be a pain in the neck. This defect usually becomes apparent at a following calibration \u2013 in other words: too late! Until then it might have caused a false temperature measurement and compromised the process in the end. WIKA\u2019s newly developed temperature transmitter T38 now [&hellip;]<\/p>\n","protected":false},"author":382,"featured_media":51505,"comment_status":"closed","ping_status":"closed","sticky":false,"template":"","format":"standard","meta":{"_acf_changed":false,"footnotes":""},"categories":[6,221],"tags":[286,262,719,714,721,304,367],"class_list":["post-51502","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-products","category-temperature-products","tag-chemical","tag-functional-safety-sil","tag-oil-and-gas","tag-pharmaceuticals-and-biotechnology","tag-process-safety","tag-thermometer","tag-transmitter"],"acf":[],"yoast_head":"<!-- This site is optimized with the Yoast SEO plugin v27.6 - https:\/\/yoast.com\/product\/yoast-seo-wordpress\/ -->\n<title>Temperature transmitter T38 doesn\u2019t give drift a chance - WIKA blog<\/title>\n<meta name=\"description\" content=\"WIKA\u2019s newly developed temperature transmitter T38 is prominent for the unique True Drift Detection (TDD) feature.\" \/>\n<meta name=\"robots\" content=\"index, follow, max-snippet:-1, max-image-preview:large, max-video-preview:-1\" \/>\n<link rel=\"canonical\" href=\"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/\" \/>\n<meta property=\"og:locale\" content=\"en_GB\" \/>\n<meta property=\"og:type\" content=\"article\" \/>\n<meta property=\"og:title\" content=\"Temperature transmitter T38 doesn\u2019t give drift a chance - WIKA blog\" \/>\n<meta property=\"og:description\" content=\"WIKA\u2019s newly developed temperature transmitter T38 is prominent for the unique True Drift Detection (TDD) feature.\" \/>\n<meta property=\"og:url\" content=\"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/\" \/>\n<meta property=\"og:site_name\" content=\"WIKA blog\" \/>\n<meta property=\"og:image\" content=\"https:\/\/blog.wika.com\/en\/files\/2024\/09\/truedriftdetection_en-co.jpg\" \/>\n\t<meta property=\"og:image:width\" content=\"838\" \/>\n\t<meta property=\"og:image:height\" content=\"471\" \/>\n\t<meta property=\"og:image:type\" content=\"image\/jpeg\" \/>\n<meta name=\"author\" content=\"Nadine Daniel\" \/>\n<meta name=\"twitter:label1\" content=\"Written by\" \/>\n\t<meta name=\"twitter:data1\" content=\"Nadine Daniel\" \/>\n\t<meta name=\"twitter:label2\" content=\"Estimated reading time\" \/>\n\t<meta name=\"twitter:data2\" content=\"4 minutes\" \/>\n<script type=\"application\/ld+json\" class=\"yoast-schema-graph\">{\"@context\":\"https:\\\/\\\/schema.org\",\"@graph\":[{\"@type\":\"Article\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/products\\\/temperature-products\\\/temperature-transmitter-t38-doesnt-give-drift-a-chance\\\/#article\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/products\\\/temperature-products\\\/temperature-transmitter-t38-doesnt-give-drift-a-chance\\\/\"},\"author\":{\"name\":\"Nadine Daniel\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/0b045f4071a55b765f8c162e9abd9225\"},\"headline\":\"Temperature transmitter T38 doesn\u2019t give drift a chance\",\"datePublished\":\"2024-09-05T09:21:14+00:00\",\"dateModified\":\"2026-05-04T10:08:45+00:00\",\"mainEntityOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/products\\\/temperature-products\\\/temperature-transmitter-t38-doesnt-give-drift-a-chance\\\/\"},\"wordCount\":804,\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/products\\\/temperature-products\\\/temperature-transmitter-t38-doesnt-give-drift-a-chance\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2024\\\/09\\\/truedriftdetection_en-co.jpg\",\"keywords\":[\"Chemical\",\"Functional safety (SIL)\",\"Oil &amp; Gas\",\"Pharmaceuticals &amp; Biotechnology\",\"Process safety\",\"Thermometer\",\"Transmitter\"],\"articleSection\":[\"Products\",\"Temperature\"],\"inLanguage\":\"en-GB\"},{\"@type\":\"WebPage\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/products\\\/temperature-products\\\/temperature-transmitter-t38-doesnt-give-drift-a-chance\\\/\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/products\\\/temperature-products\\\/temperature-transmitter-t38-doesnt-give-drift-a-chance\\\/\",\"name\":\"Temperature transmitter T38 doesn\u2019t give drift a chance - WIKA blog\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\"},\"primaryImageOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/products\\\/temperature-products\\\/temperature-transmitter-t38-doesnt-give-drift-a-chance\\\/#primaryimage\"},\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/products\\\/temperature-products\\\/temperature-transmitter-t38-doesnt-give-drift-a-chance\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2024\\\/09\\\/truedriftdetection_en-co.jpg\",\"datePublished\":\"2024-09-05T09:21:14+00:00\",\"dateModified\":\"2026-05-04T10:08:45+00:00\",\"author\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/0b045f4071a55b765f8c162e9abd9225\"},\"description\":\"WIKA\u2019s newly developed temperature transmitter T38 is prominent for the unique True Drift Detection (TDD) feature.\",\"breadcrumb\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/products\\\/temperature-products\\\/temperature-transmitter-t38-doesnt-give-drift-a-chance\\\/#breadcrumb\"},\"inLanguage\":\"en-GB\",\"potentialAction\":[{\"@type\":\"ReadAction\",\"target\":[\"https:\\\/\\\/blog.wika.com\\\/en\\\/products\\\/temperature-products\\\/temperature-transmitter-t38-doesnt-give-drift-a-chance\\\/\"]}]},{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/products\\\/temperature-products\\\/temperature-transmitter-t38-doesnt-give-drift-a-chance\\\/#primaryimage\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2024\\\/09\\\/truedriftdetection_en-co.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2024\\\/09\\\/truedriftdetection_en-co.jpg\",\"width\":838,\"height\":471},{\"@type\":\"BreadcrumbList\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/products\\\/temperature-products\\\/temperature-transmitter-t38-doesnt-give-drift-a-chance\\\/#breadcrumb\",\"itemListElement\":[{\"@type\":\"ListItem\",\"position\":1,\"name\":\"Home\",\"item\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\"},{\"@type\":\"ListItem\",\"position\":2,\"name\":\"Temperature transmitter T38 doesn\u2019t give drift a chance\"}]},{\"@type\":\"WebSite\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\",\"name\":\"WIKA blog\",\"description\":\"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.\",\"potentialAction\":[{\"@type\":\"SearchAction\",\"target\":{\"@type\":\"EntryPoint\",\"urlTemplate\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/?s={search_term_string}\"},\"query-input\":{\"@type\":\"PropertyValueSpecification\",\"valueRequired\":true,\"valueName\":\"search_term_string\"}}],\"inLanguage\":\"en-GB\"},{\"@type\":\"Person\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/0b045f4071a55b765f8c162e9abd9225\",\"name\":\"Nadine Daniel\",\"image\":{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2024\\\/09\\\/danielnadine_de-de-120x120.jpg\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2024\\\/09\\\/danielnadine_de-de-120x120.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2024\\\/09\\\/danielnadine_de-de-120x120.jpg\",\"caption\":\"Nadine Daniel\"},\"description\":\"Since completing my studies in 2021, I have been working as a product manager in the electrical temperature measurement division at WIKA. My areas of expertise include temperature transmitters and digital displays. Previously, I was able to gain valuable experience in calibration technology as a working student at WIKA. After graduating, I started as a junior product manager at ETM before taking on full responsibility as a product manager after 1.5 years. In this blog, I would like to share my knowledge with you and give you exciting insights into new functions and interesting aspects of my specialist area. I look forward to your suggestions and comments!\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/author\\\/nadinedaniel\\\/\"}]}<\/script>\n<!-- \/ Yoast SEO plugin. -->","yoast_head_json":{"title":"Temperature transmitter T38 doesn\u2019t give drift a chance - WIKA blog","description":"WIKA\u2019s newly developed temperature transmitter T38 is prominent for the unique True Drift Detection (TDD) feature.","robots":{"index":"index","follow":"follow","max-snippet":"max-snippet:-1","max-image-preview":"max-image-preview:large","max-video-preview":"max-video-preview:-1"},"canonical":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/","og_locale":"en_GB","og_type":"article","og_title":"Temperature transmitter T38 doesn\u2019t give drift a chance - WIKA blog","og_description":"WIKA\u2019s newly developed temperature transmitter T38 is prominent for the unique True Drift Detection (TDD) feature.","og_url":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/","og_site_name":"WIKA blog","og_image":[{"width":838,"height":471,"url":"https:\/\/blog.wika.com\/en\/files\/2024\/09\/truedriftdetection_en-co.jpg","type":"image\/jpeg"}],"author":"Nadine Daniel","twitter_misc":{"Written by":"Nadine Daniel","Estimated reading time":"4 minutes"},"schema":{"@context":"https:\/\/schema.org","@graph":[{"@type":"Article","@id":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/#article","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/"},"author":{"name":"Nadine Daniel","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/0b045f4071a55b765f8c162e9abd9225"},"headline":"Temperature transmitter T38 doesn\u2019t give drift a chance","datePublished":"2024-09-05T09:21:14+00:00","dateModified":"2026-05-04T10:08:45+00:00","mainEntityOfPage":{"@id":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/"},"wordCount":804,"image":{"@id":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2024\/09\/truedriftdetection_en-co.jpg","keywords":["Chemical","Functional safety (SIL)","Oil &amp; Gas","Pharmaceuticals &amp; Biotechnology","Process safety","Thermometer","Transmitter"],"articleSection":["Products","Temperature"],"inLanguage":"en-GB"},{"@type":"WebPage","@id":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/","url":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/","name":"Temperature transmitter T38 doesn\u2019t give drift a chance - WIKA blog","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/#website"},"primaryImageOfPage":{"@id":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/#primaryimage"},"image":{"@id":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2024\/09\/truedriftdetection_en-co.jpg","datePublished":"2024-09-05T09:21:14+00:00","dateModified":"2026-05-04T10:08:45+00:00","author":{"@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/0b045f4071a55b765f8c162e9abd9225"},"description":"WIKA\u2019s newly developed temperature transmitter T38 is prominent for the unique True Drift Detection (TDD) feature.","breadcrumb":{"@id":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/#breadcrumb"},"inLanguage":"en-GB","potentialAction":[{"@type":"ReadAction","target":["https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/"]}]},{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/#primaryimage","url":"https:\/\/blog.wika.com\/en\/files\/2024\/09\/truedriftdetection_en-co.jpg","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2024\/09\/truedriftdetection_en-co.jpg","width":838,"height":471},{"@type":"BreadcrumbList","@id":"https:\/\/blog.wika.com\/en\/products\/temperature-products\/temperature-transmitter-t38-doesnt-give-drift-a-chance\/#breadcrumb","itemListElement":[{"@type":"ListItem","position":1,"name":"Home","item":"https:\/\/blog.wika.com\/en\/"},{"@type":"ListItem","position":2,"name":"Temperature transmitter T38 doesn\u2019t give drift a chance"}]},{"@type":"WebSite","@id":"https:\/\/blog.wika.com\/en\/#website","url":"https:\/\/blog.wika.com\/en\/","name":"WIKA blog","description":"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.","potentialAction":[{"@type":"SearchAction","target":{"@type":"EntryPoint","urlTemplate":"https:\/\/blog.wika.com\/en\/?s={search_term_string}"},"query-input":{"@type":"PropertyValueSpecification","valueRequired":true,"valueName":"search_term_string"}}],"inLanguage":"en-GB"},{"@type":"Person","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/0b045f4071a55b765f8c162e9abd9225","name":"Nadine Daniel","image":{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/files\/2024\/09\/danielnadine_de-de-120x120.jpg","url":"https:\/\/blog.wika.com\/en\/files\/2024\/09\/danielnadine_de-de-120x120.jpg","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2024\/09\/danielnadine_de-de-120x120.jpg","caption":"Nadine Daniel"},"description":"Since completing my studies in 2021, I have been working as a product manager in the electrical temperature measurement division at WIKA. My areas of expertise include temperature transmitters and digital displays. Previously, I was able to gain valuable experience in calibration technology as a working student at WIKA. After graduating, I started as a junior product manager at ETM before taking on full responsibility as a product manager after 1.5 years. In this blog, I would like to share my knowledge with you and give you exciting insights into new functions and interesting aspects of my specialist area. I look forward to your suggestions and comments!","url":"https:\/\/blog.wika.com\/en\/author\/nadinedaniel\/"}]}},"_links":{"self":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/51502","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/users\/382"}],"replies":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/comments?post=51502"}],"version-history":[{"count":7,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/51502\/revisions"}],"predecessor-version":[{"id":52348,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/51502\/revisions\/52348"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media\/51505"}],"wp:attachment":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media?parent=51502"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/categories?post=51502"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/tags?post=51502"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}