{"id":51941,"date":"2025-07-08T07:10:51","date_gmt":"2025-07-08T05:10:51","guid":{"rendered":"https:\/\/blog.wika.com\/en\/?p=51941"},"modified":"2026-02-23T11:32:08","modified_gmt":"2026-02-23T10:32:08","slug":"level-measurement-for-demanding-biorefinery-applications","status":"publish","type":"post","link":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/","title":{"rendered":"Level measurement for demanding biorefinery applications"},"content":{"rendered":"<p><strong>The production of biofuels is subject to demanding process conditions. These therefore also pose major challenges for level measurement in biorefineries. The instruments used in the core processes, depending on where they are used, must operate in hydrogen-containing hydrocarbons under high pressure and at the same time in liquids with extremely low densities. WIKA supplied a customer with magnetic level indicators with a special configuration that reliably meet these requirements.<\/strong><\/p>\n<p>In the quest for a carbon-reduced fuel supply, high-quality HVO (hydrotreated vegetable oil) and HEFA (hydroprocessed esters and fatty acids) play a central role. Both are sustainable products, primarily made from vegetable oils, used cooking oils and also animal fats. They are sold as diesel, but also as aviation fuel.<\/p>\n<h2>Large numbers of vessels in a biorefinery require precise level measurement<\/h2>\n<p>The production of HVO and HEFA involves important production processes, including hydrotreatment and hydroisomerisation. A large number of reactors, tanks and other vessels are used in this process. These fulfil various functions such as catalytic reactions, separation and washing processes as well as regeneration and storage. In all cases, the operators of a biorefinery require precise level measurement.<\/p>\n<p>Reliable level monitoring is difficult to guarantee with standard instruments, especially under the production conditions described at the beginning. The instruments must function reliably in hydrogen-containing hydrocarbons under increased pressures of up to 58 barg and, at the same time, measure precisely in liquids with exceptionally low densities of down to 462 kg\/m\u00b3.<\/p>\n<h2>Titanium floats are pressure-resistant and light enough for low liquid density<\/h2>\n\n      <div class=\"wp-caption alignright\" style=\"max-width:396px;\"><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/en\/files\/2025\/07\/textbild_biokraftstoffe_test_2-388x471-1.jpg\" \/><p class=\"wp-caption-text\">The product label indicates the application: In this example, the corresponding model BNA bypass level indicator is designed for liquid biopropane. Depending on the respective process media, model BNA for level measurement in biorefineries \u2013 the depicted version features a magnetostrictive sensor and switch contacts \u2013 sometimes requires a DLC-coated titanium float (bottom right).<\/p><\/div>\n    \n<p>The engineering team at the CoE (Centre of Excellence) Level solved this task with a comprehensive approach and the model BNA bypass level indicator as the basic model. Titanium was selected as the material for the float. This material can withstand high pressures. It is also lightweight, which ensures the buoyancy required for precise measurement \u2013 even in the case of a very low liquid density.<\/p>\n<h2>Protection through DLC coating<\/h2>\n<p>For level measurement in a biorefinery, however, the titanium floats had to be given special protection. This is because there is a risk of hydrogen embrittlement under certain process conditions. For this reason, the floats were coated with a special DLC (diamond-like carbon) coating. This layer forms a strong barrier against hydrogen infiltration and also protects against mechanical damage.<\/p>\n<p>The customer\u2019s technical specifications also necessitated an unconventional, oversized instrument design, which added to the complexity. This required a change from a standard chamber (2-inch, schedule 10) to a more robust 3-inch schedule-40 configuration. Consequently, customer-specific floats with an outer diameter of 72 mm had to be manufactured. This was a challenge that was overcome with innovative technical solutions and precise manufacturing processes.<\/p>\n<h2>Special material for the case due to increased risk of corrosion<\/h2>\n<p>Special attention was also paid to the case material when designing the BNA. This is because there is an increased risk of corrosion at certain measuring locations due to the potential presence of free fatty acids, carbon dioxide, water and chlorine in the process media. Inconel 625 was therefore chosen as the material for these measuring locations.<\/p>\n<h2>Level measurement in the biorefinery \u2013 even in the event of a power failure<\/h2>\n<p>By integrating advanced materials, precision engineering and customised manufacturing solutions, WIKA delivered magnetic level indicators that meet stringent performance requirements while ensuring long-term reliability in a demanding refinery environment. As the BNA provides a continuous level indication even without a power supply, reliable process control is ensured even in the event of a power failure.<\/p>\n<p><strong>Note<\/strong><br \/>\nWIKA has also compiled a\u00a0<a href=\"https:\/\/www.wika.com\/en-en\/biofuel_whitepaper_ondemand.WIKA\" target=\"_blank\" rel=\"noopener external\">white paper<\/a>\u00a0containing useful information on biofuels and the measuring instruments used for their production. General technical information on the\u00a0<a href=\"https:\/\/www.wika.com\/en-en\/bna.WIKA\" target=\"_blank\" rel=\"noopener external\">model BNA<\/a>\u00a0bypass level indicator is available on the WIKA website. You can also download our brochure \u201c<a href=\"https:\/\/www.wika.com\/media\/Brochures-and-flyers\/Products_Services\/fl_bna_tailormadelevelsolutions_en_co.pdf\" target=\"_blank\" rel=\"noopener external\">Tailor-made level solutions for the process industry<\/a>\u201d there. We also present further solutions for the\u00a0oil and gas\u00a0market segment. If you have any further questions, please do not hesitate to <a href=\"https:\/\/www.wika.com\/en-en\/contact.WIKA\" target=\"_blank\" rel=\"noopener external\">contact us<\/a> in person.<\/p>\n<p><strong>\u00a0<\/strong><\/p>\n<p><strong>Also read our posts<\/strong><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/applications\/biofuels-and-e-fuels-as-a-boost-for-many-engines\/\" target=\"_blank\" rel=\"noopener\">Biofuels and e-fuels as a boost for many engines<\/a><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/applications\/biofuels-precise-temperature-profile-for-production\/\" target=\"_blank\" rel=\"noopener\">Biofuels: Precise temperature profile for production<\/a><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/applications\/using-a-multipoint-thermocouple-to-produce-sustainable-aviation-fuel\/\" target=\"_blank\" rel=\"noopener\">Using a multipoint thermocouple to produce sustainable aviation fuel<\/a><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/knowhow\/level-limit-switches-innovation-meets-all-rounder\/\" target=\"_blank\" rel=\"noopener\">Level limit switches: innovation meets all-rounder<\/a><\/p>\n<p><strong>\u00a0<\/strong><strong>This video also provides information about bypass level indicator<br \/>\n<\/strong><\/p>\n<div data-fullscreen=\"disabled\" data-mode=\"normal\" data-oembed=\"1\" data-provider=\"youtube\" data-reset-after-played id=\"arve-youtube-praycvqns0m\" style=\"max-width:900px;\" class=\"arve\">\n<div class=\"arve-inner\">\n<div style=\"aspect-ratio:500\/281\" class=\"arve-embed arve-embed--has-aspect-ratio\">\n<div class=\"arve-ar\" style=\"padding-top:56.200000%\"><\/div>\n<p>\t\t\t<iframe allow=\"accelerometer &apos;none&apos;;autoplay &apos;none&apos;;bluetooth &apos;none&apos;;browsing-topics &apos;none&apos;;camera &apos;none&apos;;clipboard-read &apos;none&apos;;clipboard-write;display-capture &apos;none&apos;;encrypted-media &apos;none&apos;;gamepad &apos;none&apos;;geolocation &apos;none&apos;;gyroscope &apos;none&apos;;hid &apos;none&apos;;identity-credentials-get &apos;none&apos;;idle-detection &apos;none&apos;;keyboard-map &apos;none&apos;;local-fonts;magnetometer &apos;none&apos;;microphone &apos;none&apos;;midi &apos;none&apos;;otp-credentials &apos;none&apos;;payment &apos;none&apos;;picture-in-picture;publickey-credentials-create &apos;none&apos;;publickey-credentials-get &apos;none&apos;;screen-wake-lock &apos;none&apos;;serial &apos;none&apos;;summarizer &apos;none&apos;;sync-xhr;usb &apos;none&apos;;web-share;window-management &apos;none&apos;;xr-spatial-tracking &apos;none&apos;;\" allowfullscreen=\"\" class=\"arve-iframe fitvidsignore\" credentialless data-arve=\"arve-youtube-praycvqns0m\" data-lenis-prevent=\"\" data-src-no-ap=\"https:\/\/www.youtube-nocookie.com\/embed\/PrAYcvqNs0M?feature=oembed&amp;iv_load_policy=3&amp;modestbranding=1&amp;rel=0&amp;autohide=1&amp;playsinline=0&amp;autoplay=0&amp;enablejsapi=1\" frameborder=\"0\" height=\"505.8\" loading=\"lazy\" name=\"\" referrerpolicy=\"strict-origin-when-cross-origin\" sandbox=\"allow-scripts allow-same-origin allow-presentation allow-popups allow-popups-to-escape-sandbox\" scrolling=\"no\" src=\"https:\/\/www.youtube-nocookie.com\/embed\/PrAYcvqNs0M?feature=oembed&#038;iv_load_policy=3&#038;modestbranding=1&#038;rel=0&#038;autohide=1&#038;playsinline=0&#038;autoplay=0&#038;enablejsapi=1\" title=\"WIKA - Level indication with bypass indicator\" width=\"900\"><\/iframe><\/p><\/div>\n<\/p><\/div>\n<p>\t<script type=\"application\/ld+json\">{\"@context\":\"http:\\\/\\\/schema.org\\\/\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/#arve-youtube-praycvqns0m\",\"@type\":\"VideoObject\",\"author\":{\"@type\":\"Organization\",\"name\":\"WIKA Group\"},\"embedURL\":\"https:\\\/\\\/www.youtube-nocookie.com\\\/embed\\\/PrAYcvqNs0M?feature=oembed&iv_load_policy=3&modestbranding=1&rel=0&autohide=1&playsinline=0&autoplay=0&enablejsapi=1\",\"name\":\"WIKA - Level indication with bypass indicator\",\"thumbnailUrl\":\"https:\\\/\\\/i.ytimg.com\\\/vi\\\/PrAYcvqNs0M\\\/hqdefault.jpg\",\"uploadDate\":\"2018-06-11T06:22:04Z\",\"description\":\"In a communicating bypass chamber mounted to the side of a vessel a float moves with the level of the medium to be measured. The magnetic field of the radial-symmetric magnetic system activates the magnetic display attached to the outside of the bypass chamber as well as the switching and measuring elements. \\nThe bypass level indicator with magnetic display provides uninterrupted level measurement without power supply. Made of diverse corrosion-resistant materials, it is suitable for all industrial applications.\\n \\n\\ud83c\\udf10 On our website, you'll find information about the bypass level indicator with magnetic display Model BNA  \\n \\n\\u2699\\ufe0f Accessories for bypass level indicators can be found here:  \\n \\n_ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ _ \\n \\nFollow us on our social media channels:\\n\\ud83d\\udcfa YouTube: \\n\\ud83c\\udfaf LinkedIn:\"}<\/script><\/p>\n<\/div>\n","protected":false},"excerpt":{"rendered":"<p>The production of biofuels is subject to demanding process conditions. These therefore also pose major challenges for level measurement in biorefineries. The instruments used in the core processes, depending on where they are used, must operate in hydrogen-containing hydrocarbons under high pressure and at the same time in liquids with extremely low densities. WIKA supplied [&hellip;]<\/p>\n","protected":false},"author":416,"featured_media":51946,"comment_status":"closed","ping_status":"closed","sticky":false,"template":"","format":"standard","meta":{"_acf_changed":false,"footnotes":""},"categories":[232],"tags":[774,756,719,721,465,720],"class_list":["post-51941","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-applications","tag-biofuel","tag-level","tag-oil-and-gas","tag-process-safety","tag-renewable-energy","tag-sustainability"],"acf":[],"yoast_head":"<!-- This site is optimized with the Yoast SEO plugin v27.6 - https:\/\/yoast.com\/product\/yoast-seo-wordpress\/ -->\n<title>Level measurement for demanding biorefinery applications - WIKA blog<\/title>\n<meta name=\"description\" content=\"Level measurement in a biorefinery presents unique challenges. WIKA demonstrates how they can be overcome.\" \/>\n<meta name=\"robots\" content=\"index, follow, max-snippet:-1, max-image-preview:large, max-video-preview:-1\" \/>\n<link rel=\"canonical\" href=\"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/\" \/>\n<meta property=\"og:locale\" content=\"en_GB\" \/>\n<meta property=\"og:type\" content=\"article\" \/>\n<meta property=\"og:title\" content=\"Level measurement for demanding biorefinery applications - WIKA blog\" \/>\n<meta property=\"og:description\" content=\"Level measurement in a biorefinery presents unique challenges. WIKA demonstrates how they can be overcome.\" \/>\n<meta property=\"og:url\" content=\"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/\" \/>\n<meta property=\"og:site_name\" content=\"WIKA blog\" \/>\n<meta property=\"og:image\" content=\"https:\/\/blog.wika.com\/en\/files\/2025\/07\/beitragsbild_biokraftstoffe_level.jpg\" \/>\n\t<meta property=\"og:image:width\" content=\"838\" \/>\n\t<meta property=\"og:image:height\" content=\"471\" \/>\n\t<meta property=\"og:image:type\" content=\"image\/jpeg\" \/>\n<meta name=\"author\" content=\"Ansgar Baule\" \/>\n<meta name=\"twitter:label1\" content=\"Written by\" \/>\n\t<meta name=\"twitter:data1\" content=\"Ansgar Baule\" \/>\n\t<meta name=\"twitter:label2\" content=\"Estimated reading time\" \/>\n\t<meta name=\"twitter:data2\" content=\"5 minutes\" \/>\n<script type=\"application\/ld+json\" class=\"yoast-schema-graph\">{\"@context\":\"https:\\\/\\\/schema.org\",\"@graph\":[{\"@type\":\"Article\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/#article\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/\"},\"author\":{\"name\":\"Ansgar Baule\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/821d6c308cf57dfbadd9200494f82fda\"},\"headline\":\"Level measurement for demanding biorefinery applications\",\"datePublished\":\"2025-07-08T05:10:51+00:00\",\"dateModified\":\"2026-02-23T10:32:08+00:00\",\"mainEntityOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/\"},\"wordCount\":773,\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2025\\\/07\\\/beitragsbild_biokraftstoffe_level.jpg\",\"keywords\":[\"Biofuel\",\"Level\",\"Oil &amp; Gas\",\"Process safety\",\"Renewable energy\",\"Sustainability\"],\"articleSection\":[\"Applications\"],\"inLanguage\":\"en-GB\"},{\"@type\":\"WebPage\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/\",\"name\":\"Level measurement for demanding biorefinery applications - WIKA blog\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\"},\"primaryImageOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/#primaryimage\"},\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2025\\\/07\\\/beitragsbild_biokraftstoffe_level.jpg\",\"datePublished\":\"2025-07-08T05:10:51+00:00\",\"dateModified\":\"2026-02-23T10:32:08+00:00\",\"author\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/821d6c308cf57dfbadd9200494f82fda\"},\"description\":\"Level measurement in a biorefinery presents unique challenges. WIKA demonstrates how they can be overcome.\",\"breadcrumb\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/#breadcrumb\"},\"inLanguage\":\"en-GB\",\"potentialAction\":[{\"@type\":\"ReadAction\",\"target\":[\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/\"]}]},{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/#primaryimage\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2025\\\/07\\\/beitragsbild_biokraftstoffe_level.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2025\\\/07\\\/beitragsbild_biokraftstoffe_level.jpg\",\"width\":838,\"height\":471},{\"@type\":\"BreadcrumbList\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/level-measurement-for-demanding-biorefinery-applications\\\/#breadcrumb\",\"itemListElement\":[{\"@type\":\"ListItem\",\"position\":1,\"name\":\"Home\",\"item\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\"},{\"@type\":\"ListItem\",\"position\":2,\"name\":\"Level measurement for demanding biorefinery applications\"}]},{\"@type\":\"WebSite\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\",\"name\":\"WIKA blog\",\"description\":\"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.\",\"potentialAction\":[{\"@type\":\"SearchAction\",\"target\":{\"@type\":\"EntryPoint\",\"urlTemplate\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/?s={search_term_string}\"},\"query-input\":{\"@type\":\"PropertyValueSpecification\",\"valueRequired\":true,\"valueName\":\"search_term_string\"}}],\"inLanguage\":\"en-GB\"},{\"@type\":\"Person\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/821d6c308cf57dfbadd9200494f82fda\",\"name\":\"Ansgar Baule\",\"image\":{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2025\\\/04\\\/ansgarbaule-120x120.png\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2025\\\/04\\\/ansgarbaule-120x120.png\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2025\\\/04\\\/ansgarbaule-120x120.png\",\"caption\":\"Ansgar Baule\"},\"description\":\"Als Global Market Segment Manager f\u00fcr \u00d6l &amp; Gas\\\/Wasserstoff arbeite ich an der Schnittstelle zwischen den traditionellen Energiesektoren und der aufstrebenden Wasserstoffwirtschaft mit dem Ziel, den \u00dcbergang zu einer nachhaltigeren Energiezukunft mitzugestalten. Dabei greife ich auf meine Erfahrungen aus 27+ Jahren in der \u00d6l- &amp; Gasindustrie zur\u00fcck. Mit dem Schreiben von Blog-Beitr\u00e4gen teile ich gerne mein Fachwissen und die Expertise unseres WIKA-Teams, um Einblicke in die Herausforderungen der Wasserstoff- und Dekarbonisierungs-Prozesse und in innovative Instrumentierungsl\u00f6sungen zu geben.\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/author\\\/bauleansgar\\\/\"}]}<\/script>\n<!-- \/ Yoast SEO plugin. -->","yoast_head_json":{"title":"Level measurement for demanding biorefinery applications - WIKA blog","description":"Level measurement in a biorefinery presents unique challenges. WIKA demonstrates how they can be overcome.","robots":{"index":"index","follow":"follow","max-snippet":"max-snippet:-1","max-image-preview":"max-image-preview:large","max-video-preview":"max-video-preview:-1"},"canonical":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/","og_locale":"en_GB","og_type":"article","og_title":"Level measurement for demanding biorefinery applications - WIKA blog","og_description":"Level measurement in a biorefinery presents unique challenges. WIKA demonstrates how they can be overcome.","og_url":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/","og_site_name":"WIKA blog","og_image":[{"width":838,"height":471,"url":"https:\/\/blog.wika.com\/en\/files\/2025\/07\/beitragsbild_biokraftstoffe_level.jpg","type":"image\/jpeg"}],"author":"Ansgar Baule","twitter_misc":{"Written by":"Ansgar Baule","Estimated reading time":"5 minutes"},"schema":{"@context":"https:\/\/schema.org","@graph":[{"@type":"Article","@id":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/#article","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/"},"author":{"name":"Ansgar Baule","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/821d6c308cf57dfbadd9200494f82fda"},"headline":"Level measurement for demanding biorefinery applications","datePublished":"2025-07-08T05:10:51+00:00","dateModified":"2026-02-23T10:32:08+00:00","mainEntityOfPage":{"@id":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/"},"wordCount":773,"image":{"@id":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2025\/07\/beitragsbild_biokraftstoffe_level.jpg","keywords":["Biofuel","Level","Oil &amp; Gas","Process safety","Renewable energy","Sustainability"],"articleSection":["Applications"],"inLanguage":"en-GB"},{"@type":"WebPage","@id":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/","url":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/","name":"Level measurement for demanding biorefinery applications - WIKA blog","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/#website"},"primaryImageOfPage":{"@id":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/#primaryimage"},"image":{"@id":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2025\/07\/beitragsbild_biokraftstoffe_level.jpg","datePublished":"2025-07-08T05:10:51+00:00","dateModified":"2026-02-23T10:32:08+00:00","author":{"@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/821d6c308cf57dfbadd9200494f82fda"},"description":"Level measurement in a biorefinery presents unique challenges. WIKA demonstrates how they can be overcome.","breadcrumb":{"@id":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/#breadcrumb"},"inLanguage":"en-GB","potentialAction":[{"@type":"ReadAction","target":["https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/"]}]},{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/#primaryimage","url":"https:\/\/blog.wika.com\/en\/files\/2025\/07\/beitragsbild_biokraftstoffe_level.jpg","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2025\/07\/beitragsbild_biokraftstoffe_level.jpg","width":838,"height":471},{"@type":"BreadcrumbList","@id":"https:\/\/blog.wika.com\/en\/applications\/level-measurement-for-demanding-biorefinery-applications\/#breadcrumb","itemListElement":[{"@type":"ListItem","position":1,"name":"Home","item":"https:\/\/blog.wika.com\/en\/"},{"@type":"ListItem","position":2,"name":"Level measurement for demanding biorefinery applications"}]},{"@type":"WebSite","@id":"https:\/\/blog.wika.com\/en\/#website","url":"https:\/\/blog.wika.com\/en\/","name":"WIKA blog","description":"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.","potentialAction":[{"@type":"SearchAction","target":{"@type":"EntryPoint","urlTemplate":"https:\/\/blog.wika.com\/en\/?s={search_term_string}"},"query-input":{"@type":"PropertyValueSpecification","valueRequired":true,"valueName":"search_term_string"}}],"inLanguage":"en-GB"},{"@type":"Person","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/821d6c308cf57dfbadd9200494f82fda","name":"Ansgar Baule","image":{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/files\/2025\/04\/ansgarbaule-120x120.png","url":"https:\/\/blog.wika.com\/en\/files\/2025\/04\/ansgarbaule-120x120.png","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2025\/04\/ansgarbaule-120x120.png","caption":"Ansgar Baule"},"description":"Als Global Market Segment Manager f\u00fcr \u00d6l &amp; Gas\/Wasserstoff arbeite ich an der Schnittstelle zwischen den traditionellen Energiesektoren und der aufstrebenden Wasserstoffwirtschaft mit dem Ziel, den \u00dcbergang zu einer nachhaltigeren Energiezukunft mitzugestalten. Dabei greife ich auf meine Erfahrungen aus 27+ Jahren in der \u00d6l- &amp; Gasindustrie zur\u00fcck. Mit dem Schreiben von Blog-Beitr\u00e4gen teile ich gerne mein Fachwissen und die Expertise unseres WIKA-Teams, um Einblicke in die Herausforderungen der Wasserstoff- und Dekarbonisierungs-Prozesse und in innovative Instrumentierungsl\u00f6sungen zu geben.","url":"https:\/\/blog.wika.com\/en\/author\/bauleansgar\/"}]}},"_links":{"self":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/51941","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/users\/416"}],"replies":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/comments?post=51941"}],"version-history":[{"count":7,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/51941\/revisions"}],"predecessor-version":[{"id":51953,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/51941\/revisions\/51953"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media\/51946"}],"wp:attachment":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media?parent=51941"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/categories?post=51941"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/tags?post=51941"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}