{"id":52510,"date":"2026-08-28T08:02:37","date_gmt":"2026-08-28T06:02:37","guid":{"rendered":"https:\/\/blog.wika.com\/en\/?p=52510"},"modified":"2026-09-25T08:07:55","modified_gmt":"2026-09-25T06:07:55","slug":"traps-in-nuclear-power-plants-more-than-a-standard-component","status":"publish","type":"post","link":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/","title":{"rendered":"Traps in nuclear power plants: More than a standard component"},"content":{"rendered":"<p><strong>The new N-IA TR from WIKA is a passive trap for use in nuclear power plants. Its function is simple. The real challenge lies in meeting nuclear requirements \u2013 from material quality and cleanliness through complete documentation and traceability to qualified production and testing processes. To this end, WIKA has set up a complete production line.<\/strong><\/p>\n<p>The design of the N-IA TR is particularly simplified, featuring a fully welded stainless steel cylinder with several process connections and without moving parts or an active control. Components that are not present cannot fail. This principle makes the trap reliable throughout the entire plant lifetime. Its function is provided solely by the internal geometry. Depending on the version, it collects condensate, separates gases or forms a stable reference column for differential pressure measurement. Thus it is used equally in process, instrumentation and auxiliary systems of nuclear power plants.<\/p>\n<p>A component without moving parts, however, cannot be readjusted. It must meet the specifications starting from the first manufactured part. Therefore, WIKA has set up a complete production line for the N-IA TR that is designed to meet nuclear requirements. After all, while the component itself may be simple, the processes around it are all the more demanding: a quality management system certified per ISO 19443, the highest demands on material quality and cleanliness, complete traceability and documentation. Moreover, all quality-critical and safety-critical manufacturing and testing steps must be carried out by skilled personnel.<\/p>\n<p>&nbsp;<\/p>\n<h2><strong>Material and proofs in accordance with RCC\u2011M<\/strong><\/h2>\n<p>&nbsp;<\/p>\n\n      <div class=\"wp-caption alignright\" style=\"max-width:396px;\"><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/en\/wp-content\/blogs.dir\/18\/files\/2026\/08\/quiring_abscheider-im-kernkraftwerk_n-ia-tr-388x501.png\" alt=\"Der N-IA TR ist ein vollverschwei\u00dfter CrNi-Stahl-Abscheider, der speziell f\u00fcr den Einsatz in Kernkraftwerken entwickelt wurde.\" \/><p class=\"wp-caption-text\">Stainless steel trap, model N-IA TR<\/p><\/div>\n    \n<p>In nuclear technology, reliably manufacturing a component is not sufficient. Every material, every weld seam and every test step must be qualified, documented and traceable at all times. With the N-IA TR, WIKA therefore not only supplies the component but also takes on the complete implementation of these requirements.<\/p>\n<p>The N-IA TR is fully welded and manufactured from stainless steel \u2013 optionally made from 1.4404 or the seawater\u2011resistant material 1.4547. Its design is carried out in accordance with the French design code RCC\u2011M Subsection E, which is the established European standard for small nuclear components. All pressure connections are produced using qualified welding procedures. If desired, WIKA inspects every weld seam 100 percent visually and additionally examines selected seams using dye penetrant testing and X\u2011ray. If this documentation chain were incomplete at a single point, the component would not meet the requirements of nuclear engineering. This applies regardless of whether it was manufactured flawlessly.<\/p>\n<p>WIKA makes sure to consistently align with the specifics of each project. This already starts with material procurement. The materials are sourced in accordance with customer requirements and documented with a 3.1 inspection certificate per EN 10204, including supplier certificates and chemical analysis. Nothing is used in production that cannot be traced back down to the material batch.<\/p>\n<h2>Every nuclear power plant is different<\/h2>\n<p>What the end product is in concrete terms is decided by the respective mounting location. Every nuclear power plant is different. Accordingly, the N-IA TR is not an off\u2011the\u2011shelf product but is designed on a project\u2011specific basis. Number, size and arrangement of the process connections \u2013 at the top, bottom or side; in DN 8 or DN 25 \u2013 depend on the respective mounting location, as do material and internal geometry. This leads to different available variants: condensate traps for steam or hot\u2011water systems, reference traps for differential pressure measurements as well as degassing and drain traps for the controlled drainage of gases and liquids. While the internal geometry determines the respective function, the external design remains deliberately compact.<\/p>\n<p>An internal volume of less than one litre also facilitates regulatory classification. Together with the ability to qualify up to the highest WIKA Safety Class SC1, the N-IA TR covers the entire spectrum of nuclear requirements \u2013 from use in normal operation to safety\u2011relevant function.<\/p>\n<h2>Conclusion: A door opener for worldwide projects in civil nuclear technology<\/h2>\n<p>This very consistent qualification creates the prerequisites for use in demanding nuclear projects worldwide. It makes it possible to meet a wide range of national and project\u2011specific regulatory requirements.<\/p>\n<p>The N-IA TR thus exemplifies WIKA\u2019s role in the field of nuclear power, being not only a component supplier but an engineering partner that takes on the nuclear requirements from project\u2011specific design through manufacturing to complete proof documentation. Furthermore, due to its flexible design, the N-IA TR is also suitable for retrofit projects. It can be integrated into existing nuclear power plants to meet modern measurement requirements and current safety standards.<\/p>\n<p><strong>Note<\/strong><br \/>\nFurther information on WIKA\u2019s measurement solutions for power generation can be found on our\u00a0<a href=\"https:\/\/www.wika.com\/en-en\/power_generation.WIKA\" rel=\"external\" target=\"_blank\">website<\/a>. Do you have any questions? Please feel free to reach out to your\u00a0<a href=\"https:\/\/www.wika.com\/en-en\/contact_form.WIKA\" rel=\"external\" target=\"_blank\">contact person<\/a>\u00a0at any time.<\/p>\n<p>Also read our posts<br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/applications\/level-measurement-in-nuclear-power-plants-reliability-during-accidents\/\">Level measurement in nuclear power plants: Reliability during accidents<\/a><br \/>\n<a href=\"https:\/\/blog.wika.com\/en\/knowhow\/wika-certified-in-accordance-with-iso-19443-for-civil-nuclear-projects\/\">WIKA certified in accordance with ISO 19443 for civil nuclear projects<\/a><br \/>\n<a href=\"https:\/\/blog.wika.com\/de\/wika-insight\/wika-china-von-der-lokalen-fertigung-zum-anerkannten-kompetenzzentrum\/\">WIKA China: From local production to a recognised competence centre<\/a><\/p>\n<p>&nbsp;<\/p>\n","protected":false},"excerpt":{"rendered":"<p>The new N-IA TR from WIKA is a passive trap for use in nuclear power plants. Its function is simple. The real challenge lies in meeting nuclear requirements \u2013 from material quality and cleanliness through complete documentation and traceability to qualified production and testing processes. To this end, WIKA has set up a complete production [&hellip;]<\/p>\n","protected":false},"author":445,"featured_media":52513,"comment_status":"closed","ping_status":"closed","sticky":false,"template":"","format":"standard","meta":{"_acf_changed":false,"footnotes":""},"categories":[232],"tags":[780,721,611],"class_list":["post-52510","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-applications","tag-nuclear-power","tag-process-safety","tag-project"],"acf":[],"yoast_head":"<!-- This site is optimized with the Yoast SEO plugin v27.6 - https:\/\/yoast.com\/product\/yoast-seo-wordpress\/ -->\n<title>Traps in nuclear power plants \u2013 WIKA-Blog<\/title>\n<meta name=\"description\" content=\"As a trap used in nuclear power plants, the WIKA N-IA TR meets all requirements for quality, traceability, and documentation.\" \/>\n<meta name=\"robots\" content=\"index, follow, max-snippet:-1, max-image-preview:large, max-video-preview:-1\" \/>\n<link rel=\"canonical\" href=\"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/\" \/>\n<meta property=\"og:locale\" content=\"en_GB\" \/>\n<meta property=\"og:type\" content=\"article\" \/>\n<meta property=\"og:title\" content=\"Traps in nuclear power plants \u2013 WIKA-Blog\" \/>\n<meta property=\"og:description\" content=\"As a trap used in nuclear power plants, the WIKA N-IA TR meets all requirements for quality, traceability, and documentation.\" \/>\n<meta property=\"og:url\" content=\"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/\" \/>\n<meta property=\"og:site_name\" content=\"WIKA blog\" \/>\n<meta property=\"og:image\" content=\"https:\/\/blog.wika.com\/en\/files\/2026\/08\/lyu_abscheider-im-kernkraftwerk_gettyimages-492691621.jpg\" \/>\n\t<meta property=\"og:image:width\" content=\"1575\" \/>\n\t<meta property=\"og:image:height\" content=\"1181\" \/>\n\t<meta property=\"og:image:type\" content=\"image\/jpeg\" \/>\n<meta name=\"author\" content=\"Joshua Quiring\" \/>\n<meta name=\"twitter:label1\" content=\"Written by\" \/>\n\t<meta name=\"twitter:data1\" content=\"Joshua Quiring\" \/>\n\t<meta name=\"twitter:label2\" content=\"Estimated reading time\" \/>\n\t<meta name=\"twitter:data2\" content=\"5 minutes\" \/>\n<script type=\"application\/ld+json\" class=\"yoast-schema-graph\">{\"@context\":\"https:\\\/\\\/schema.org\",\"@graph\":[{\"@type\":\"Article\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/traps-in-nuclear-power-plants-more-than-a-standard-component\\\/#article\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/traps-in-nuclear-power-plants-more-than-a-standard-component\\\/\"},\"author\":{\"name\":\"Joshua Quiring\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/d6146f3ef3e3f2247b0b82be78eeaf50\"},\"headline\":\"Traps in nuclear power plants: More than a standard component\",\"datePublished\":\"2026-08-28T06:02:37+00:00\",\"dateModified\":\"2026-09-25T06:07:55+00:00\",\"mainEntityOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/traps-in-nuclear-power-plants-more-than-a-standard-component\\\/\"},\"wordCount\":832,\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/traps-in-nuclear-power-plants-more-than-a-standard-component\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2026\\\/08\\\/lyu_abscheider-im-kernkraftwerk_gettyimages-492691621.jpg\",\"keywords\":[\"Nuclear power\",\"Process safety\",\"Project\"],\"articleSection\":[\"Applications\"],\"inLanguage\":\"en-GB\"},{\"@type\":\"WebPage\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/traps-in-nuclear-power-plants-more-than-a-standard-component\\\/\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/traps-in-nuclear-power-plants-more-than-a-standard-component\\\/\",\"name\":\"Traps in nuclear power plants \u2013 WIKA-Blog\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\"},\"primaryImageOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/traps-in-nuclear-power-plants-more-than-a-standard-component\\\/#primaryimage\"},\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/traps-in-nuclear-power-plants-more-than-a-standard-component\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2026\\\/08\\\/lyu_abscheider-im-kernkraftwerk_gettyimages-492691621.jpg\",\"datePublished\":\"2026-08-28T06:02:37+00:00\",\"dateModified\":\"2026-09-25T06:07:55+00:00\",\"author\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/d6146f3ef3e3f2247b0b82be78eeaf50\"},\"description\":\"As a trap used in nuclear power plants, the WIKA N-IA TR meets all requirements for quality, traceability, and documentation.\",\"breadcrumb\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/traps-in-nuclear-power-plants-more-than-a-standard-component\\\/#breadcrumb\"},\"inLanguage\":\"en-GB\",\"potentialAction\":[{\"@type\":\"ReadAction\",\"target\":[\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/traps-in-nuclear-power-plants-more-than-a-standard-component\\\/\"]}]},{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/traps-in-nuclear-power-plants-more-than-a-standard-component\\\/#primaryimage\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2026\\\/08\\\/lyu_abscheider-im-kernkraftwerk_gettyimages-492691621.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2026\\\/08\\\/lyu_abscheider-im-kernkraftwerk_gettyimages-492691621.jpg\",\"width\":1575,\"height\":1181,\"caption\":\"Traps in nuclear power plants: More than a standard component\"},{\"@type\":\"BreadcrumbList\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/applications\\\/traps-in-nuclear-power-plants-more-than-a-standard-component\\\/#breadcrumb\",\"itemListElement\":[{\"@type\":\"ListItem\",\"position\":1,\"name\":\"Home\",\"item\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\"},{\"@type\":\"ListItem\",\"position\":2,\"name\":\"Traps in nuclear power plants: More than a standard component\"}]},{\"@type\":\"WebSite\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\",\"name\":\"WIKA blog\",\"description\":\"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.\",\"potentialAction\":[{\"@type\":\"SearchAction\",\"target\":{\"@type\":\"EntryPoint\",\"urlTemplate\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/?s={search_term_string}\"},\"query-input\":{\"@type\":\"PropertyValueSpecification\",\"valueRequired\":true,\"valueName\":\"search_term_string\"}}],\"inLanguage\":\"en-GB\"},{\"@type\":\"Person\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/d6146f3ef3e3f2247b0b82be78eeaf50\",\"name\":\"Joshua Quiring\",\"image\":{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2026\\\/08\\\/quiringjoshua_wir0705-1377-10er-300dpi-120x120.jpg\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2026\\\/08\\\/quiringjoshua_wir0705-1377-10er-300dpi-120x120.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2026\\\/08\\\/quiringjoshua_wir0705-1377-10er-300dpi-120x120.jpg\",\"caption\":\"Joshua Quiring\"},\"description\":\"Mich begeistert es, Produkte von der ersten Idee \u00fcber die Entwicklung bis hin zum Einsatz in Kernkraftwerken zu begleiten. Dabei fasziniert mich besonders die Herausforderung, die Anforderungen von Kunden, Betreibern und Beh\u00f6rden miteinander zu vereinen. Die Verbindung von Technologie, Sicherheit und langfristiger Verantwortung macht den Kern meiner Arbeit aus. Mein Ziel ist es, L\u00f6sungen zu entwickeln, die h\u00f6chste Anforderungen erf\u00fcllen und zu einem sicheren sowie zuverl\u00e4ssigen Anlagenbetrieb beitragen.\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/author\\\/quiringj\\\/\"}]}<\/script>\n<!-- \/ Yoast SEO plugin. -->","yoast_head_json":{"title":"Traps in nuclear power plants \u2013 WIKA-Blog","description":"As a trap used in nuclear power plants, the WIKA N-IA TR meets all requirements for quality, traceability, and documentation.","robots":{"index":"index","follow":"follow","max-snippet":"max-snippet:-1","max-image-preview":"max-image-preview:large","max-video-preview":"max-video-preview:-1"},"canonical":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/","og_locale":"en_GB","og_type":"article","og_title":"Traps in nuclear power plants \u2013 WIKA-Blog","og_description":"As a trap used in nuclear power plants, the WIKA N-IA TR meets all requirements for quality, traceability, and documentation.","og_url":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/","og_site_name":"WIKA blog","og_image":[{"width":1575,"height":1181,"url":"https:\/\/blog.wika.com\/en\/files\/2026\/08\/lyu_abscheider-im-kernkraftwerk_gettyimages-492691621.jpg","type":"image\/jpeg"}],"author":"Joshua Quiring","twitter_misc":{"Written by":"Joshua Quiring","Estimated reading time":"5 minutes"},"schema":{"@context":"https:\/\/schema.org","@graph":[{"@type":"Article","@id":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/#article","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/"},"author":{"name":"Joshua Quiring","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/d6146f3ef3e3f2247b0b82be78eeaf50"},"headline":"Traps in nuclear power plants: More than a standard component","datePublished":"2026-08-28T06:02:37+00:00","dateModified":"2026-09-25T06:07:55+00:00","mainEntityOfPage":{"@id":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/"},"wordCount":832,"image":{"@id":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2026\/08\/lyu_abscheider-im-kernkraftwerk_gettyimages-492691621.jpg","keywords":["Nuclear power","Process safety","Project"],"articleSection":["Applications"],"inLanguage":"en-GB"},{"@type":"WebPage","@id":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/","url":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/","name":"Traps in nuclear power plants \u2013 WIKA-Blog","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/#website"},"primaryImageOfPage":{"@id":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/#primaryimage"},"image":{"@id":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2026\/08\/lyu_abscheider-im-kernkraftwerk_gettyimages-492691621.jpg","datePublished":"2026-08-28T06:02:37+00:00","dateModified":"2026-09-25T06:07:55+00:00","author":{"@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/d6146f3ef3e3f2247b0b82be78eeaf50"},"description":"As a trap used in nuclear power plants, the WIKA N-IA TR meets all requirements for quality, traceability, and documentation.","breadcrumb":{"@id":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/#breadcrumb"},"inLanguage":"en-GB","potentialAction":[{"@type":"ReadAction","target":["https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/"]}]},{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/#primaryimage","url":"https:\/\/blog.wika.com\/en\/files\/2026\/08\/lyu_abscheider-im-kernkraftwerk_gettyimages-492691621.jpg","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2026\/08\/lyu_abscheider-im-kernkraftwerk_gettyimages-492691621.jpg","width":1575,"height":1181,"caption":"Traps in nuclear power plants: More than a standard component"},{"@type":"BreadcrumbList","@id":"https:\/\/blog.wika.com\/en\/applications\/traps-in-nuclear-power-plants-more-than-a-standard-component\/#breadcrumb","itemListElement":[{"@type":"ListItem","position":1,"name":"Home","item":"https:\/\/blog.wika.com\/en\/"},{"@type":"ListItem","position":2,"name":"Traps in nuclear power plants: More than a standard component"}]},{"@type":"WebSite","@id":"https:\/\/blog.wika.com\/en\/#website","url":"https:\/\/blog.wika.com\/en\/","name":"WIKA blog","description":"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.","potentialAction":[{"@type":"SearchAction","target":{"@type":"EntryPoint","urlTemplate":"https:\/\/blog.wika.com\/en\/?s={search_term_string}"},"query-input":{"@type":"PropertyValueSpecification","valueRequired":true,"valueName":"search_term_string"}}],"inLanguage":"en-GB"},{"@type":"Person","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/d6146f3ef3e3f2247b0b82be78eeaf50","name":"Joshua Quiring","image":{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/files\/2026\/08\/quiringjoshua_wir0705-1377-10er-300dpi-120x120.jpg","url":"https:\/\/blog.wika.com\/en\/files\/2026\/08\/quiringjoshua_wir0705-1377-10er-300dpi-120x120.jpg","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2026\/08\/quiringjoshua_wir0705-1377-10er-300dpi-120x120.jpg","caption":"Joshua Quiring"},"description":"Mich begeistert es, Produkte von der ersten Idee \u00fcber die Entwicklung bis hin zum Einsatz in Kernkraftwerken zu begleiten. Dabei fasziniert mich besonders die Herausforderung, die Anforderungen von Kunden, Betreibern und Beh\u00f6rden miteinander zu vereinen. Die Verbindung von Technologie, Sicherheit und langfristiger Verantwortung macht den Kern meiner Arbeit aus. Mein Ziel ist es, L\u00f6sungen zu entwickeln, die h\u00f6chste Anforderungen erf\u00fcllen und zu einem sicheren sowie zuverl\u00e4ssigen Anlagenbetrieb beitragen.","url":"https:\/\/blog.wika.com\/en\/author\/quiringj\/"}]}},"_links":{"self":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/52510","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/users\/445"}],"replies":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/comments?post=52510"}],"version-history":[{"count":3,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/52510\/revisions"}],"predecessor-version":[{"id":52516,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/52510\/revisions\/52516"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media\/52513"}],"wp:attachment":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media?parent=52510"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/categories?post=52510"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/tags?post=52510"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}