{"id":7928,"date":"2017-08-28T10:50:31","date_gmt":"2017-08-28T08:50:31","guid":{"rendered":"https:\/\/blog.wika.com\/en\/?p=7928"},"modified":"2024-09-19T11:24:56","modified_gmt":"2024-09-19T09:24:56","slug":"mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers","status":"publish","type":"post","link":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/","title":{"rendered":"Mineral-insulated cables \u2013 a core component for the construction of electrical thermometers"},"content":{"rendered":"<p><strong>Mineral-insulated cable, often also abbreviated to MI cable, consists of a metal sheath and ceramic-insulated internal conductors. The ceramic is a metal oxide powder (standard material is MgO) with a purity of &gt; 99.0%, which ensures the insulation of the internal conductors from each other and also the insulation of the conductors from the outer sheath. The construction of an MI cable is similar to ordinary cable, however, it has the special feature of high temperature resistance. By using stainless steels instead of, for example, PVC or Teflon, application temperatures up to approx. 850 \u00b0C (1.4571, 316L, 1.4541) or even up to approx. 1150 \u00b0C (2.4816) are possible.<\/strong><\/p>\n<h2>Design<\/h2>\n<p>The starting point is a long metal tube (typical length approx. 15 m) of the desired sheath material, into which bored ceramic cylinders are inserted. Matching the bores of the ceramic cylinder and the later sheathed cable type, corresponding internal conductors are inserted. For the subsequent construction of resistance thermometers, internal conductors made from copper or nickel are usually used. When constructing thermocouples, the appropriate material pairing must be considered, dependent on the thermocouple type. This overall structure, consisting of outer tube, ceramic cylinders and inner conductors is subsequently compacted by alternately drawing it through carbide or diamond drawing dies and then heating, until the desired diameter is achieved. The compacting of the mineral ceramic to powder ensures a rapid heat transfer between the sheath material and the internal conductors.<\/p>\n\n      <div class=\"wp-caption alignright\" style=\"max-width:396px;\"><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/en\/files\/2017\/06\/keramikzylinder-1-388x225.jpg\" alt=\"Ceramic cylinder\" \/><p class=\"wp-caption-text\">Ceramic cylinder<\/p><\/div>\n    \n<h2>Application<\/h2>\n<p>Since only mineral components are used for insulation, operation is also possible at significantly higher temperatures than would be the case with plastic-insulated cables (e.g. PVC, PTFE). Protected by the metallic sheath material, mineral-insulated cables are also fire-resistant and therefore ideally suited for temperature measurement. The diameter of the MI cable is primarily determined by the requirements of the subsequent technical application.<\/p>\n<h2>Variety<\/h2>\n<p>The smallest diameter of electrical thermometer ever manufactured by WIKA was 0.25 mm. If this diameter is compared with that of conventional cables, the user is offered considerable advantages when using relatively thin dimensions. The combination of outer diameter, sheath material, wall thickness, number, material and arrangement of the internal conductors and also the accuracy class (only with thermocouple wires) leads to a large variety of different mineral-insulated cables.<\/p>\n\n      <div class=\"wp-caption alignright\" style=\"max-width:396px;\"><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/en\/files\/2017\/06\/schliffbild-mantelleitung-388x169.png\" alt=\"Microsection of various sheathed cables\" \/><p class=\"wp-caption-text\">Microsection of various sheathed cables<\/p><\/div>\n    \n<h2>Special feature<\/h2>\n<p>The special feature of MI cable lies in the relative position of the inner conductors to each other as well as to the outer sheath, which are always constant. Even when the cable is bent or twisted, the position within the composite is ensured. The permissible bending radius is three times the diameter. The defined insulation properties, resulting from the exact positioning of the internal conductors, are fundamental when it comes to the construction of explosion-protected thermometers.<\/p>\n\n      <div class=\"wp-caption alignright\" style=\"max-width:396px;\"><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/en\/files\/2017\/06\/aufbau-eines-widerstandsthermometers-388x217.png\" alt=\"Construction of a resistance thermometer\" \/><p class=\"wp-caption-text\">Construction of a resistance thermometer<\/p><\/div>\n    \n<h2>Further processing<\/h2>\n<p>With any further processing of the mineral-insulated cable, particular attention must be paid to the hygroscopic characteristic of the insulating ceramic. If this is not guarded against, the cable immediately absorbs moisture from the environment, which, within a few minutes, reduces the insulation resistance. For this reason, the MI cable should only be stored hermetically-sealed or, if open, in a furnace with a correspondingly high temperature.<\/p>\n<h2>Common standards<\/h2>\n<ul>\n<li>IEC 60751<\/li>\n<li>IEC 60584<\/li>\n<li>ASTM E230<\/li>\n<\/ul>\n<p><strong>Note<br \/>\n<\/strong>Further information on <a href=\"https:\/\/www.wika.com\/en-en\/thermocouples.WIKA\" rel=\"external\" target=\"_blank\">thermocouples<\/a> and <a href=\"https:\/\/www.wika.com\/en-en\/resistance_thermometers.WIKA\" rel=\"external\" target=\"_blank\">resistance thermometers<\/a> can be found on the WIKA website.<strong><br \/>\n<\/strong><\/p>\n<p>Learn more about how a thermocouple and a resistance thermometer work in the following videos:<\/p>\n<div data-fullscreen=\"disabled\" data-mode=\"normal\" data-oembed=\"1\" data-provider=\"youtube\" data-reset-after-played id=\"arve-youtube-9wp9u9wcqq0\" style=\"max-width:900px;\" class=\"arve\">\n<div class=\"arve-inner\">\n<div style=\"aspect-ratio:500\/281\" class=\"arve-embed arve-embed--has-aspect-ratio\">\n<div class=\"arve-ar\" style=\"padding-top:56.200000%\"><\/div>\n<p>\t\t\t<iframe allow=\"accelerometer &apos;none&apos;;autoplay &apos;none&apos;;bluetooth &apos;none&apos;;browsing-topics &apos;none&apos;;camera &apos;none&apos;;clipboard-read &apos;none&apos;;clipboard-write;display-capture &apos;none&apos;;encrypted-media &apos;none&apos;;gamepad &apos;none&apos;;geolocation &apos;none&apos;;gyroscope &apos;none&apos;;hid &apos;none&apos;;identity-credentials-get &apos;none&apos;;idle-detection &apos;none&apos;;keyboard-map &apos;none&apos;;local-fonts;magnetometer &apos;none&apos;;microphone &apos;none&apos;;midi &apos;none&apos;;otp-credentials &apos;none&apos;;payment &apos;none&apos;;picture-in-picture;publickey-credentials-create &apos;none&apos;;publickey-credentials-get &apos;none&apos;;screen-wake-lock &apos;none&apos;;serial &apos;none&apos;;summarizer &apos;none&apos;;sync-xhr;usb &apos;none&apos;;web-share;window-management &apos;none&apos;;xr-spatial-tracking &apos;none&apos;;\" allowfullscreen=\"\" class=\"arve-iframe fitvidsignore\" credentialless data-arve=\"arve-youtube-9wp9u9wcqq0\" data-lenis-prevent=\"\" data-src-no-ap=\"https:\/\/www.youtube-nocookie.com\/embed\/9wp9U9wCqQ0?feature=oembed&amp;iv_load_policy=3&amp;modestbranding=1&amp;rel=0&amp;autohide=1&amp;playsinline=0&amp;autoplay=0&amp;enablejsapi=1\" frameborder=\"0\" height=\"505.8\" loading=\"lazy\" name=\"\" referrerpolicy=\"strict-origin-when-cross-origin\" sandbox=\"allow-scripts allow-same-origin allow-presentation allow-popups allow-popups-to-escape-sandbox\" scrolling=\"no\" src=\"https:\/\/www.youtube-nocookie.com\/embed\/9wp9U9wCqQ0?feature=oembed&#038;iv_load_policy=3&#038;modestbranding=1&#038;rel=0&#038;autohide=1&#038;playsinline=0&#038;autoplay=0&#038;enablejsapi=1\" title=\"Thermocouple basic working principles |  How does a thermocouple work?\" width=\"900\"><\/iframe><\/p><\/div>\n<\/p><\/div>\n<p>\t<script type=\"application\/ld+json\">{\"@context\":\"http:\\\/\\\/schema.org\\\/\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/#arve-youtube-9wp9u9wcqq0\",\"@type\":\"VideoObject\",\"author\":{\"@type\":\"Organization\",\"name\":\"WIKA Group\"},\"embedURL\":\"https:\\\/\\\/www.youtube-nocookie.com\\\/embed\\\/9wp9U9wCqQ0?feature=oembed&iv_load_policy=3&modestbranding=1&rel=0&autohide=1&playsinline=0&autoplay=0&enablejsapi=1\",\"name\":\"Thermocouple basic working principles |  How does a thermocouple work?\",\"thumbnailUrl\":\"https:\\\/\\\/i.ytimg.com\\\/vi\\\/9wp9U9wCqQ0\\\/hqdefault.jpg\",\"uploadDate\":\"2019-05-15T08:33:53Z\",\"description\":\"What is a thermocouple and its working principles? What are the types of thermocouple and how do they work? Up to how many degrees Celsius or Fahrenheit can you use thermocouples? These and other basics are explained in this video.\\n\\n\\u25ac Contents of this video \\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac \\n00:00 - Intro \\n00:04 - How do thermocouples work?\\n00:55 - When is a reference junction compensation necessary when using thermocouples?\\n01:25 - What is a thermoelectric voltage curve and what material pairings are used for it?\\n01:58 - What are the types of thermocouples?\\n\\n#Thermocouple #ThermocoupleWorkingPrinciples #WIKAgroup #ThermocoupleTypes #HowThermocouplesWork \\n\\nThermocouples are made from two wires of different metals, which are in contact with each other at the measuring point. Due to their high vibration resistance, thermocouples that are welded firmly together are used in industrial applications. Thermocouples are temperature sensors that generate a voltage directly dependent on temperature. Compared to resistance thermometers, they are particularly suited for high temperatures up to 1,700 \\u00b0C. \\n\\nThere are a variety of thermocouple types that are suitable for a number of temperature ranges. Their accuracies are defined by the standards IEC 60584-1 and ASTM E230 and can be read in limit value tables. \\n\\n-------------------------------------------------------------------------------\\n\\u00a0\\n\\ud83d\\udd27 A detailed explanation of the \\u201cuse of thermocouples\\u201d can be found in our Technical information IN 00.23, which you can download free of charge from our website: \\n \\n\\ud83c\\udf10 Through our product configurator, which is available for the different types, you can assemble the perfect thermocouple for your application: \\n \\n\\ud83d\\udcf0 Please also read our trade article on \\u201cSpoilt for choice  - Criteria for selecting the most suitable electrical temperature measuring point\\u201d:  \\n \\n\\ud83d\\udcd6 In the following blog post we explain to you mineral-insulated cables, which are important components of electrical thermometers: \\n\\n\\ud83d\\udcfa How a resistance thermometer works is explained in this video: \\n\\n-------------------------------------------------------------------------------\\n\\nFollow us on our social media channels:\\n\\ud83d\\udcfa YouTube: \\n\\ud83c\\udfaf LinkedIn:\"}<\/script><\/p>\n<\/div>\n<div data-fullscreen=\"disabled\" data-mode=\"normal\" data-oembed=\"1\" data-provider=\"youtube\" data-reset-after-played id=\"arve-youtube-hxmytpddn7g\" style=\"max-width:900px;\" class=\"arve\">\n<div class=\"arve-inner\">\n<div style=\"aspect-ratio:500\/281\" class=\"arve-embed arve-embed--has-aspect-ratio\">\n<div class=\"arve-ar\" style=\"padding-top:56.200000%\"><\/div>\n<p>\t\t\t<iframe allow=\"accelerometer &apos;none&apos;;autoplay &apos;none&apos;;bluetooth &apos;none&apos;;browsing-topics &apos;none&apos;;camera &apos;none&apos;;clipboard-read &apos;none&apos;;clipboard-write;display-capture &apos;none&apos;;encrypted-media &apos;none&apos;;gamepad &apos;none&apos;;geolocation &apos;none&apos;;gyroscope &apos;none&apos;;hid &apos;none&apos;;identity-credentials-get &apos;none&apos;;idle-detection &apos;none&apos;;keyboard-map &apos;none&apos;;local-fonts;magnetometer &apos;none&apos;;microphone &apos;none&apos;;midi &apos;none&apos;;otp-credentials &apos;none&apos;;payment &apos;none&apos;;picture-in-picture;publickey-credentials-create &apos;none&apos;;publickey-credentials-get &apos;none&apos;;screen-wake-lock &apos;none&apos;;serial &apos;none&apos;;summarizer &apos;none&apos;;sync-xhr;usb &apos;none&apos;;web-share;window-management &apos;none&apos;;xr-spatial-tracking &apos;none&apos;;\" allowfullscreen=\"\" class=\"arve-iframe fitvidsignore\" credentialless data-arve=\"arve-youtube-hxmytpddn7g\" data-lenis-prevent=\"\" data-src-no-ap=\"https:\/\/www.youtube-nocookie.com\/embed\/HXMytpddn7g?feature=oembed&amp;iv_load_policy=3&amp;modestbranding=1&amp;rel=0&amp;autohide=1&amp;playsinline=0&amp;autoplay=0&amp;enablejsapi=1\" frameborder=\"0\" height=\"505.8\" loading=\"lazy\" name=\"\" referrerpolicy=\"strict-origin-when-cross-origin\" sandbox=\"allow-scripts allow-same-origin allow-presentation allow-popups allow-popups-to-escape-sandbox\" scrolling=\"no\" src=\"https:\/\/www.youtube-nocookie.com\/embed\/HXMytpddn7g?feature=oembed&#038;iv_load_policy=3&#038;modestbranding=1&#038;rel=0&#038;autohide=1&#038;playsinline=0&#038;autoplay=0&#038;enablejsapi=1\" title=\"How does a resistance thermometer work? | Resistance thermometers per IEC 60751\" width=\"900\"><\/iframe><\/p><\/div>\n<\/p><\/div>\n<p>\t<script type=\"application\/ld+json\">{\"@context\":\"http:\\\/\\\/schema.org\\\/\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/#arve-youtube-hxmytpddn7g\",\"@type\":\"VideoObject\",\"author\":{\"@type\":\"Organization\",\"name\":\"WIKA Group\"},\"embedURL\":\"https:\\\/\\\/www.youtube-nocookie.com\\\/embed\\\/HXMytpddn7g?feature=oembed&iv_load_policy=3&modestbranding=1&rel=0&autohide=1&playsinline=0&autoplay=0&enablejsapi=1\",\"name\":\"How does a resistance thermometer work? | Resistance thermometers per IEC 60751\",\"thumbnailUrl\":\"https:\\\/\\\/i.ytimg.com\\\/vi\\\/HXMytpddn7g\\\/hqdefault.jpg\",\"uploadDate\":\"2019-03-08T15:11:46Z\",\"description\":\"What exactly is a resistance thermometer, a Pt100 or a Pt1000 sensor? How do Pt100 and Pt1000 resistance sensors differ? These and other important differences are explained in this video about electrical thermometers.\\n\\n#Temperature #ProcessControl #Thermometer #TemperatureMeasurement #IndustrialAutomation\\n\\n\\u25ac Contents of this video \\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac\\u25ac \\n0:00 Intro \\n0:12 Resistance thermometer working principle\\n0:47 Platinum resistance thermometer range\\n1:21 RTD: accuracy and standard measuring range\\n1:57 Pt100 temperature sensor: an industrial standard\\n2:10 Pt1000 and Pt25: for special cases\\n\\u00a0\\nUsually, two different types of electrical thermometers are used in industrial applications \\u2013 resistance thermometers and thermocouples. How thermocouples work is explained in this video:  With resistance thermometers, the temperature is determined using an ohmic measuring resistor. The \\u201cPt\\u201d in Pt100 stands for the chemical element platinum, the next digit indicates the resistance value of the sensor at zero degrees Celsius. The most frequently used measuring resistor, the Pt100, therefore has an electrical resistance of 100 \\u03a9 (ohms) at 0 \\u00b0C. In special applications, Pt1000 temperature sensors are also used. As the temperature drops or rises, the electrical resistance changes \\u2013 following a defined characteristic curve which is regulated by international standards. The temperature can be determined very precisely on the basis of the measured resistance.\\n\\u00a0\\nAccuracy and measuring ranges of Pt100\\\/Pt1000 temperature probes\\nAs with the traditional dial thermometer (see also our video for correct reading of thermometers:  the resistance thermometer has different accuracy classes. The following applies: The more accurately a resistance thermometer should measure, the more limited its permissible measuring range is. Likewise, you must also consider the type (design) of the measuring resistor.\\nIs a thin-film or wire-wound resistor used? Depending on the measuring resistor selected, there are different temperature measuring ranges based on the IEC 60751 standard. For example, class B wire-wound resistance thermometers have a defined measuring range of -196 \\u00b0C to a maximum of 600 \\u00b0C. If the temperature exceeds or drops below this range, the measured values of the temperature sensors begin to drift so they no longer measure within the defined accuracy and thus the measuring result is falsified. With the current level of technology, for thin-film sensors, this drift is stronger than with wire-wound sensors.\\n\\u00a0\\nFurther information on Pt100 and Pt1000 sensors can be found on our website: \\n\\u00a0\\n\\ud83d\\uded2 With WIKA, you can configure and order the most common resistance thermometers directly in the online shop:  \\n\\n\\ud83c\\udf10 You can find an overview of all resistance thermometers on our website: \\n\\u00a0\\n\\ud83d\\udcd6 Would you like to learn more about resistance thermometers? Then read our blog ( or the technical information on the subject \\u201cOperating limits and accuracies of platinum resistance thermometers per DIN EN IEC 60751\\u201d (\\n\\n-------------------------------------------------------------------------------\\n\\nFollow us on our social media channels:\\n\\ud83d\\udcfa YouTube: \\n\\u2705 LinkedIn:\"}<\/script><\/p>\n<\/div>\n","protected":false},"excerpt":{"rendered":"<p>Mineral-insulated cable, often also abbreviated to MI cable, consists of a metal sheath and ceramic-insulated internal conductors. The ceramic is a metal oxide powder (standard material is MgO) with a purity of &gt; 99.0%, which ensures the insulation of the internal conductors from each other and also the insulation of the conductors from the outer [&hellip;]<\/p>\n","protected":false},"author":92,"featured_media":7935,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"_acf_changed":false,"footnotes":""},"categories":[5],"tags":[254,322,324,323,304],"class_list":["post-7928","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-knowhow","tag-ex-protection","tag-resistance-thermometer","tag-temperature","tag-thermocouple","tag-thermometer"],"acf":[],"yoast_head":"<!-- This site is optimized with the Yoast SEO plugin v27.6 - https:\/\/yoast.com\/product\/yoast-seo-wordpress\/ -->\n<title>Mineral-insulated cables for electrical thermometers - WIKA blog<\/title>\n<meta name=\"description\" content=\"Mineral-insulated cable, often also abbreviated to MI cable, consists of a metal sheath and ceramic-insulated internal conductors.\" \/>\n<meta name=\"robots\" content=\"index, follow, max-snippet:-1, max-image-preview:large, max-video-preview:-1\" \/>\n<link rel=\"canonical\" href=\"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/\" \/>\n<meta property=\"og:locale\" content=\"en_GB\" \/>\n<meta property=\"og:type\" content=\"article\" \/>\n<meta property=\"og:title\" content=\"Mineral-insulated cables for electrical thermometers - WIKA blog\" \/>\n<meta property=\"og:description\" content=\"Mineral-insulated cable, often also abbreviated to MI cable, consists of a metal sheath and ceramic-insulated internal conductors.\" \/>\n<meta property=\"og:url\" content=\"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/\" \/>\n<meta property=\"og:site_name\" content=\"WIKA blog\" \/>\n<meta property=\"og:image\" content=\"https:\/\/blog.wika.com\/en\/files\/2017\/06\/mineralstoffisolierte-leitungen.png\" \/>\n\t<meta property=\"og:image:width\" content=\"837\" \/>\n\t<meta property=\"og:image:height\" content=\"471\" \/>\n\t<meta property=\"og:image:type\" content=\"image\/png\" \/>\n<meta name=\"author\" content=\"Jochen Gries\" \/>\n<meta name=\"twitter:label1\" content=\"Written by\" \/>\n\t<meta name=\"twitter:data1\" content=\"Jochen Gries\" \/>\n\t<meta name=\"twitter:label2\" content=\"Estimated reading time\" \/>\n\t<meta name=\"twitter:data2\" content=\"4 minutes\" \/>\n<script type=\"application\/ld+json\" class=\"yoast-schema-graph\">{\"@context\":\"https:\\\/\\\/schema.org\",\"@graph\":[{\"@type\":\"Article\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/#article\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/\"},\"author\":{\"name\":\"Jochen Gries\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/adfa0a861739af30395ac2bb41943ed1\"},\"headline\":\"Mineral-insulated cables \u2013 a core component for the construction of electrical thermometers\",\"datePublished\":\"2017-08-28T08:50:31+00:00\",\"dateModified\":\"2024-09-19T09:24:56+00:00\",\"mainEntityOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/\"},\"wordCount\":617,\"commentCount\":0,\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2017\\\/06\\\/mineralstoffisolierte-leitungen.png\",\"keywords\":[\"Ex protection\",\"Resistance thermometer\",\"Temperature\",\"Thermocouple\",\"Thermometer\"],\"articleSection\":[\"Know-how\"],\"inLanguage\":\"en-GB\"},{\"@type\":\"WebPage\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/\",\"name\":\"Mineral-insulated cables for electrical thermometers - WIKA blog\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\"},\"primaryImageOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/#primaryimage\"},\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2017\\\/06\\\/mineralstoffisolierte-leitungen.png\",\"datePublished\":\"2017-08-28T08:50:31+00:00\",\"dateModified\":\"2024-09-19T09:24:56+00:00\",\"author\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/adfa0a861739af30395ac2bb41943ed1\"},\"description\":\"Mineral-insulated cable, often also abbreviated to MI cable, consists of a metal sheath and ceramic-insulated internal conductors.\",\"breadcrumb\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/#breadcrumb\"},\"inLanguage\":\"en-GB\",\"potentialAction\":[{\"@type\":\"ReadAction\",\"target\":[\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/\"]}]},{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/#primaryimage\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2017\\\/06\\\/mineralstoffisolierte-leitungen.png\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2017\\\/06\\\/mineralstoffisolierte-leitungen.png\",\"width\":837,\"height\":471,\"caption\":\"Mineral-insulated cables\"},{\"@type\":\"BreadcrumbList\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\\\/#breadcrumb\",\"itemListElement\":[{\"@type\":\"ListItem\",\"position\":1,\"name\":\"Home\",\"item\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\"},{\"@type\":\"ListItem\",\"position\":2,\"name\":\"Mineral-insulated cables \u2013 a core component for the construction of electrical thermometers\"}]},{\"@type\":\"WebSite\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\",\"name\":\"WIKA blog\",\"description\":\"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.\",\"potentialAction\":[{\"@type\":\"SearchAction\",\"target\":{\"@type\":\"EntryPoint\",\"urlTemplate\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/?s={search_term_string}\"},\"query-input\":{\"@type\":\"PropertyValueSpecification\",\"valueRequired\":true,\"valueName\":\"search_term_string\"}}],\"inLanguage\":\"en-GB\"},{\"@type\":\"Person\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/adfa0a861739af30395ac2bb41943ed1\",\"name\":\"Jochen Gries\",\"image\":{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2015\\\/03\\\/default_avatar-140x140.png\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2015\\\/03\\\/default_avatar-140x140.png\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2015\\\/03\\\/default_avatar-140x140.png\",\"caption\":\"Jochen Gries\"},\"description\":\"As a Product Manager of WIKA\u2019s electrical temperature measurement division, I would like to use this blog to inform about our products and technical innovations. Furthermore, there are many interesting problems out of the daily business and possible solution approaches that can be presented in this blog. I look forward to your comments, questions and suggestions.\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/author\\\/pichurj\\\/\"}]}<\/script>\n<!-- \/ Yoast SEO plugin. -->","yoast_head_json":{"title":"Mineral-insulated cables for electrical thermometers - WIKA blog","description":"Mineral-insulated cable, often also abbreviated to MI cable, consists of a metal sheath and ceramic-insulated internal conductors.","robots":{"index":"index","follow":"follow","max-snippet":"max-snippet:-1","max-image-preview":"max-image-preview:large","max-video-preview":"max-video-preview:-1"},"canonical":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/","og_locale":"en_GB","og_type":"article","og_title":"Mineral-insulated cables for electrical thermometers - WIKA blog","og_description":"Mineral-insulated cable, often also abbreviated to MI cable, consists of a metal sheath and ceramic-insulated internal conductors.","og_url":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/","og_site_name":"WIKA blog","og_image":[{"width":837,"height":471,"url":"https:\/\/blog.wika.com\/en\/files\/2017\/06\/mineralstoffisolierte-leitungen.png","type":"image\/png"}],"author":"Jochen Gries","twitter_misc":{"Written by":"Jochen Gries","Estimated reading time":"4 minutes"},"schema":{"@context":"https:\/\/schema.org","@graph":[{"@type":"Article","@id":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/#article","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/"},"author":{"name":"Jochen Gries","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/adfa0a861739af30395ac2bb41943ed1"},"headline":"Mineral-insulated cables \u2013 a core component for the construction of electrical thermometers","datePublished":"2017-08-28T08:50:31+00:00","dateModified":"2024-09-19T09:24:56+00:00","mainEntityOfPage":{"@id":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/"},"wordCount":617,"commentCount":0,"image":{"@id":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2017\/06\/mineralstoffisolierte-leitungen.png","keywords":["Ex protection","Resistance thermometer","Temperature","Thermocouple","Thermometer"],"articleSection":["Know-how"],"inLanguage":"en-GB"},{"@type":"WebPage","@id":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/","url":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/","name":"Mineral-insulated cables for electrical thermometers - WIKA blog","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/#website"},"primaryImageOfPage":{"@id":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/#primaryimage"},"image":{"@id":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2017\/06\/mineralstoffisolierte-leitungen.png","datePublished":"2017-08-28T08:50:31+00:00","dateModified":"2024-09-19T09:24:56+00:00","author":{"@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/adfa0a861739af30395ac2bb41943ed1"},"description":"Mineral-insulated cable, often also abbreviated to MI cable, consists of a metal sheath and ceramic-insulated internal conductors.","breadcrumb":{"@id":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/#breadcrumb"},"inLanguage":"en-GB","potentialAction":[{"@type":"ReadAction","target":["https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/"]}]},{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/#primaryimage","url":"https:\/\/blog.wika.com\/en\/files\/2017\/06\/mineralstoffisolierte-leitungen.png","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2017\/06\/mineralstoffisolierte-leitungen.png","width":837,"height":471,"caption":"Mineral-insulated cables"},{"@type":"BreadcrumbList","@id":"https:\/\/blog.wika.com\/en\/knowhow\/mineral-insulated-cables-a-core-component-for-the-construction-of-electrical-thermometers\/#breadcrumb","itemListElement":[{"@type":"ListItem","position":1,"name":"Home","item":"https:\/\/blog.wika.com\/en\/"},{"@type":"ListItem","position":2,"name":"Mineral-insulated cables \u2013 a core component for the construction of electrical thermometers"}]},{"@type":"WebSite","@id":"https:\/\/blog.wika.com\/en\/#website","url":"https:\/\/blog.wika.com\/en\/","name":"WIKA blog","description":"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.","potentialAction":[{"@type":"SearchAction","target":{"@type":"EntryPoint","urlTemplate":"https:\/\/blog.wika.com\/en\/?s={search_term_string}"},"query-input":{"@type":"PropertyValueSpecification","valueRequired":true,"valueName":"search_term_string"}}],"inLanguage":"en-GB"},{"@type":"Person","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/adfa0a861739af30395ac2bb41943ed1","name":"Jochen Gries","image":{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/files\/2015\/03\/default_avatar-140x140.png","url":"https:\/\/blog.wika.com\/en\/files\/2015\/03\/default_avatar-140x140.png","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2015\/03\/default_avatar-140x140.png","caption":"Jochen Gries"},"description":"As a Product Manager of WIKA\u2019s electrical temperature measurement division, I would like to use this blog to inform about our products and technical innovations. Furthermore, there are many interesting problems out of the daily business and possible solution approaches that can be presented in this blog. I look forward to your comments, questions and suggestions.","url":"https:\/\/blog.wika.com\/en\/author\/pichurj\/"}]}},"_links":{"self":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/7928","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/users\/92"}],"replies":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/comments?post=7928"}],"version-history":[{"count":8,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/7928\/revisions"}],"predecessor-version":[{"id":12360,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/7928\/revisions\/12360"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media\/7935"}],"wp:attachment":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media?parent=7928"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/categories?post=7928"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/tags?post=7928"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}