{"id":9722,"date":"2020-05-26T07:57:59","date_gmt":"2020-05-26T05:57:59","guid":{"rendered":"https:\/\/blog.wika.com\/en\/?p=9722"},"modified":"2024-09-20T08:06:30","modified_gmt":"2024-09-20T06:06:30","slug":"electronic-differential-pressure-measurement-for-level-monitoring","status":"publish","type":"post","link":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/","title":{"rendered":"Electronic differential pressure measurement for level monitoring"},"content":{"rendered":"<p><strong>Differential pressure measurement is widely used as a method for monitoring the level of closed vessels. In many cases, operators use individual instruments with an output signal or on-site display. In contrast, a more precise and fault-immune solution is the measuring arrangement developed by WIKA using two process transmitters in a primary-secondary relationship.<\/strong><\/p>\n<p>Each level monitoring application using differential pressure measurement is based on the following principle: For the level of the contents in the vessel, the differential pressure between the liquid and the gaseous phase is determined. In addition, the hydrostatic pressure, the specific density of the medium and the vessel geometry are included in the calculation. Typical measuring instruments have two adjacent process connections for the pressures P<sub>1<\/sub> and P<sub>2<\/sub>. For level measurement, a capillary has to bridge the pronounced distance between the two measuring points.<\/p>\n\n      <div class=\"wp-caption alignright\" style=\"max-width:396px;\"><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/en\/files\/2020\/05\/elektornische-differenzdruckmessungprozesstransmitter-388x191.jpg\" \/><p class=\"wp-caption-text\">Measurement with two process transmitters as Primary instrument (right) and Secondary instrument. This measuring arrangement for level monitoring can be used flexibly, e.g. for information on the mixing ratio of liquids.<\/p><\/div>\n    \n<h2>Connection via signal cable<\/h2>\n<p>When monitoring the level using electronic differential pressure measurement, on the other hand, both measuring points have one process transmitter each. For example, the WIKA models CPT-2x and IPT-2x are suitable for this. The two transmitters are arranged as Primary instrument and Secondary instrument. They are connected, purely electrically, via a signal cable and are therefore not susceptible to disturbances. The Primary instrument supplies the Secondary instrument with power. The Secondary instrument is parameterised via a serial interface or through the display on the Primary instrument. Finally, communication takes place via an internal bus.<\/p>\n\n      <div class=\"wp-caption alignleft\" style=\"max-width:396px;\"><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/en\/files\/2020\/05\/fuellstandskontrolle_geschlossener_tank-388x301.jpg\" \/><p class=\"wp-caption-text\">Level monitoring in a closed tank<\/p><\/div>\n    \n<h2>Application example<\/h2>\n<p>The figure on the left shows a typical application example for level monitoring with electronic differential pressure measurement on a liquid tank. The Secondary instrument measures the pressure P<sub>1<\/sub>, in this case the gas pressure, and transmits it to the Primary instrument. This detects the pressure P<sub>2<\/sub>, here the pressure in the liquid column at the bottom of the tank. The Primary instrument calculates the differential pressure from P<sub>1<\/sub> and P<sub>2<\/sub>. Using the measured value and taking into account the other parameters mentioned, it determines the volume in the tank as an indication of the level. This value can be output either as an analogue or digital signal to the control room and\/or to the display of the Primary instrument.<\/p>\n<figure><\/figure>\n<h2>Advantages of the measuring arrangement with two process transmitters<\/h2>\n<p>The method for level monitoring described here has several advantages when compared to a conventional method, for example, with a differential pressure transmitter:<\/p>\n<ul>\n<li><strong>Higher accuracy and \u201cturndown\u201d<br \/>\n<\/strong>Process transmitters deliver higher levels of accuracy. In the case of the WIKA models, these are up to 0.05 % of the set span. In addition, there is the possibility of \u201cturndown\u201d, the individual setting of a specific measuring span (this is also possible retrospectively with instruments that are already installed.)<\/p>\n<\/li>\n<li><strong>Minimised temperature effect<br \/>\n<\/strong>Transmission via signal cable with electronic differential pressure measurement minimises the temperature effect. In contrast, the capillaries used in the conventional measuring method are much more susceptible here. This, in turn, can ultimately affect the measuring result.<\/p>\n<\/li>\n<li><strong>Fast commissioning<br \/>\n<\/strong>The electronic measuring arrangement can be commissioned faster. Contrary to a solution with capillaries, it does not require any test run.<\/p>\n<\/li>\n<li><strong>Reduced maintenance effort<br \/>\n<\/strong>The maintenance effort is lower: In the event of a fault, only the process transmitter concerned needs to be replaced. In contrast, with measuring differential pressure with capillaries, the complete measuring arrangement must be replaced.<\/p>\n<\/li>\n<\/ul>\n<p><strong>Note<\/strong><br \/>\nFurther information on the model CPT-2x and IPT-2x process transmitters, which are suitable for electronic differential pressure measurement for level monitoring, is available on the <a href=\"https:\/\/www.wika.com\/en-en\/process_transmitters.WIKA\" rel=\"external\" target=\"_blank\">WIKA website<\/a>.<\/p>\n","protected":false},"excerpt":{"rendered":"<p>Differential pressure measurement is widely used as a method for monitoring the level of closed vessels. In many cases, operators use individual instruments with an output signal or on-site display. In contrast, a more precise and fault-immune solution is the measuring arrangement developed by WIKA using two process transmitters in a primary-secondary relationship. Each level [&hellip;]<\/p>\n","protected":false},"author":95,"featured_media":9727,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"_acf_changed":false,"footnotes":""},"categories":[5],"tags":[294,280,563,192,566,276,367],"class_list":["post-9722","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-knowhow","tag-differential-pressure-transmitter","tag-filling-height","tag-pressure","tag-process-connection","tag-processtransmitter","tag-tank","tag-transmitter"],"acf":[],"yoast_head":"<!-- This site is optimized with the Yoast SEO plugin v27.6 - https:\/\/yoast.com\/product\/yoast-seo-wordpress\/ -->\n<title>Electronic differential pressure measurement for level monitoring<\/title>\n<meta name=\"description\" content=\"The electronic differential pressure measurement for level monitoring with closed tanks offers several advantages over conventional methods.\" \/>\n<meta name=\"robots\" content=\"index, follow, max-snippet:-1, max-image-preview:large, max-video-preview:-1\" \/>\n<link rel=\"canonical\" href=\"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/\" \/>\n<meta property=\"og:locale\" content=\"en_GB\" \/>\n<meta property=\"og:type\" content=\"article\" \/>\n<meta property=\"og:title\" content=\"Electronic differential pressure measurement for level monitoring\" \/>\n<meta property=\"og:description\" content=\"The electronic differential pressure measurement for level monitoring with closed tanks offers several advantages over conventional methods.\" \/>\n<meta property=\"og:url\" content=\"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/\" \/>\n<meta property=\"og:site_name\" content=\"WIKA blog\" \/>\n<meta property=\"og:image\" content=\"https:\/\/blog.wika.com\/en\/files\/2020\/05\/beitragsbild_elekt_diff-20200326112917.jpg\" \/>\n\t<meta property=\"og:image:width\" content=\"838\" \/>\n\t<meta property=\"og:image:height\" content=\"471\" \/>\n\t<meta property=\"og:image:type\" content=\"image\/jpeg\" \/>\n<meta name=\"author\" content=\"Bernd Reichert\" \/>\n<meta name=\"twitter:label1\" content=\"Written by\" \/>\n\t<meta name=\"twitter:data1\" content=\"Bernd Reichert\" \/>\n\t<meta name=\"twitter:label2\" content=\"Estimated reading time\" \/>\n\t<meta name=\"twitter:data2\" content=\"4 minutes\" \/>\n<script type=\"application\/ld+json\" class=\"yoast-schema-graph\">{\"@context\":\"https:\\\/\\\/schema.org\",\"@graph\":[{\"@type\":\"Article\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/electronic-differential-pressure-measurement-for-level-monitoring\\\/#article\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/electronic-differential-pressure-measurement-for-level-monitoring\\\/\"},\"author\":{\"name\":\"Bernd Reichert\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/69a52668d0eaee57551e0ab95f4b8ecd\"},\"headline\":\"Electronic differential pressure measurement for level monitoring\",\"datePublished\":\"2020-05-26T05:57:59+00:00\",\"dateModified\":\"2024-09-20T06:06:30+00:00\",\"mainEntityOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/electronic-differential-pressure-measurement-for-level-monitoring\\\/\"},\"wordCount\":636,\"commentCount\":0,\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/electronic-differential-pressure-measurement-for-level-monitoring\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2020\\\/05\\\/beitragsbild_elekt_diff-20200326112917.jpg\",\"keywords\":[\"Differential pressure transmitter\",\"Filling height\",\"Pressure\",\"Process connection\",\"Processtransmitter\",\"Tank\",\"Transmitter\"],\"articleSection\":[\"Know-how\"],\"inLanguage\":\"en-GB\"},{\"@type\":\"WebPage\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/electronic-differential-pressure-measurement-for-level-monitoring\\\/\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/electronic-differential-pressure-measurement-for-level-monitoring\\\/\",\"name\":\"Electronic differential pressure measurement for level monitoring\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\"},\"primaryImageOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/electronic-differential-pressure-measurement-for-level-monitoring\\\/#primaryimage\"},\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/electronic-differential-pressure-measurement-for-level-monitoring\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2020\\\/05\\\/beitragsbild_elekt_diff-20200326112917.jpg\",\"datePublished\":\"2020-05-26T05:57:59+00:00\",\"dateModified\":\"2024-09-20T06:06:30+00:00\",\"author\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/69a52668d0eaee57551e0ab95f4b8ecd\"},\"description\":\"The electronic differential pressure measurement for level monitoring with closed tanks offers several advantages over conventional methods.\",\"breadcrumb\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/electronic-differential-pressure-measurement-for-level-monitoring\\\/#breadcrumb\"},\"inLanguage\":\"en-GB\",\"potentialAction\":[{\"@type\":\"ReadAction\",\"target\":[\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/electronic-differential-pressure-measurement-for-level-monitoring\\\/\"]}]},{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/electronic-differential-pressure-measurement-for-level-monitoring\\\/#primaryimage\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2020\\\/05\\\/beitragsbild_elekt_diff-20200326112917.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2020\\\/05\\\/beitragsbild_elekt_diff-20200326112917.jpg\",\"width\":838,\"height\":471,\"caption\":\"Level monitoring: Electronic differential pressure measurement\"},{\"@type\":\"BreadcrumbList\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/knowhow\\\/electronic-differential-pressure-measurement-for-level-monitoring\\\/#breadcrumb\",\"itemListElement\":[{\"@type\":\"ListItem\",\"position\":1,\"name\":\"Home\",\"item\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\"},{\"@type\":\"ListItem\",\"position\":2,\"name\":\"Electronic differential pressure measurement for level monitoring\"}]},{\"@type\":\"WebSite\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#website\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/\",\"name\":\"WIKA blog\",\"description\":\"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.\",\"potentialAction\":[{\"@type\":\"SearchAction\",\"target\":{\"@type\":\"EntryPoint\",\"urlTemplate\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/?s={search_term_string}\"},\"query-input\":{\"@type\":\"PropertyValueSpecification\",\"valueRequired\":true,\"valueName\":\"search_term_string\"}}],\"inLanguage\":\"en-GB\"},{\"@type\":\"Person\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/#\\\/schema\\\/person\\\/69a52668d0eaee57551e0ab95f4b8ecd\",\"name\":\"Bernd Reichert\",\"image\":{\"@type\":\"ImageObject\",\"inLanguage\":\"en-GB\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2020\\\/02\\\/reichertbernd-140x140.jpg\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2020\\\/02\\\/reichertbernd-140x140.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/files\\\/2020\\\/02\\\/reichertbernd-140x140.jpg\",\"caption\":\"Bernd Reichert\"},\"description\":\"From 1997 to 2010 I was occupied by WIKA in the departments central marketing as a product manager and in the IT as an application specialist and project manager. Since 2010 I've been responsible for the process transmitters and I am happy to share my experiences with you here in this blog.\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/en\\\/author\\\/reicheb\\\/\"}]}<\/script>\n<!-- \/ Yoast SEO plugin. -->","yoast_head_json":{"title":"Electronic differential pressure measurement for level monitoring","description":"The electronic differential pressure measurement for level monitoring with closed tanks offers several advantages over conventional methods.","robots":{"index":"index","follow":"follow","max-snippet":"max-snippet:-1","max-image-preview":"max-image-preview:large","max-video-preview":"max-video-preview:-1"},"canonical":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/","og_locale":"en_GB","og_type":"article","og_title":"Electronic differential pressure measurement for level monitoring","og_description":"The electronic differential pressure measurement for level monitoring with closed tanks offers several advantages over conventional methods.","og_url":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/","og_site_name":"WIKA blog","og_image":[{"width":838,"height":471,"url":"https:\/\/blog.wika.com\/en\/files\/2020\/05\/beitragsbild_elekt_diff-20200326112917.jpg","type":"image\/jpeg"}],"author":"Bernd Reichert","twitter_misc":{"Written by":"Bernd Reichert","Estimated reading time":"4 minutes"},"schema":{"@context":"https:\/\/schema.org","@graph":[{"@type":"Article","@id":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/#article","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/"},"author":{"name":"Bernd Reichert","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/69a52668d0eaee57551e0ab95f4b8ecd"},"headline":"Electronic differential pressure measurement for level monitoring","datePublished":"2020-05-26T05:57:59+00:00","dateModified":"2024-09-20T06:06:30+00:00","mainEntityOfPage":{"@id":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/"},"wordCount":636,"commentCount":0,"image":{"@id":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2020\/05\/beitragsbild_elekt_diff-20200326112917.jpg","keywords":["Differential pressure transmitter","Filling height","Pressure","Process connection","Processtransmitter","Tank","Transmitter"],"articleSection":["Know-how"],"inLanguage":"en-GB"},{"@type":"WebPage","@id":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/","url":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/","name":"Electronic differential pressure measurement for level monitoring","isPartOf":{"@id":"https:\/\/blog.wika.com\/en\/#website"},"primaryImageOfPage":{"@id":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/#primaryimage"},"image":{"@id":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/en\/files\/2020\/05\/beitragsbild_elekt_diff-20200326112917.jpg","datePublished":"2020-05-26T05:57:59+00:00","dateModified":"2024-09-20T06:06:30+00:00","author":{"@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/69a52668d0eaee57551e0ab95f4b8ecd"},"description":"The electronic differential pressure measurement for level monitoring with closed tanks offers several advantages over conventional methods.","breadcrumb":{"@id":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/#breadcrumb"},"inLanguage":"en-GB","potentialAction":[{"@type":"ReadAction","target":["https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/"]}]},{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/#primaryimage","url":"https:\/\/blog.wika.com\/en\/files\/2020\/05\/beitragsbild_elekt_diff-20200326112917.jpg","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2020\/05\/beitragsbild_elekt_diff-20200326112917.jpg","width":838,"height":471,"caption":"Level monitoring: Electronic differential pressure measurement"},{"@type":"BreadcrumbList","@id":"https:\/\/blog.wika.com\/en\/knowhow\/electronic-differential-pressure-measurement-for-level-monitoring\/#breadcrumb","itemListElement":[{"@type":"ListItem","position":1,"name":"Home","item":"https:\/\/blog.wika.com\/en\/"},{"@type":"ListItem","position":2,"name":"Electronic differential pressure measurement for level monitoring"}]},{"@type":"WebSite","@id":"https:\/\/blog.wika.com\/en\/#website","url":"https:\/\/blog.wika.com\/en\/","name":"WIKA blog","description":"Our blog offers many interesting articles on pressure, temperature, level, force, flow measurement calibration technology and provides insights into the WIKA Group.","potentialAction":[{"@type":"SearchAction","target":{"@type":"EntryPoint","urlTemplate":"https:\/\/blog.wika.com\/en\/?s={search_term_string}"},"query-input":{"@type":"PropertyValueSpecification","valueRequired":true,"valueName":"search_term_string"}}],"inLanguage":"en-GB"},{"@type":"Person","@id":"https:\/\/blog.wika.com\/en\/#\/schema\/person\/69a52668d0eaee57551e0ab95f4b8ecd","name":"Bernd Reichert","image":{"@type":"ImageObject","inLanguage":"en-GB","@id":"https:\/\/blog.wika.com\/en\/files\/2020\/02\/reichertbernd-140x140.jpg","url":"https:\/\/blog.wika.com\/en\/files\/2020\/02\/reichertbernd-140x140.jpg","contentUrl":"https:\/\/blog.wika.com\/en\/files\/2020\/02\/reichertbernd-140x140.jpg","caption":"Bernd Reichert"},"description":"From 1997 to 2010 I was occupied by WIKA in the departments central marketing as a product manager and in the IT as an application specialist and project manager. Since 2010 I've been responsible for the process transmitters and I am happy to share my experiences with you here in this blog.","url":"https:\/\/blog.wika.com\/en\/author\/reicheb\/"}]}},"_links":{"self":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/9722","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/users\/95"}],"replies":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/comments?post=9722"}],"version-history":[{"count":8,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/9722\/revisions"}],"predecessor-version":[{"id":13301,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/posts\/9722\/revisions\/13301"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media\/9727"}],"wp:attachment":[{"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/media?parent=9722"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/categories?post=9722"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blog.wika.com\/en\/wp-json\/wp\/v2\/tags?post=9722"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}