In space- and price-critical applications, the ceramic pressure sensor offers a compact and cost-effective solution for implementing pressure measurement which is embedded in the customer’s application. However, there are some details to consider when integrating the ceramic cell.
For example, each sensor must be measured and adjusted (see: “Integration of a pressure sensor element – error compensation of signal for zero point and span”). Furthermore, some details must also be considered in the mechanical integration of a ceramic sensor. A seal is made either axially or radially by means of an O-ring, which must develop its sealing effect via a set clamping force. This clamping force must be evenly distributed over the circumference of the sensor during the axial sealing and must not be too large, so that a distortion of the sensor and thus a faulty measurement is avoided. Clamping the sensor between solid bodies, i.e. without any sealing gap, must be avoided in all cases.
Note
WIKA will gladly support you with installation instructions for the model SCT-1 ceramic sensor and adjustment of the interfaces on both sides. For any questions and detailed application advice on pressure transmitters and sensors from WIKA, simply consult your contact person.
See also our articles
Accuracy of pressure sensors – what ”precisely” does this mean?
Which are the available configuration levels for pressure sensors?
Integration of a pressure sensor element – error compensation of signal for zero point and span
Sensor integration – notes on mechanics and EMC