Length measuring instruments, as test instruments, fall under the risk determination of ISO 9001. As a result of increasing safety requirements, the importance of calibration in connection with this is greater. In the past, a good-bad test was often sufficient - as it …
Know-how
What role do valves play in plant safety?
Daniele Maniero | Know-howThe reliability of a valve is essential for the safety of the entire plant. Almost all pressure measuring instruments work in conjunction with a valve or a combination of valves. The choice of a high-quality valve is not only essential to ensure the accuracy of the …
3 1/2- vs. 4-digit digital indicator – What is a 1/2 digit?
Anna Zeitler | Know-howBesides 3- and 4-digit digital indicators, there are also 3 1/2-digit indicators available in the market. But what is a 1/2 digit? A full digit can indicate all numbers from “0” to “9”. A 1/2 digit, in contrast, can only display a “1”, a number …
Are there any FDA-approved measuring instruments?
Jochen Gries | Know-howDoes the FDA issue its own approvals for systems or devices and therefore also issue approvals for measuring devices? Find out more in the following blog post. There are always uncertainties with this topic, which is why I'd like to shed more light on the question in …
Ex protection – The difference between the Zone and Division model
Jens Bargon | Know-how“The product is suitable for use in Zone 1, as well as for use in Class 1, Div 1.” This statement is heard or read again and again in the descriptions for products for use in hazardous areas. But what is the difference between Zone 1 and Class 1, Div 1? Let's …