The strain sensor in practical application

strain sensor F9302

Drill two holes and cut the threads, prepare the surface, place the strain sensor and tighten both screws to the specified torque, then set the zero point and now the strain measurement can start. If only it were that easy! Of course, the procedure described for …

Read more

Load pins: Definition and application areas

three load pins made of stainless steel

A load pin provides the connection between force-transmitting machine elements and also allows the simultaneous measurement of the force acting on the sensor. The load pins are fixed in the axial direction as well as against rotation. A small gap of about one fifth of …

Read more