The calibration of ultra-high pressures is a challenge. This is because conventional test instruments are only designed for pressures up to 1,000 bar. In many applications, however, sensors work with several times this value, for example in the automotive industry. If …
Calibration software
Five points you should know about software validation
Christian Elbert | Know-howValidation of calibration software - as required by ISO 17025, for example - is a topic that people don't like to talk about. Often there is uncertainty about the following: Which software actually must be validated? If so, who should look after it? Which requirements …