Millions of cubic metres of liquids or gases flow through the pipes of industrial processes every day. In order to be able to transport, control and monitor these correctly, the flow rate must be calculated beforehand. The flow rate, also called volume flow, is a …
Calorimetric
Economical monitoring of flows using a calorimetric flow switch
Oleg Greber | FlowAnyone who has dealt with the topic of flow measurement will know that a corresponding measuring instrument costs several thousand euros. If, however, the flow in a pipeline is to be monitored, a flow switch based on the calorimetric measuring principle is a good, …
How does a calorimetric flow switch work?
Oleg Greber | FlowIf the presence of flow in a piping system must be monitored, a calorimetric flow switch – also known as a flow monitor – is often used. But how does a calorimetric flow switch actually work? The following blog post explains this in greater detail. Calorimetric …