Whoever exports measuring instruments or other technical goods to Russia and many of its neighbouring countries, has to go through the certification process of the “Eurasian Conformity” (EAC). An EAC approval is comparable with CE conformity. It is issued for each …
Pressure gauge
Against overheating: Differential pressure gauges as flow monitors
| Manuel Schwestka | Know-howDifferential pressure gauges are not only suitable for the typical applications such as monitoring and control of filters or pumps. They can take on the function of a flow monitor, for example, in heat transfer oil plants. They thus control the volume flow of the …
DirectDrive pressure gauges – features and application areas
| Sandra Broßler | PressureDirectDrive pressure gauges differ in structure and function from standard pressure gauges. Thus they feature special characteristics that qualify them for specific application areas. In DirectDrive pressure gauges, special pressure elements are fitted, which …
Fittings for pressure gauges: mitigating the effects of dynamic load cycles
| Manuel Schwestka | Know-howIn several processes, pressure gauges are temporarily subjected to heavy loading. Dynamic load cycles, for example, can permanently damage the measuring instrument. This can be prevented by mounting the appropriate Fittings. Dynamic load cycles often result from …
Certification for fire-protection applications
| Fabian Lotter | ApplicationsThe word certification is derived from joining together two Latin words, “certe” (meaning certain) and “facere” (to make). Certification describes the common practice with which the fulfilment and compliance with certain standards or requirements should be …