• Pressure
  • Facebook
  • Twitter
  • XING
  • LinkedIn
  • Send Page URL

Pressure

TA Luft now follows ISO 15848-1 for fugitive emissions

01/23/2023 | Pratik R. Vishwakarma | Know-how
The TA Luft has been revised in the area of fugitive emissions

TA Luft has been revised. For the prevention of fugitive emissions, the new version of the German directive now follows the international standard ISO 15848-1. Correspondingly, tests in accordance with TA Luft follow the same test parameters as those in the ISO …

Read more

Flushing rings in diaphragm seal systems have several advantages

12/22/2022 | Tobias Hench | Know-how
Flushing ring in a diaphragm seal system for the process industry

The extension of a flanged diaphragm seal system using a flushing ring brings significant advantages. Among other things, it enables easy cleaning and, in addition, on-site calibration of the measuring location. Diaphragm seal systems are used in processes with …

Read more

Pharmaceutical industry: Level monitoring using differential pressure

11/23/2022 | Jing Lyu | Applications
The DPT-EL measuring system also enables level monitoring in the pharmaceutical industry

In many processes in the pharmaceutical industry, reliable level monitoring is indispensable. Numerous solutions are available for this task. For level control in the preparation of culture media, for example, a manufacturer of antibiotics has opted for WIKA's …

Read more

Pesticide production with backup pressure measurement

09/13/2022 | Jing Lyu | Applications
Plant protection production with redundant pressure measurement

The high requirements placed on pesticides and their production are also reflected in the pressure measurement in the process. A WIKA customer has therefore supplemented the electronic instrumentation for pressure monitoring with a mechanical backup. For this …

Read more

Lasting accuracy for diaphragm seal systems for vacuum process

05/20/2022 | Jing Lyu | Applications
Diaphragm seal system in the vacuum process

A diaphragm seal system in a vacuum process must master a major challenge – it must deliver a reliable measuring result, even when the pressure drops and the temperature rises at the same time. The example of a chemical company producing phthalic anhydride (PA) shows …

Read more
Welcome to the WIKA blog

In our English-language blog you can expect many interesting articles on pressure, temperature, level, force and flow measurement, and also on the subject of calibration technology. Furthermore, there are various insights into the world of the WIKA group of companies – seen from different angles.

Most-read articles
  • Difference between gauge pressure and absolute pressure measurement
  • Pt100 in 2-, 3- or 4-wire connection?
  • Bourdon tube pressure gauge – operating principle
Accuracy Calibration Ex protection Hydrostatic International Pressure Pressure gauge Pressure sensor Pressure switch Safety Social commitment Standards/approvals/directives Subsidiary Temperature Thermometer
News subscription
The WIKA news subscription informs you, free of charge, by e-mail whenever there is a new blog article. Simply define what subjects interest you and you'll be kept up-to-date! Subscribe

© 2023 WIKA Alexander Wiegand SE & Co. KG

  • Privacy policy
  • Legal notice