TA Luft has been revised. For the prevention of fugitive emissions, the new version of the German directive now follows the international standard ISO 15848-1. Correspondingly, tests in accordance with TA Luft follow the same test parameters as those in the ISO …
Standards/approvals/directives
WIKA certified in accordance with ISO 19443 for civil nuclear projects
| Martin Schnatz | Know-howThe civil use of nuclear power is a significant market. In order to better position itself globally as a solution partner in this segment, WIKA has therefore had itself certified in accordance with the new quality management standard, ISO 19443:2018, for civil nuclear …
Repeal of EC79/2009 for hydrogen-powered vehicles: Impact on pressure sensors
| Christian Wirl | Know-howComponents in a hydrogen-powered vehicle must have an application-specific safety approval, for which the European Union issued regulation EC79/2009. Although this regulation expired in July 2022, it has not lost its relevance - manufacturers and users will continue to …
Not the same: temperature range and temperature limit
| Michèle Beyer | Know-howTemperature range and temperature limit for pressure sensors – is there a difference? My intuitive answer would be: Yes! The first term describes a section and the second its border. On second glance, however, I have to conclude that both words ultimately express the …
WIKA develops pressure sensor for hydrogen-powered vehicles
| Christian Wirl | ApplicationsDue to customers‘ demand for greater safety, eco friendliness, performance and efficiency, manufacturers of mobile working machines, trucks and buses are increasingly interested in hydrogen as a fuel source. In hydrogen-powered vehicles, the gas in the H 2 storage …