Does the FDA issue its own approvals for systems or devices and therefore also issue approvals for measuring devices? Find out more in the following blog post. There are always uncertainties with this topic, which is why I'd like to shed more light on the question in …
Standards/approvals/directives
DIN 3852-E or DIN EN ISO 1179-2?
Sabine Mai | Know-howThe DIN 3852-E pressure connection thread standard has been invalid since 2012. The standard that has been valid since then for pipe threads (e.g. for G ¼ A) is DIN EN ISO 1179-2: “Connections for general use and fluid power - Ports and stud ends with ISO 228-1 …
Drinking water suitability of measuring instruments
Torsten Püschel | ApplicationsIn connection with the drinking water suitability of measuring instruments, the terms Drinking Water Directive, 4MS List, UBA Positive List, Evaluation Criteria for Metallic Substances are increasingly appearing. This article should shed some light on the suitability …
The technical passport – the ID card for a product in the Commonwealth of Independent States (CIS)
Oleg Greber | Know-howSimilar to an identity card, all technical products and equipment used in one of the CIS countries (Commonwealth of Independent States: Armenia, Azerbaijan, Belarus, Kazakhstan, Kyrgyzstan, Moldova, Russia, Tajikistan, Turkmenistan, Ukraine and Uzbekistan) have a …
The metrological certificate – Measuring equipment approval in the Eurasian Economic Zone
Oleg Greber | Know-howIn addition to the EAC certificate, when importing measuring instruments into the Eurasian Economic Zone (members 2017: Russia, Belarus, Kazakhstan, Armenia, Kyrgyzstan) and into the other member states of the CIS (Commonwealth of Independent States: Armenia, …