A submersible pressure transmitter or level probe is a hydrostatic pressure sensor, specifically developed for the purpose of level measurement. Submersible pressure transmitters are level sensors with special characteristics and specific technical features, which …
Submersible pressure transmitter
Hydrostatic level measurement in closed geometries – calculation of the filling height
Enrico Bossart | LevelIn a previous blog post, I explained the calculation of the filling height in open geometries and vessels . Unlike open vessels, the calculation of level in closed geometries, such as gas-tight tanks or pressurised vessels, requires a compensation of the pressure of …
Hydrostatic level measurement in open geometries and vessels – calculation of the filling height
Enrico Bossart | LevelIn my last blog post, I introduced the way in which hydrostatic level measurement works . The hydrostatic pressure is used to determine the level through the measurement of the liquid column and is directly proportional to the filling height, as well as to the density …
What is meant by hydrostatic level measurement or hydrostatic pressure?
Enrico Bossart | LevelHydrostatic pressure sensors are gaining in popularity within continuous level measurement through their simple application, quick installation and commissioning. However, how does hydrostatic level measurement work, what is meant by hydrostatic pressure and how can I …
Definition of the IP68 rating in theory and practice
Michèle Beyer | GeneralUnfortunately, we are asked too rarely regarding the specification of the IP68 rating for our pressure sensors and submersible pressure transmitters, i.e. how deep such an instrument may be submersed. However, this is not only a very meaningful question but also a …