{"id":10107,"date":"2018-10-04T11:31:30","date_gmt":"2018-10-04T16:31:30","guid":{"rendered":"https:\/\/blog.wika.com\/us\/\/?p=10107"},"modified":"2023-08-23T05:27:25","modified_gmt":"2023-08-23T10:27:25","slug":"strain-sensor-force-measurement","status":"publish","type":"post","link":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/","title":{"rendered":"The Strain Sensor in Practical Application"},"content":{"rendered":"<p><strong>Drill two holes and cut the threads, prepare the surface, place the strain\u00a0sensor and tighten both screws to the specified moment, and then set the zero point. Now the strain measurement can start.<\/strong><\/p>\n<p>If only it were that easy! Of course, the procedure described for force measurement with strain\u00a0sensors works: The strains acting are measured following screw-mounting. Whether the measurement at the selected location makes sense, however, is another question. In some applications, such as the supports of a silo, the selection of the measuring point is, of course, easy. In other applications, such as impact crushers, the determination of the measuring point is immediately more difficult.<\/p>\n<h2>Strain Sensor: A short introduction<\/h2>\n<p>First, to summarize, a short explanation of the term: Strain\u00a0sensors, also referred to as strain\u00a0transducers, are a special form of force sensors. Since they are screwed to the application from the outside, they are easy and quick to mount but do not directly measure force flow; strain sensors measure indirectly. Nevertheless, high accuracies can also be achieved.<\/p>\n<p>These force measuring instruments are used when deformations (due to external forces) must be detected on existing (mostly solid) elements. As already described, the sensor is attached to the component, adjusted accordingly, and then starts to measure. The strain is transferred by frictional connection from the solid element to the strain transducer. The applications for these sensors are diverse, with two examples presented in more detail below.<\/p>\n<h2>Practical Example 1: Silo weighing with strain sensors<\/h2>\n<div class=\"wp-caption alignright\"><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/files\/2018\/09\/linde-tank-388x517.jpg\" alt=\"A strain sensor on the foot of a tank as a weighing system\" \/><\/p>\n<p class=\"wp-caption-text\">A strain sensor on the foot of a tank as a weighing system<\/p>\n<\/div>\n<p>Silo weighing systems are typically used to determine the amount of material that is to be emptied into a truck. Often it is also important to know how much material is stored in a silo at any given time. If such weighing systems are planned from the start of the design of the silo, the weight of the contents can be determined with a very high level of accuracy. For this purpose, shear beams and bending beams can be provided in the feet of the silo.<\/p>\n<p>But what if the silo or tank is already standing, and the weighing or level system must be installed afterwards? An upgrade to bending or shear beams for force measurement can then quickly become very expensive \u2013 even impossible.<\/p>\n<p>Strain\u00a0sensors can be retrofitted to silos or tanks. The measuring instruments are simply screwed to the supports, since strain sensors \u2013 as described \u2013 are designed for applications in which deformation by external forces acting on an existing component is to be measured. If one knows the deformation of the columns, it is easy to estimate the level of the silo.<\/p>\n<h2>\nPractical Example 2: Use of strain\u00a0sensors in impact crushers<\/h2>\n<p>Another example of the use of strain\u00a0sensors is in impact crushers. Impact crushers are <a href=\"https:\/\/blog.wika.com\/us\/\/applications\/wika-mobile-working-machines\/\">mobile working machines<\/a> used to crush material, such as stones. These are broken by &#8220;impact crushing&#8221; into smaller and smaller parts. As a result, stress spikes occur, which in turn deform the material of the container or machine. The resulting strains can be detected using the strain sensor. If the strain becomes too great \u2013 for example, if a stone gets caught in the spindle \u2013 the system can be automatically switched off.<\/p>\n<p>Again, the impact crusher does not need to be redesigned; the strain sensor can simply be screwed onto the right place, and it will subsequently detect the occurring stresses. In most cases, the location where the strain\u00a0sensor is best placed is determined by FE calculation (so that the strain is within the specified limits).<\/p>\n<p>The finite element method (FEM) splits solid bodies into a large number of small subdivisions (a finite number of elements that are not infinitely small) for the investigation of strength and deformation. Their behavior individually is easier to calculate than that of the entire, complex body. The basis for the calculations is the solution of multiple differential equations.<\/p>\n<h2>Conclusion<\/h2>\n<p>In summary, if one installs measuring instruments from the beginning, there are measurement techniques that are\u00a0more exact than the strain sensor, which only measures indirectly and not directly in the force flow. However, if the system already exists, the strain transducer is a cost-effective alternative that can still deliver reliable measured values. In the application itself, the\u00a0sensor is quickly integrated and is suitable for both static and dynamic tasks. Furthermore, the\u00a0sensors have a high shock and vibration resistance and good long-term stability. The output signal can be supplied as 4-20 mA, 0-10 V, CAN, or CANopen.<\/p>\n<p><strong>Note<\/strong><br \/>\nGo to the WIKA USA website for information on our universal, versatile <a href=\"https:\/\/www.wika.com\/en-us\/f9302.WIKA\" rel=\"external\" target=\"_blank\">Model F9302 strain\u00a0sensor<\/a>,\u00a0<a href=\"https:\/\/www.wika.com\/en-us\/f3831.WIKA\" target=\"_blank\" rel=\"external noopener noreferrer\">shear beam Model F3831<\/a>, and <a href=\"https:\/\/www.wika.com\/en-us\/f3833.WIKA\" rel=\"external\" target=\"_blank\">bending beam Model F3833<\/a>.<\/p>\n<p>[contact-form-7 id=&#8221;14552&#8243; title=&#8221;Blog Contact Form&#8221;]<\/p>\n","protected":false},"excerpt":{"rendered":"<p>Drill two holes and cut the threads, prepare the surface, place the strain\u00a0sensor and tighten both screws to the specified moment, and then set the zero point. Now the strain measurement can start. If only it were that easy! Of course, the procedure described for force measurement with strain\u00a0sensors works: The strains acting are measured [&hellip;]<\/p>\n","protected":false},"author":349,"featured_media":10120,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"_acf_changed":false,"footnotes":""},"categories":[673],"tags":[704,581],"class_list":["post-10107","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-force-products","tag-force-measurement","tag-mobile-working-machines"],"acf":[],"yoast_head":"<!-- This site is optimized with the Yoast SEO plugin v27.6 - https:\/\/yoast.com\/product\/yoast-seo-wordpress\/ -->\n<title>Strain Sensor for Force Measurement in Practical Applications<\/title>\n<meta name=\"description\" content=\"A strain sensor is an accurate, cost-effective force measurement device that is easily installed on silo supports, impact crushers, etc. to sense deformations. Although more-accurate force sensors exist, a strain sensor \u2013 also called strain transducer \u2013 is a good solutions for existing systems.\" \/>\n<meta name=\"robots\" content=\"index, follow, max-snippet:-1, max-image-preview:large, max-video-preview:-1\" \/>\n<link rel=\"canonical\" href=\"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/\" \/>\n<meta property=\"og:locale\" content=\"en_US\" \/>\n<meta property=\"og:type\" content=\"article\" \/>\n<meta property=\"og:title\" content=\"Strain Sensor for Force Measurement in Practical Applications\" \/>\n<meta property=\"og:description\" content=\"A strain sensor is an accurate, cost-effective force measurement device that is easily installed on silo supports, impact crushers, etc. to sense deformations. Although more-accurate force sensors exist, a strain sensor \u2013 also called strain transducer \u2013 is a good solutions for existing systems.\" \/>\n<meta property=\"og:url\" content=\"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/\" \/>\n<meta property=\"og:site_name\" content=\"WIKA blog\" \/>\n<meta property=\"og:image\" content=\"https:\/\/blog.wika.com\/us\/files\/2018\/10\/pic_pr_f9302_de_de.jpg\" \/>\n\t<meta property=\"og:image:width\" content=\"837\" \/>\n\t<meta property=\"og:image:height\" content=\"471\" \/>\n\t<meta property=\"og:image:type\" content=\"image\/jpeg\" \/>\n<meta name=\"author\" content=\"Chaz Marsinick\" \/>\n<meta name=\"twitter:label1\" content=\"Written by\" \/>\n\t<meta name=\"twitter:data1\" content=\"Chaz Marsinick\" \/>\n\t<meta name=\"twitter:label2\" content=\"Est. reading time\" \/>\n\t<meta name=\"twitter:data2\" content=\"4 minutes\" \/>\n<script type=\"application\/ld+json\" class=\"yoast-schema-graph\">{\"@context\":\"https:\\\/\\\/schema.org\",\"@graph\":[{\"@type\":\"Article\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/#article\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/\"},\"author\":{\"name\":\"Chaz Marsinick\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/#\\\/schema\\\/person\\\/441378e487a3c070e3c606613c6e8ed9\"},\"headline\":\"The Strain Sensor in Practical Application\",\"datePublished\":\"2018-10-04T16:31:30+00:00\",\"dateModified\":\"2023-08-23T10:27:25+00:00\",\"mainEntityOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/\"},\"wordCount\":790,\"commentCount\":0,\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2018\\\/10\\\/pic_pr_f9302_de_de.jpg\",\"keywords\":[\"force measurement\",\"Mobile Working Machines\"],\"articleSection\":[\"Force\"],\"inLanguage\":\"en-US\",\"potentialAction\":[{\"@type\":\"CommentAction\",\"name\":\"Comment\",\"target\":[\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/#respond\"]}]},{\"@type\":\"WebPage\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/\",\"name\":\"Strain Sensor for Force Measurement in Practical Applications\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/#website\"},\"primaryImageOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/#primaryimage\"},\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2018\\\/10\\\/pic_pr_f9302_de_de.jpg\",\"datePublished\":\"2018-10-04T16:31:30+00:00\",\"dateModified\":\"2023-08-23T10:27:25+00:00\",\"author\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/#\\\/schema\\\/person\\\/441378e487a3c070e3c606613c6e8ed9\"},\"description\":\"A strain sensor is an accurate, cost-effective force measurement device that is easily installed on silo supports, impact crushers, etc. to sense deformations. Although more-accurate force sensors exist, a strain sensor \u2013 also called strain transducer \u2013 is a good solutions for existing systems.\",\"breadcrumb\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/#breadcrumb\"},\"inLanguage\":\"en-US\",\"potentialAction\":[{\"@type\":\"ReadAction\",\"target\":[\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/\"]}]},{\"@type\":\"ImageObject\",\"inLanguage\":\"en-US\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/#primaryimage\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2018\\\/10\\\/pic_pr_f9302_de_de.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2018\\\/10\\\/pic_pr_f9302_de_de.jpg\",\"width\":837,\"height\":471,\"caption\":\"A strain sensor on the foot of a tank as a weighing system\"},{\"@type\":\"BreadcrumbList\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/force-products\\\/strain-sensor-force-measurement\\\/#breadcrumb\",\"itemListElement\":[{\"@type\":\"ListItem\",\"position\":1,\"name\":\"Home\",\"item\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/\"},{\"@type\":\"ListItem\",\"position\":2,\"name\":\"The Strain Sensor in Practical Application\"}]},{\"@type\":\"WebSite\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/#website\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/\",\"name\":\"WIKA blog\",\"description\":\"Our blog offers many interesting articles on pressure, temperature, level, flow measurement calibration technology and provides insights into the WIKA Group.\",\"potentialAction\":[{\"@type\":\"SearchAction\",\"target\":{\"@type\":\"EntryPoint\",\"urlTemplate\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/?s={search_term_string}\"},\"query-input\":{\"@type\":\"PropertyValueSpecification\",\"valueRequired\":true,\"valueName\":\"search_term_string\"}}],\"inLanguage\":\"en-US\"},{\"@type\":\"Person\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/#\\\/schema\\\/person\\\/441378e487a3c070e3c606613c6e8ed9\",\"name\":\"Chaz Marsinick\",\"image\":{\"@type\":\"ImageObject\",\"inLanguage\":\"en-US\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2024\\\/02\\\/chaz_marsinick-2-120x120.jpg\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2024\\\/02\\\/chaz_marsinick-2-120x120.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2024\\\/02\\\/chaz_marsinick-2-120x120.jpg\",\"caption\":\"Chaz Marsinick\"},\"url\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/author\\\/chazmarsinick\\\/\"}]}<\/script>\n<!-- \/ Yoast SEO plugin. -->","yoast_head_json":{"title":"Strain Sensor for Force Measurement in Practical Applications","description":"A strain sensor is an accurate, cost-effective force measurement device that is easily installed on silo supports, impact crushers, etc. to sense deformations. Although more-accurate force sensors exist, a strain sensor \u2013 also called strain transducer \u2013 is a good solutions for existing systems.","robots":{"index":"index","follow":"follow","max-snippet":"max-snippet:-1","max-image-preview":"max-image-preview:large","max-video-preview":"max-video-preview:-1"},"canonical":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/","og_locale":"en_US","og_type":"article","og_title":"Strain Sensor for Force Measurement in Practical Applications","og_description":"A strain sensor is an accurate, cost-effective force measurement device that is easily installed on silo supports, impact crushers, etc. to sense deformations. Although more-accurate force sensors exist, a strain sensor \u2013 also called strain transducer \u2013 is a good solutions for existing systems.","og_url":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/","og_site_name":"WIKA blog","og_image":[{"width":837,"height":471,"url":"https:\/\/blog.wika.com\/us\/files\/2018\/10\/pic_pr_f9302_de_de.jpg","type":"image\/jpeg"}],"author":"Chaz Marsinick","twitter_misc":{"Written by":"Chaz Marsinick","Est. reading time":"4 minutes"},"schema":{"@context":"https:\/\/schema.org","@graph":[{"@type":"Article","@id":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/#article","isPartOf":{"@id":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/"},"author":{"name":"Chaz Marsinick","@id":"https:\/\/blog.wika.com\/us\/#\/schema\/person\/441378e487a3c070e3c606613c6e8ed9"},"headline":"The Strain Sensor in Practical Application","datePublished":"2018-10-04T16:31:30+00:00","dateModified":"2023-08-23T10:27:25+00:00","mainEntityOfPage":{"@id":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/"},"wordCount":790,"commentCount":0,"image":{"@id":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/us\/files\/2018\/10\/pic_pr_f9302_de_de.jpg","keywords":["force measurement","Mobile Working Machines"],"articleSection":["Force"],"inLanguage":"en-US","potentialAction":[{"@type":"CommentAction","name":"Comment","target":["https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/#respond"]}]},{"@type":"WebPage","@id":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/","url":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/","name":"Strain Sensor for Force Measurement in Practical Applications","isPartOf":{"@id":"https:\/\/blog.wika.com\/us\/#website"},"primaryImageOfPage":{"@id":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/#primaryimage"},"image":{"@id":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/us\/files\/2018\/10\/pic_pr_f9302_de_de.jpg","datePublished":"2018-10-04T16:31:30+00:00","dateModified":"2023-08-23T10:27:25+00:00","author":{"@id":"https:\/\/blog.wika.com\/us\/#\/schema\/person\/441378e487a3c070e3c606613c6e8ed9"},"description":"A strain sensor is an accurate, cost-effective force measurement device that is easily installed on silo supports, impact crushers, etc. to sense deformations. Although more-accurate force sensors exist, a strain sensor \u2013 also called strain transducer \u2013 is a good solutions for existing systems.","breadcrumb":{"@id":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/#breadcrumb"},"inLanguage":"en-US","potentialAction":[{"@type":"ReadAction","target":["https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/"]}]},{"@type":"ImageObject","inLanguage":"en-US","@id":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/#primaryimage","url":"https:\/\/blog.wika.com\/us\/files\/2018\/10\/pic_pr_f9302_de_de.jpg","contentUrl":"https:\/\/blog.wika.com\/us\/files\/2018\/10\/pic_pr_f9302_de_de.jpg","width":837,"height":471,"caption":"A strain sensor on the foot of a tank as a weighing system"},{"@type":"BreadcrumbList","@id":"https:\/\/blog.wika.com\/us\/products\/force-products\/strain-sensor-force-measurement\/#breadcrumb","itemListElement":[{"@type":"ListItem","position":1,"name":"Home","item":"https:\/\/blog.wika.com\/us\/"},{"@type":"ListItem","position":2,"name":"The Strain Sensor in Practical Application"}]},{"@type":"WebSite","@id":"https:\/\/blog.wika.com\/us\/#website","url":"https:\/\/blog.wika.com\/us\/","name":"WIKA blog","description":"Our blog offers many interesting articles on pressure, temperature, level, flow measurement calibration technology and provides insights into the WIKA Group.","potentialAction":[{"@type":"SearchAction","target":{"@type":"EntryPoint","urlTemplate":"https:\/\/blog.wika.com\/us\/?s={search_term_string}"},"query-input":{"@type":"PropertyValueSpecification","valueRequired":true,"valueName":"search_term_string"}}],"inLanguage":"en-US"},{"@type":"Person","@id":"https:\/\/blog.wika.com\/us\/#\/schema\/person\/441378e487a3c070e3c606613c6e8ed9","name":"Chaz Marsinick","image":{"@type":"ImageObject","inLanguage":"en-US","@id":"https:\/\/blog.wika.com\/us\/files\/2024\/02\/chaz_marsinick-2-120x120.jpg","url":"https:\/\/blog.wika.com\/us\/files\/2024\/02\/chaz_marsinick-2-120x120.jpg","contentUrl":"https:\/\/blog.wika.com\/us\/files\/2024\/02\/chaz_marsinick-2-120x120.jpg","caption":"Chaz Marsinick"},"url":"https:\/\/blog.wika.com\/us\/author\/chazmarsinick\/"}]}},"_links":{"self":[{"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/posts\/10107","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/users\/349"}],"replies":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/comments?post=10107"}],"version-history":[{"count":11,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/posts\/10107\/revisions"}],"predecessor-version":[{"id":16633,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/posts\/10107\/revisions\/16633"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/media\/10120"}],"wp:attachment":[{"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/media?parent=10107"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/categories?post=10107"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/tags?post=10107"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}