{"id":10164,"date":"2018-10-16T10:28:19","date_gmt":"2018-10-16T15:28:19","guid":{"rendered":"https:\/\/blog.wika.com\/us\/\/?p=10164"},"modified":"2023-06-14T14:55:59","modified_gmt":"2023-06-14T19:55:59","slug":"magnetic-float-switch-robust-design","status":"publish","type":"post","link":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/","title":{"rendered":"WIKA\u2019s Magnetic Float Switch Offers Robust Design, Customizable Level Measurement for Mobile Working Machines"},"content":{"rendered":"<p><strong>Correct fluid levels ensure proper and safe operation in mobile working machines. The reliability and space-saving design of WIKA\u2019s miniature magnetic float switches mean they can be used for almost all applications where fluid levels need to be monitored, from fertilizer tanks to engine coolant reservoirs. In addition, WIKA partners with customers to offer personalized solutions for level measurement.<\/strong><\/p>\n<p>WIKA\u2019s horizontal miniature magnetic float switch is simple, compact, and very effective for monitoring fluid levels and as an indicator of maximum\/minimum fluid levels in mobile machines. Just 98.5 mm to 134.5 mm (3.9 to 5.3 inches) in length, this device is ideal for applications where access to the top of the tank or available space is limited. It is particularly well suited for applications such as engine coolant units, hydraulic reservoirs, and agricultural chemical tanks.<\/p>\n<h2>How Does a Magnetic Float Switch Work?<\/h2>\n\n      <div class=\"wp-caption alignright\" style=\"max-width:396px;\"><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/us\/\/files\/2018\/10\/hls-m-diagram-388x204.png\" alt=\"Diagram of a WIKA Model HLS-M Magnetic Float Switch\" \/><p class=\"wp-caption-text\">The float of an HLS-M magnetic float switch is mounted on a hinged lever and travels with the level of the liquid. A built-in permanent magnet triggers a reed switch when the switch point is reached.<\/p><\/div>\n    \n<p>Magnetic float switches are one of the most reliable, low-maintenance tools for level monitoring. In this type of level instrumentation, a float \u2013 attached to a supported, swiveling lever \u2013 rests on the fluid\u2019s surface. A permanent magnet is integrated into the lever, which moves up or down as the fluid level rises or falls. When the magnet in the lever reaches a pre-determined point, it actuates a magnetic reed contact that, in turn, closes (the standard operation) or opens a circuit \u2013 thereby triggering an alarm or another signal.<\/p>\n<p>Since the switching function relies on the interaction between two permanent magnets, the operation is contact-free, meaning there\u2019s no wear and tear. Furthermore, the switching function does not need a power supply.<\/p>\n<p>Magnetic float switches work best when the media is not overly contaminated, does not have coarse particulates, and does not tend to crystallize. Any of these conditions can result in buildup on the float, which will hinder its movement and, therefore, impair the accuracy of the switch.<\/p>\n<h2>Advantages of WIKA\u2019s Magnetic Float Switch<\/h2>\n<p>Designed to be mounted horizontally, WIKA\u2019s <a href=\"https:\/\/www.wika.com\/en-us\/hls_m.WIKA\" rel=\"external\" target=\"_blank\">HLS-M miniature magnetic float switches<\/a> are compact and cost-effective tools for monitoring fluid levels in mobile working machines. The float itself is only 25 mm (1 inch) long in the plastic versions and 47 mm (1.85 inches) in the stainless-steel versions, making the HLS-M series ideal for small tanks, reservoirs, and any other vessels where space is an issue. As indicators of minimum and maximum fluid levels in tanks, the magnetic float switches are routinely used as dry-run and overflow protection.<\/p>\n<p>The HLS-M comes in different materials to suit media type and conditions. The two models of plastic (polypropylene) switches work well between \u221210\u00b0C and 80\u00b0C (14\u00b0F to 176\u00b0F) and can withstand up to 1 bar of pressure, while the three stainless-steel versions are designed for temperatures between \u221240\u00b0C and 120\u00b0C (\u221240\u00b0F to 248\u00b0F) and pressure up to 5 bar. All five have ingress protection IP65 and are certified ISO 9001 and ISO 14001.<\/p>\n<p>To make installation easier, the two models can be installed from the inside, and three from the outside.<span>\u00a0 <\/span>To optimize operations, you can choose from a variety of electrical and process connections. Custom cable assemblies are also available. The switching function is set for a rising level, and in standard use the contact is open. However, the switch can be configured as normally closed simply by rotating it 180 degrees. Thanks to its simple design and quality materials, there are minimal costs associated with mounting, commissioning, operating, and maintaining the HLS-M series.<\/p>\n<table style=\"width: 836px\">\n<tbody>\n<tr style=\"height: 10px\">\n<td style=\"width: 167px;height: 10px\">\n<p><strong>Float switch model<\/strong><\/p>\n<\/td>\n<td style=\"width: 212px;height: 10px\">\n<p><strong>Material<\/strong><\/p>\n<\/td>\n<td style=\"width: 234px;height: 10px\">\n<p><strong>Installation<\/strong><\/p>\n<\/td>\n<td style=\"width: 417px;height: 10px\">\n<p><strong>Electrical connection<\/strong><\/p>\n<\/td>\n<td style=\"width: 305px;height: 10px\">\n<p><strong>Length <\/strong>(not including cable)<\/p>\n<\/td>\n<\/tr>\n<tr style=\"height: 10px\">\n<td style=\"width: 167px;height: 10px\">\n<p>HLS-M11<\/p>\n<\/td>\n<td style=\"width: 212px;height: 10px\">\n<p>Plastic (polypropylene)<\/p>\n<\/td>\n<td style=\"width: 234px;height: 10px\">\n<p>From inside<\/p>\n<\/td>\n<td style=\"width: 417px;height: 10px\">\n<p>Cable<\/p>\n<\/td>\n<td style=\"width: 305px;height: 10px\">\n<p>98.5mm \/ 3.88 in.<\/p>\n<\/td>\n<\/tr>\n<tr style=\"height: 10px\">\n<td style=\"width: 167px;height: 10px\">\n<p>HLS-M12<\/p>\n<\/td>\n<td style=\"width: 212px;height: 10px\">\n<p>Plastic (polypropylene)<\/p>\n<\/td>\n<td style=\"width: 234px;height: 10px\">\n<p>From outside<\/p>\n<\/td>\n<td style=\"width: 417px;height: 10px\">\n<p>Cable<\/p>\n<\/td>\n<td style=\"width: 305px;height: 10px\">\n<p>98.5mm \/ 3.88 in.<\/p>\n<\/td>\n<\/tr>\n<tr style=\"height: 10px\">\n<td style=\"width: 167px;height: 10px\">\n<p>HLS-M21<\/p>\n<\/td>\n<td style=\"width: 212px;height: 10px\">\n<p>Stainless steel 1.4301<\/p>\n<\/td>\n<td style=\"width: 234px;height: 10px\">\n<p>From inside<\/p>\n<\/td>\n<td style=\"width: 417px;height: 10px\">\n<p>Cable<\/p>\n<\/td>\n<td style=\"width: 305px;height: 10px\">\n<p>97mm \/ 3.82 in.<\/p>\n<\/td>\n<\/tr>\n<tr style=\"height: 10px\">\n<td style=\"width: 167px;height: 10px\">\n<p>HLS-M22<\/p>\n<\/td>\n<td style=\"width: 212px;height: 10px\">\n<p>Stainless steel 1.4301<\/p>\n<\/td>\n<td style=\"width: 234px;height: 10px\">\n<p>From outside<\/p>\n<\/td>\n<td style=\"width: 417px;height: 10px\">\n<p>Cable<\/p>\n<\/td>\n<td style=\"width: 305px;height: 10px\">\n<p>94mm \/ 3.7 in.<\/p>\n<\/td>\n<\/tr>\n<tr style=\"height: 10px\">\n<td style=\"width: 167px;height: 10px\">\n<p>HLS-M23<\/p>\n<\/td>\n<td style=\"width: 212px;height: 10px\">\n<p>Stainless steel 1.4301<\/p>\n<\/td>\n<td style=\"width: 234px;height: 10px\">\n<p>From outside<\/p>\n<\/td>\n<td style=\"width: 417px;height: 10px\">\n<p>Connector<\/p>\n<\/td>\n<td style=\"width: 305px;height: 10px\">\n<p>134.5mm \/ 5.3 in.<\/p>\n<\/td>\n<\/tr>\n<\/tbody>\n<\/table>\n<p>A reliable magnetic float switch with a small footprint, such as WIKA\u2019s HLS-M series, can make a big difference in the operation, maintenance, and associated costs of your applications in mobile working machinery. <a href=\"https:\/\/www.wika.com\/en-us\/contact.WIKA\" rel=\"external\" target=\"_blank\">Contact us today<\/a> to learn more about these switches, their customizable options, and other innovative level measurement solutions from WIKA USA.<\/p>\n<p><a href=\"http:\/\/bit.ly\/2A01py7\" rel=\"external\" target=\"_blank\">Click here<\/a> to learn more about WIKA product applications in mobile working machines.\u00a0<\/p>\n<figure><img decoding=\"async\" src=\"https:\/\/blog.wika.com\/us\/\/files\/2018\/03\/shutterstock_123529891-388x258.jpg\" alt=\"Wheel loader excavator with backhoe unloading clay\" class=\"alignnone\" \/><\/figure>\n<p><span style=\"font-family: Calibri;font-size: 11pt\">[contact-form-7 id=&#8221;14552&#8243; title=&#8221;Blog Contact Form&#8221;]<\/span><\/p>\n","protected":false},"excerpt":{"rendered":"<p>Correct fluid levels ensure proper and safe operation in mobile working machines. The reliability and space-saving design of WIKA\u2019s miniature magnetic float switches mean they can be used for almost all applications where fluid levels need to be monitored, from fertilizer tanks to engine coolant reservoirs. In addition, WIKA partners with customers to offer personalized [&hellip;]<\/p>\n","protected":false},"author":188,"featured_media":10168,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"_acf_changed":false,"footnotes":""},"categories":[223],"tags":[436,799,876,581],"class_list":["post-10164","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-level-products","tag-level-measurement","tag-level-monitoring","tag-miniature","tag-mobile-working-machines"],"acf":[],"yoast_head":"<!-- This site is optimized with the Yoast SEO plugin v27.6 - https:\/\/yoast.com\/product\/yoast-seo-wordpress\/ -->\n<title>WIKA\u2019s Miniature Magnetic Float Switch for Mobile Machine Applications<\/title>\n<meta name=\"description\" content=\"Model HLS-M, a high-quality magnetic float switch, is designed for reliable monitoring of fluid levels practically anywhere in mobile working machines. Because it is compact and the switching operation does not require power, the HLS-M is ideal for space-constrained applications.\" \/>\n<meta name=\"robots\" content=\"index, follow, max-snippet:-1, max-image-preview:large, max-video-preview:-1\" \/>\n<link rel=\"canonical\" href=\"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/\" \/>\n<meta property=\"og:locale\" content=\"en_US\" \/>\n<meta property=\"og:type\" content=\"article\" \/>\n<meta property=\"og:title\" content=\"WIKA\u2019s Miniature Magnetic Float Switch for Mobile Machine Applications\" \/>\n<meta property=\"og:description\" content=\"Model HLS-M, a high-quality magnetic float switch, is designed for reliable monitoring of fluid levels practically anywhere in mobile working machines. Because it is compact and the switching operation does not require power, the HLS-M is ideal for space-constrained applications.\" \/>\n<meta property=\"og:url\" content=\"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/\" \/>\n<meta property=\"og:site_name\" content=\"WIKA blog\" \/>\n<meta property=\"og:image\" content=\"https:\/\/blog.wika.com\/us\/files\/2018\/10\/hls-m_resized.jpeg\" \/>\n\t<meta property=\"og:image:width\" content=\"838\" \/>\n\t<meta property=\"og:image:height\" content=\"471\" \/>\n\t<meta property=\"og:image:type\" content=\"image\/jpeg\" \/>\n<meta name=\"author\" content=\"Jeff Placek\" \/>\n<meta name=\"twitter:label1\" content=\"Written by\" \/>\n\t<meta name=\"twitter:data1\" content=\"Jeff Placek\" \/>\n\t<meta name=\"twitter:label2\" content=\"Est. reading time\" \/>\n\t<meta name=\"twitter:data2\" content=\"4 minutes\" \/>\n<script type=\"application\/ld+json\" class=\"yoast-schema-graph\">{\"@context\":\"https:\\\/\\\/schema.org\",\"@graph\":[{\"@type\":\"Article\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/#article\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/\"},\"author\":{\"name\":\"Jeff Placek\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/#\\\/schema\\\/person\\\/8d2cbbabfb4ec43b285229fb14d04066\"},\"headline\":\"WIKA\u2019s Magnetic Float Switch Offers Robust Design, Customizable Level Measurement for Mobile Working Machines\",\"datePublished\":\"2018-10-16T15:28:19+00:00\",\"dateModified\":\"2023-06-14T19:55:59+00:00\",\"mainEntityOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/\"},\"wordCount\":743,\"commentCount\":0,\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2018\\\/10\\\/hls-m_resized.jpeg\",\"keywords\":[\"Level Measurement\",\"level monitoring\",\"miniature\",\"Mobile Working Machines\"],\"articleSection\":[\"Level\"],\"inLanguage\":\"en-US\",\"potentialAction\":[{\"@type\":\"CommentAction\",\"name\":\"Comment\",\"target\":[\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/#respond\"]}]},{\"@type\":\"WebPage\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/\",\"name\":\"WIKA\u2019s Miniature Magnetic Float Switch for Mobile Machine Applications\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/#website\"},\"primaryImageOfPage\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/#primaryimage\"},\"image\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/#primaryimage\"},\"thumbnailUrl\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2018\\\/10\\\/hls-m_resized.jpeg\",\"datePublished\":\"2018-10-16T15:28:19+00:00\",\"dateModified\":\"2023-06-14T19:55:59+00:00\",\"author\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/#\\\/schema\\\/person\\\/8d2cbbabfb4ec43b285229fb14d04066\"},\"description\":\"Model HLS-M, a high-quality magnetic float switch, is designed for reliable monitoring of fluid levels practically anywhere in mobile working machines. Because it is compact and the switching operation does not require power, the HLS-M is ideal for space-constrained applications.\",\"breadcrumb\":{\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/#breadcrumb\"},\"inLanguage\":\"en-US\",\"potentialAction\":[{\"@type\":\"ReadAction\",\"target\":[\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/\"]}]},{\"@type\":\"ImageObject\",\"inLanguage\":\"en-US\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/#primaryimage\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2018\\\/10\\\/hls-m_resized.jpeg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2018\\\/10\\\/hls-m_resized.jpeg\",\"width\":838,\"height\":471,\"caption\":\"Model HLS-M is designed for reliable monitoring of fluid levels practically anywhere in mobile working machines. Because it is compact and the switching operation does not require power, the HLS-M is ideal for space-constrained applications.\"},{\"@type\":\"BreadcrumbList\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/products\\\/level-products\\\/magnetic-float-switch-robust-design\\\/#breadcrumb\",\"itemListElement\":[{\"@type\":\"ListItem\",\"position\":1,\"name\":\"Home\",\"item\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/\"},{\"@type\":\"ListItem\",\"position\":2,\"name\":\"WIKA\u2019s Magnetic Float Switch Offers Robust Design, Customizable Level Measurement for Mobile Working Machines\"}]},{\"@type\":\"WebSite\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/#website\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/\",\"name\":\"WIKA blog\",\"description\":\"Our blog offers many interesting articles on pressure, temperature, level, flow measurement calibration technology and provides insights into the WIKA Group.\",\"potentialAction\":[{\"@type\":\"SearchAction\",\"target\":{\"@type\":\"EntryPoint\",\"urlTemplate\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/?s={search_term_string}\"},\"query-input\":{\"@type\":\"PropertyValueSpecification\",\"valueRequired\":true,\"valueName\":\"search_term_string\"}}],\"inLanguage\":\"en-US\"},{\"@type\":\"Person\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/#\\\/schema\\\/person\\\/8d2cbbabfb4ec43b285229fb14d04066\",\"name\":\"Jeff Placek\",\"image\":{\"@type\":\"ImageObject\",\"inLanguage\":\"en-US\",\"@id\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2023\\\/08\\\/jeffplacek2022_blog-120x120.jpg\",\"url\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2023\\\/08\\\/jeffplacek2022_blog-120x120.jpg\",\"contentUrl\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/files\\\/2023\\\/08\\\/jeffplacek2022_blog-120x120.jpg\",\"caption\":\"Jeff Placek\"},\"url\":\"https:\\\/\\\/blog.wika.com\\\/us\\\/author\\\/jplacek\\\/\"}]}<\/script>\n<!-- \/ Yoast SEO plugin. -->","yoast_head_json":{"title":"WIKA\u2019s Miniature Magnetic Float Switch for Mobile Machine Applications","description":"Model HLS-M, a high-quality magnetic float switch, is designed for reliable monitoring of fluid levels practically anywhere in mobile working machines. Because it is compact and the switching operation does not require power, the HLS-M is ideal for space-constrained applications.","robots":{"index":"index","follow":"follow","max-snippet":"max-snippet:-1","max-image-preview":"max-image-preview:large","max-video-preview":"max-video-preview:-1"},"canonical":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/","og_locale":"en_US","og_type":"article","og_title":"WIKA\u2019s Miniature Magnetic Float Switch for Mobile Machine Applications","og_description":"Model HLS-M, a high-quality magnetic float switch, is designed for reliable monitoring of fluid levels practically anywhere in mobile working machines. Because it is compact and the switching operation does not require power, the HLS-M is ideal for space-constrained applications.","og_url":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/","og_site_name":"WIKA blog","og_image":[{"width":838,"height":471,"url":"https:\/\/blog.wika.com\/us\/files\/2018\/10\/hls-m_resized.jpeg","type":"image\/jpeg"}],"author":"Jeff Placek","twitter_misc":{"Written by":"Jeff Placek","Est. reading time":"4 minutes"},"schema":{"@context":"https:\/\/schema.org","@graph":[{"@type":"Article","@id":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/#article","isPartOf":{"@id":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/"},"author":{"name":"Jeff Placek","@id":"https:\/\/blog.wika.com\/us\/#\/schema\/person\/8d2cbbabfb4ec43b285229fb14d04066"},"headline":"WIKA\u2019s Magnetic Float Switch Offers Robust Design, Customizable Level Measurement for Mobile Working Machines","datePublished":"2018-10-16T15:28:19+00:00","dateModified":"2023-06-14T19:55:59+00:00","mainEntityOfPage":{"@id":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/"},"wordCount":743,"commentCount":0,"image":{"@id":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/us\/files\/2018\/10\/hls-m_resized.jpeg","keywords":["Level Measurement","level monitoring","miniature","Mobile Working Machines"],"articleSection":["Level"],"inLanguage":"en-US","potentialAction":[{"@type":"CommentAction","name":"Comment","target":["https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/#respond"]}]},{"@type":"WebPage","@id":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/","url":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/","name":"WIKA\u2019s Miniature Magnetic Float Switch for Mobile Machine Applications","isPartOf":{"@id":"https:\/\/blog.wika.com\/us\/#website"},"primaryImageOfPage":{"@id":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/#primaryimage"},"image":{"@id":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.wika.com\/us\/files\/2018\/10\/hls-m_resized.jpeg","datePublished":"2018-10-16T15:28:19+00:00","dateModified":"2023-06-14T19:55:59+00:00","author":{"@id":"https:\/\/blog.wika.com\/us\/#\/schema\/person\/8d2cbbabfb4ec43b285229fb14d04066"},"description":"Model HLS-M, a high-quality magnetic float switch, is designed for reliable monitoring of fluid levels practically anywhere in mobile working machines. Because it is compact and the switching operation does not require power, the HLS-M is ideal for space-constrained applications.","breadcrumb":{"@id":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/#breadcrumb"},"inLanguage":"en-US","potentialAction":[{"@type":"ReadAction","target":["https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/"]}]},{"@type":"ImageObject","inLanguage":"en-US","@id":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/#primaryimage","url":"https:\/\/blog.wika.com\/us\/files\/2018\/10\/hls-m_resized.jpeg","contentUrl":"https:\/\/blog.wika.com\/us\/files\/2018\/10\/hls-m_resized.jpeg","width":838,"height":471,"caption":"Model HLS-M is designed for reliable monitoring of fluid levels practically anywhere in mobile working machines. Because it is compact and the switching operation does not require power, the HLS-M is ideal for space-constrained applications."},{"@type":"BreadcrumbList","@id":"https:\/\/blog.wika.com\/us\/products\/level-products\/magnetic-float-switch-robust-design\/#breadcrumb","itemListElement":[{"@type":"ListItem","position":1,"name":"Home","item":"https:\/\/blog.wika.com\/us\/"},{"@type":"ListItem","position":2,"name":"WIKA\u2019s Magnetic Float Switch Offers Robust Design, Customizable Level Measurement for Mobile Working Machines"}]},{"@type":"WebSite","@id":"https:\/\/blog.wika.com\/us\/#website","url":"https:\/\/blog.wika.com\/us\/","name":"WIKA blog","description":"Our blog offers many interesting articles on pressure, temperature, level, flow measurement calibration technology and provides insights into the WIKA Group.","potentialAction":[{"@type":"SearchAction","target":{"@type":"EntryPoint","urlTemplate":"https:\/\/blog.wika.com\/us\/?s={search_term_string}"},"query-input":{"@type":"PropertyValueSpecification","valueRequired":true,"valueName":"search_term_string"}}],"inLanguage":"en-US"},{"@type":"Person","@id":"https:\/\/blog.wika.com\/us\/#\/schema\/person\/8d2cbbabfb4ec43b285229fb14d04066","name":"Jeff Placek","image":{"@type":"ImageObject","inLanguage":"en-US","@id":"https:\/\/blog.wika.com\/us\/files\/2023\/08\/jeffplacek2022_blog-120x120.jpg","url":"https:\/\/blog.wika.com\/us\/files\/2023\/08\/jeffplacek2022_blog-120x120.jpg","contentUrl":"https:\/\/blog.wika.com\/us\/files\/2023\/08\/jeffplacek2022_blog-120x120.jpg","caption":"Jeff Placek"},"url":"https:\/\/blog.wika.com\/us\/author\/jplacek\/"}]}},"_links":{"self":[{"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/posts\/10164","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/users\/188"}],"replies":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/comments?post=10164"}],"version-history":[{"count":19,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/posts\/10164\/revisions"}],"predecessor-version":[{"id":16162,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/posts\/10164\/revisions\/16162"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/media\/10168"}],"wp:attachment":[{"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/media?parent=10164"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/categories?post=10164"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blog.wika.com\/us\/wp-json\/wp\/v2\/tags?post=10164"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}