WIKA has put into operation a new plant in Saudi Arabia, strengthening its commitment in the region. In February, Alexander Wiegand opened the factory in Dammam together with the employees, customers and business …
Read moreWIKA India is socially committed: Nursery and women’s project
Stefan Schneider | WIKA insightWIKA India is considerably socially active. Both employees and the company benefit from this commitment. In January, the subsidiary inaugurated a nursery at the location in Pune, for example, to promote the …
Read morePressure monitoring at high temperature is a challenge
Jing Lyu | ApplicationsPressure monitoring at high temperature is a demanding measuring requirement. This requires a specially designed diaphragm seal. With model 990.45, WIKA offers such an instrument in its portfolio and was therefore …
Read moreCoatings of measuring instruments: Use and advantages
Sina Odenwald | Know-howProcess applications are becoming increasingly complex. Measuring instruments must therefore meet the highest requirements and function reliably – even with harsh outdoor conditions or aggressive media. Coatings are …
Read moreHydrostatic pressure test with a digital pressure gauge
Jing Lyu | ApplicationsA hydrostatic pressure test is used as a proof of strength and leak tightness of containers and pipelines that hold liquids and gases. The procedure and documentation of such a test can be increased in efficiency by …
Read moreIgnition protection type Ex i for pressure measuring instruments with battery operation
Jing Lyu | PressureWhich ignition protection type is suitable for battery-operated pressure measuring instruments, which are increasingly being used in combination with a radio unit? WIKA has clearly answered this question for its …
Read moreLevel limit switches: innovation meets all-rounder
Andreas Krüger | Know-howIn the world of industrial process measurement, precise level measurements are of vital importance. Level limit switches play a crucial role here to ensure that liquids in a tank are optimally controlled and monitored. …
Read morePressure transducer: Digitally connected with EtherCAT®
Fabian Mayer | PressurePressure transducers with EtherCAT ® as the communication protocol continue the digitalisation of the semiconductor industry at the transmitter level. In future, in every production plant, dozens of pressure measuring …
Read more