No other term is as misleading as "compensated temperature range". Let´s first begin with what is meant: The compensated temperature range is the temperature range in which the temperature error, and accordingly the temperature coefficients, are valid. Not, as one …
All posts by Michèle Beyer
What is volume weight?
Michèle Beyer | Know-howOr why it is important to find the right packaging for each product. Next to the actual weight which can be determined by weighing, there is also a so-called "volume weight". This is used for calculating transport costs. In addition to the actual weight, the …
Terminal boxes and angular connectors with M12x1: scope of delivery or accessories?
Michèle Beyer | GeneralWe are often asked whether for instruments with M12 x 1 connector the corresponding mating connector (also called cable socket or angular connector) is included in the scope of delivery of our pressure sensors. Our clear answer is: no. Unlike the DIN connectors forms A …
Angular connector form A leaking/ loss of IP ingress protection
Michèle Beyer | GeneralWhat are the rules that must be observed when assembling the angular connector EN 175301-803 A, to ensure that the IP rating is maintained, that is, connector and device remain really leak-tight? Unfortunately, a lot of things can go wrong when using the angular …
Aim and purpose of a vent hole in pressure sensors
Michèle Beyer | PressureIn so-called “gauge sensors” pressure is always measured relative to the currently prevailing ambient pressure. However, the ambient pressure is by no means constant. It is location- and height-dependent and changes with the weather. This means that for a …