In industrial applications, the corrosion of pressure sensors is a rather negligible phenomenon, since in the majority of applications, oils (in particular hydraulic oils) are used, and contact with the pressure medium is mainly limited to the pressure channel and the …
All posts by Enrico Bossart
Cleaning of submersible pressure transmitters or level probes
Enrico Bossart | Know-howIf the specific pressure sensor design of the submersible pressure transmitter or level probe is selected to measure the filling levels, this often means that the probe is used under environmental requirements which would cause failure of common level sensors. …
Selection criteria for the prevention of moisture-related failures of submersible pressure transmitters or level probes
Enrico Bossart | Know-howSubmersible pressure transmitters as well known as level probes are intended to be used in immersion applications, thus they are immersed completely into the medium and, therefore, must withstand the properties of the media at all times. Both in water and …
The design of a submersible pressure transmitter / level probe – Part 2
Enrico Bossart | Know-howIn my last article, the design of a submersible pressure transmitter / level probe - Part 1, I was explaining the design of a submersible pressure transmitter, beginning with the measuring cell and its electronics. Specifically with respect to the media resistance …
The design of a submersible pressure transmitter / level probe – Part 1
Enrico Bossart | LevelA submersible pressure transmitter or level probe is a hydrostatic pressure sensor, specifically developed for the purpose of level measurement. Submersible pressure transmitters, such as the WIKA model LH-20 , are level sensors with special characteristics and …