A frequently recurring question is about the definition of the so-called IP protection types or sometimes referred to as “IP rating”. The IP ingress protection types provide a system that describes how the housing of electrical equipment is protected against the …
All posts by Dominik Lorenz
Pressure equipment directive 97/23/EC PED – Pressure limits 0.5 bar and 200 bar for pressure sensors and pressure transmitters
Dominik Lorenz | PressureIn connection with the pressure equipment directive 97/23/EC (PED), a pressure limit of 200 bar is often mentioned. But what does this limit mean for manufacturers and/or companies that place pressure sensors, pressure transmitters and pressure equipment on the market? …
Active and passive temperature compensation of pressure sensors
Dominik Lorenz | GeneralHow does an active or passive temperature compensation of pressure transmitters actually work? High-quality pressure transmitters, especially those used in precision critical applications, are almost always provided with an individual temperature compensation. But …