TA Luft has been revised. For the prevention of fugitive emissions, the new version of the German directive now follows the international standard ISO 15848-1. Correspondingly, tests in accordance with TA Luft follow the same test parameters as those in the ISO …
All posts by Pratik R. Vishwakarma
Pressure measuring system against fugitive methane emissions
Pratik R. Vishwakarma | Pressure, ProductsWhether in the chemical industry, in petrochemical companies or in the processing of crude oil and natural gas: Numerous processes contain methane, which also damages the climate via fugitive emissions. Any escape of this greenhouse gas or any similar substance via the …
Play it safe with double block & bleed
Pratik R. Vishwakarma | Know-howWhat is the safest way to separate a process and the attached pressure measurement technology? The HSG 253 standard must be applied to this question, and it answers unequivocally: by means of an instrumentation valve with double block & bleed (DBB). This …
Avoid fugitive emissions through prevention
Pratik R. Vishwakarma | Know-howFugitive emissions attack the atmosphere and escape through numerous small leaks. Even instrumentation valves can become such points over the course of time. The most effective protection against fugitive emissions is prevention: In the case of instrumentation valves, …