Numerous industrial processes have an inherently high risk potential. Special pressure switches support the safety of people and the environment. Example: the vulcanisation of tyres for motor vehicles. To monitor this process, leading manufacturers use the model MW …
Applications
Safe filter monitoring with differential pressure gauges
Jing Lyu | ApplicationsFilter monitoring is a core task of differential pressure gauges - the differential pressure increases as soon as the filter becomes clogged. The measuring instruments thus signal when the filter needs to be cleaned or replaced. The efficiency of such a solution can be …
Natural gas: On-site calibration optimised at the metering skid
Jing Lyu | ApplicationsOn-site calibration of measuring instruments is often very time-consuming and expensive. This is especially true for applications with several measurands. One example of this is the metering skid, a system for the custody transfer measurement of the amount of natural …
Measurement technology in compressors
Roland Sachs | ApplicationsThe measurement technology used in compressors is tending to increase more and more. And for good reason. The balancing act between increased compressed air demands and reduced energy consumption also depends, to a large extent, on the intelligent use of measuring …
The ELMS1 overload protection saves lives
Markus Heidl | ApplicationsThere is always a lot going on in a port like Antwerp. Ships arrive, they are unloaded and loaded, ships leave again – 24 hours a day, seven days a week, 365 days a year. All as fast as possible, because time is money. In Antwerp in 2018, a container throughput of …