Metal bellows - pressure switches

What advantages do pressure switches with metal bellows offer and what is the basis for these? The advantages are based on the seamless design of their measuring system. This solution enables permanently stable repeatability and, at the same time, eliminates the risk of leakage.

Bellows measuring systems are based on a mature manufacturing technology. The production of metal bellows, for example from stainless steel or a copper alloy, takes place in several steps. Circular discs are first cut from a flat piece of metal, and these are then shaped into cup-shaped objects. They are softened through an annealing process in a furnace at more than 600 °C and then drawn into long, thin-walled and seamless tubes.

Constant elasticity

The tubes are corrugated by using forming tools at high pressure, and then are trimmed to the designed size. In the next stage, the spring-like metal cylinders are pressed together in accordance with the specified dimensions (length, outer and inner diameter). This creates the constant elasticity needed for the stable repeatability of the movement. In the final step, the bellows are degreased and passivated, i.e. given a protective coating against corrosion.

Bellows manufactured from stainless steel for pressure switches

Seal-free functionality

In a pressure switch, the metal bellows is brazed or welded to the process connection. Its other end is in contact with the transmission mechanism. This means that the instrument has a fully seamless measuring system without the need for any rubber sealing materials and the risk of leakage is eliminated. This feature makes pressure switches with metal bellows suitable for a wide range of applications. Process reliability is also guaranteed with liquid media.

Permanent accuracy

A metal bellows changes its length in line with the pressure. When a defined switch point is reached, it triggers the switching function via a transmission mechanism. If the pressure drops or rises again, the bellows returns to its original shape and the switch contact returns to its original position.

The expansion movement of a metal bellows has a high linearity. The switch differential, which is precisely adjusted via a specific calibrated spring system, remains correspondingly constant. This ensures the accuracy of pressure control and switching, even over a long period of time.

Note
Detailed information on pressure switches with metal bellows, e.g. models PSM-520, PSM-550 and PSM-700, can be found on the WIKA website. You would like to buy pressure switches with metal bellows? In our WIKA online-shop you will find some of our standard designs. If you have any questions, your contact will gladly help you.



Post a comment