Our customers like to talk about a maximum operating pressure or working pressure. Unfortunately, these two terms are not defined for pressure sensors, which means that a definitive answer cannot be given. All we can assume is that, by maximum operating pressure or …
Burst pressure
Autofrettage in pressure sensors ensures zero-point stability
Eugen Gaßmann | PressureIn the manufacturing operation of pressure sensors, autofrettage denotes the process of active "overload" by subjecting the pressure sensor selectively once or several times to a pressure above the nominal pressure range . This process is applied, in order to achieve …
How does a pressure sensor behave in the overload area, that means outside the measuring range?
Anna Gries | PressureI have often been asked about the behaviour of a pressure sensor outside the specified measuring range, that means in the overload area and what will happen if the overload limit of a pressure sensor is exceeded. This fact is described as follows in the book …