Dual piston deadweight testers can greatly enhance a lab’s ability to calibrate wide pressure ranges with the highest accuracy. With transducers and devices under test (DUTs) that have a wide measuring range, calibration can be a lengthy process, as you must change …
Calibration
Pressure measurement in precision: 50 years of Mensor
Stefan Schneider | WIKA insightWithout doubt, Mensor plays a prominent role in the world of electronic pressure measurement. This WIKA Group company is based in San Marcos (Texas) and it was founded precisely 50 years ago. Since then, time and again it has set new benchmarks in the precision …
Thermometer calibration – an overview
Danica Schwarzkopf | Know-howNot all calibrations are the same. This is illustrated by the example of “Thermometer calibration” - which test method is used depends on various factors such as process conditions, quality standards and safety requirements. Depending on the method, the calibration …
Record! 18-inch flow nozzle manufactured in just 20 weeks
Stefan Schneider | WIKA insightAt the end of 2018, for a flow measurement application in India, the WIKA Group manufactured a PTC-6 nozzle with a diameter of 18 inches for the first time - and in a record time of just 20 weeks. The overall length of this nozzle, including upstream/downstream piping, …
Calibration / contamination control with a block and bleed valve
Larry Mock | Know-howA block and bleed valve can be used to prevent flow of contamination from a device under test (DUT) to a pressure controlling calibrator. This procedure includes “exercising” and purging the DUT and the actual calibration. Your procedure may be different but the …