Process applications are becoming increasingly complex. Measuring instruments must therefore meet the highest requirements and function reliably – even with harsh outdoor conditions or aggressive media. Coatings are usually indispensable for use, for example, in the …
Measuring instruments
Ignition protection type Ex i for pressure measuring instruments with battery operation
Jing Lyu | Pressure, ProductsWhich ignition protection type is suitable for battery-operated pressure measuring instruments, which are increasingly being used in combination with a radio unit? WIKA has clearly answered this question for its portfolio: “Ex i”, i.e. intrinsic safety. This …
Calculate the flow rate correctly
Michael Lutz | Applications, FlowMillions of cubic metres of liquids or gases flow through the pipes of industrial processes every day. In order to be able to transport, control and monitor these correctly, the flow rate must be calculated beforehand. The flow rate, also called volume flow, is a …
Unscrupulous: Faking the website of WIKA China
Stefan Schneider | WIKA insightTrademark pirates won't even stop at faking a website in order to distribute counterfeit products via the internet. WIKA has now also been affected by such criminality – under the domain www.wika-wika.cn, a company from Shanghai faked the homepage of WIKA China. …
Monitoring the level in liquid gas tanks with a Cryo Gauge
Hardy Orzikowski | Level, ProductsIn the past, monitoring the filling level in liquid gas tanks using differential pressure has always been a challenge. This is because the manufacturers of tank equipment had to construct their own measuring systems in order to record the liquid level and the operating …