Pressure monitoring in the pharmaceutical industry is a demanding task with a wide variety of requirements. However, a corresponding diversification in instrumentation does not have to be an inevitable consequence. This is demonstrated by the use of a universal process …
Pharmaceuticals & Biotechnology
Diaphragm seal system with diaphragm monitoring – also digital
Tobias Hench | Pressure, ProductsA diaphragm seal system with diaphragm monitoring from WIKA meets the highest safety requirements in sanitary applications. The model DMSU21SA with process transmitter and HART ® protocol (cover picture) can also be integrated into digitalised environments. Why …
Unique: Diaphragm pressure gauge for pharmaceutical industry
Jing Lyu | ApplicationsRequirement and solution − The following example from China shows WIKA's competence in the pharmaceutical sector: One of the biggest vaccine manufacturers in China urgently needed a safe and autoclavable pressure gauge in hygienic design for the production of an …
Safe pressure monitoring for vaccine production
Silvia Weber | PressureIt can take up to three years to turn bacteria, viruses or cell cultures into a vaccine. Since vaccines are injected directly into the body, safety and purity have the highest priority in production. The demands on the plant equipment are correspondingly high, for …
Hygienic pressure gauge: IP68 with cleaning from the outside
Silvia Weber | ProductsVent valve instead of vent hole: With this option, the model PG43SA-S hygienic diaphragm pressure gauge is even suitable for pharmaceutical cleaning from the outside with particularly aggressive agents. The closed valve seals the inside of the pressure gauge in …