Switch contacts in pressure gauges and mechanical thermometers significantly extend the functionality of the measuring instruments. They enable limit value monitoring in addition to on-site indication. Such instruments with switch contacts are therefore an important …
Pressure gauge
Stainless steel pressure gauges: Facelift brings digital features
Christopher Ott | PressureNew look plus enhanced functionality: WIKA has given its stainless steel pressure gauges and mechanical thermometers a comprehensive facelift. Customers benefit from this in several ways and at no extra cost. For example, they can use a QR code on the dial to open a …
Pressure monitoring at high temperature is a challenge
Jing Lyu | ApplicationsPressure monitoring at high temperature is a demanding measuring requirement. This requires a specially designed diaphragm seal. With model 990.45, WIKA offers such an instrument in its portfolio and was therefore awarded the contract by the operator of an oil …
Coatings of measuring instruments: Use and advantages
Sina Odenwald | Know-howProcess applications are becoming increasingly complex. Measuring instruments must therefore meet the highest requirements and function reliably – even with harsh outdoor conditions or aggressive media. Coatings are usually indispensable for use, for example, in the …
Injectables: Pressure measurement without risk of contamination
Jing Lyu | ApplicationsInjectables are among the most sensitive products in the pharmaceutical industry. Sterility is essential during production. This is because the active ingredient enters the patient's body directly, bypassing the patient's natural defences. It is therefore important to …