Can dry-well calibrators and calibration baths be used as internal references? Temperature dry-well calibrators and baths are a practical solution for temperature calibrations. This is true both in the field and in laboratories, as they provide a free-standing, stable …
Sensor
Calibration bath or dry-well calibrator – which is the right choice?
Danica Schwarzkopf | Know-howTemperature sensors – like all other sensors – must be calibrated at regular intervals. This ensures that they deliver accurate and consistent measured values. Temperature calibration (e.g. using a calibration bath or dry-well calibrator) is generally carried out …
Comparative calibration vs. fixed point calibration
Fabian Ehing | Know-howIn temperature calibration technology, there are two methods of calibration - the comparative calibration and the fixed point calibration. The method of calibration to be used will be defined through the demands on the accuracy and the type of test instrument. The …
Quick-mounting clip: Cost reduction in the fitting of strap-on sensors
Gerhard Renz | TemperatureA quick-mounting clip enables fast and cost-effective fitting of strap-on temperature sensors in heating systems and heat pumps. These can be quickly and easily clipped onto the heating pipe without the need for any tools. Generally, in practice, strap-on …