What advantages do pressure switches with metal bellows offer and what is the basis for these? The advantages are based on the seamless design of their measuring system. This solution enables permanently stable repeatability and, at the same time, eliminates the risk …
Strain
The strain sensor in practical application
Markus Heidl | ForceDrill two holes and cut the threads, prepare the surface, place the strain sensor and tighten both screws to the specified torque, then set the zero point and now the strain measurement can start. If only it were that easy! Of course, the procedure described for …