One speaks of an interface measurement when two different liquids in a tank or container are measured independently of one another. Such an interface measurement is always useful when the liquids are not miscible with each other, as is the case with oil and water, for …
Tank
Level monitoring in milk tanks using a process transmitter
Jing Lyu | ApplicationsLevel monitoring using a process transmitter with a flush diaphragm is an option for applications in the food industry. It is highly accurate and at the same time suitable for aseptic tanks. A manufacturer of dairy products (milk, cream and yoghurt), for example, uses …
Measuring tank levels in boiler systems with DELTA-trans
Jing Lyu | ApplicationsThe fill level in the feed tank of industrial boiler systems is a crucial process parameter to ensure a smooth energy supply of steam or hot water. A manufacturer of such systems uses the model DPGT40 differential pressure gauge from WIKA's DELTA-line product family to …
Monitoring the level in liquid gas tanks with a Cryo Gauge
Hardy Orzikowski | Level, ProductsIn the past, monitoring the filling level in liquid gas tanks using differential pressure has always been a challenge. This is because the manufacturers of tank equipment had to construct their own measuring systems in order to record the liquid level and the operating …
Electronic differential pressure measurement for level monitoring
Bernd Reichert | Know-howDifferential pressure measurement is widely used as a method for monitoring the level of closed vessels. In many cases, operators use individual instruments with an output signal or on-site display. In contrast, a more precise and fault-immune solution is the measuring …