Pressure monitoring at high temperature is a demanding measuring requirement. This requires a specially designed diaphragm seal. With model 990.45, WIKA offers such an instrument in its portfolio and was therefore awarded the contract by the operator of an oil …
Temperature
Coatings of measuring instruments: Use and advantages
Sina Odenwald | Know-howProcess applications are becoming increasingly complex. Measuring instruments must therefore meet the highest requirements and function reliably – even with harsh outdoor conditions or aggressive media. Coatings are usually indispensable for use, for example, in the …
NAMUR working group for pressure and temperature at WIKA
Stefan Schneider | WIKA insightThe NAMUR working group 3.11 (pressure and temperature) was a guest at WIKA. NAMUR are an international user association of automation technology and digitalisation in the process industry. The NAMUR working group started its two-day visit in May with a highlight: …
Measuring the response times of electrical thermometers
Joachim Brückner | Know-howThere are many reasons for using electrical thermometers with short response times: optimisation of the efficiency, more efficient utilisation of the working range of a process, avoidance of thermal overload of the process medium. But how are response times measured, …
Not the same: temperature range and temperature limit
Michèle Beyer | Know-howTemperature range and temperature limit for pressure sensors – is there a difference? My intuitive answer would be: Yes! The first term describes a section and the second its border. On second glance, however, I have to conclude that both words ultimately express the …