In temperature calibration, high demands are placed on reference thermometers in terms of accuracy and reproducibility and thus long-term stability. Therefore, RTDs (“resistance temperature detectors”) – here specifically platinum resistance thermometers – and …
Temperature
Temperature calibration with reference probes, dry-well calibrators and baths
Katja Strecke | Know-howCan dry-well calibrators and calibration baths be used as internal references? Temperature dry-well calibrators and baths are a practical solution for temperature calibrations. This is true both in the field and in laboratories, as they provide a free-standing, stable …
Pressure and temperature measurement at extremely low ambient temperatures
Christopher Ott | Know-howStandard pressure gauges and thermometers generally cope with ambient temperatures down to -40 °C. But what must be the features of a mechanical measuring instrument that works perfectly well in polar climates with even lower temperatures? This can be explained using …
Pt100 in class B or F 0.3 – what does IEC 60751 say?
Roland Sachs | Know-howPerhaps you've already noticed that in some instances a Pt100 is specified with an accuracy class B or A. At other times, it has the class F 0.3 or F 0.15. This blog post looks at the specifications for Pt100 in the international IEC 60751 standard and explains the …
Filter monitoring: A crucial component for energy-efficient operation
Jürgen Arndt | Know-howIf the careful use of “energy” as a resource used to be for cost reasons, today there is also increased environmental awareness. All of this also becomes mandatory thanks to legal requirements and the state of the technology. In this article you can read about how …