Pressure measurement could be so simple: Installing a pressure gauge, pressure transmitter or IIoT measuring instrument with radio unit – done. But in many cases, a measuring location requires more components than just the measuring instrument, especially in the …
Valves & Controllers
Advantages of in-situ calibration using the example of pressure switches
Jing Lyu | ApplicationsIn-situ calibration of measuring instruments is carried out in numerous industrial processes. The advantages are obvious: The instruments remain installed, so the process does not have to be opened. In this way, plant operators reduce the time and costs involved in …
Differential pressure switches ensure safe filter operation
Jing Lyu | ApplicationsDifferential pressure switches take on central tasks within monitoring and control. A manufacturer of filter systems for the process industry uses the WIKA model DE switches with an attached valve manifold for these functions. The decision in favour of this solution …
TA Luft now follows ISO 15848-1 for fugitive emissions
Pratik R. Vishwakarma | Know-howTA Luft has been revised. For the prevention of fugitive emissions, the new version of the German directive now follows the international standard ISO 15848-1. Correspondingly, tests in accordance with TA Luft follow the same test parameters as those in the ISO …
Flushing rings in diaphragm seal systems have several advantages
Tobias Hench | Know-howThe extension of a flanged diaphragm seal system using a flushing ring brings significant advantages. Among other things, it enables easy cleaning and, in addition, on-site calibration of the measuring location. Diaphragm seal systems are used in processes with …