Sulfur hexafluoride (SF 6 ) has been used for decades as an insulator in power plants and electrical transmission and distribution. This gas has excellent dielectric properties, almost three times better than air and nitrogen, and it works well as arc quencher in …
Products
Pressure Measurement: Understanding PSI, PSIA and PSIG
Hardy Orzikowski | PressurePressure measurement is all about PSI. That’s because pounds per square inch (PSI) is the most common unit for measuring pressure in the U.S. It’s important to understand what PSI means and how it is used, as pressure measurement is an important part of life in the …
Eugene Bourdon and the History of the Bourdon Gauge
Hardy Orzikowski | PressureThe Industrial Revolution was underpinned by the fortunes of a few dozen financiers, the blood, sweat and tears of millions of factory workers, and a handful of key technical innovations. One of the key inventions of the mid-19 th century was the Bourdon gauge. …
Common Causes of Diaphragm Seal Failure
Chi-Che Ma | PressureA diaphragm seal is an efficient, affordable solution for those instances in which pressure instrumentation cannot be in direct contact with the process. A flexible diaphragm seal protects pressure transmitters, transducers, gauges, and switches from contact with …
WIKA’s ScrutonWell®: Thermowell with Helical Strakes to Reduce Vibration
Gabriel Gonzales | TemperatureA thermowell is a protective housing for a thermometer used to provide temperature readings for an industrial process. Given that process media in many industries are corrosive, abrasive or under high pressure, a thermometer is placed inside a thermowell so the …