Predictive maintenance, a system where inputs from electronic sensors and transmitters are used to help forecast when equipment needs to be serviced or replaced, is the key to minimizing downtime, maximizing efficiency, and saving money. Whether production lines …
Pressure
XSEL® Industrial Process Gauges, Durability for Peace of Mind
Hardy OrzikowskiProcess industries rely on pressure instruments for safe and efficient operations. WIKA USA’s XSEL ® process gauges offer exceptional performance, reliability, and safety, even in the harshest conditions. The process industry converts raw materials – crude …
The S-20 Industrial Pressure Sensor: Excellence Under Extreme Conditions
Robert LukatHigh temperatures, aggressive media, vibration, submersion — the S-20 industrial pressure sensor can be customized to operate in these and other tough conditions without affecting accuracy. Its versatility and durability are what make this transmitter the pressure …
NEMA Rating and IP Rating: Explaining the Difference Between the Two Designations
Robert LukatFor optimal safety and performance, electrical equipment needs to be sheltered from the environment. Both a NEMA rating and an IP rating indicate the level of protection a device has against outside conditions, ranging from falling dust to ocean waves. These two …
Diaphragm Seals: Ultimate Protection for Safer, More Sanitary Pressure Measurement
Chi-Che MaCertain process media can damage pressure gauges, which, in turn, can contaminate clean process media. By using a diaphragm seal as a protective barrier, plant operators save time and money by avoiding instrument damage, batch losses, and expensive downtime. If …