Pumps are vital to many different industries – from air conditioning to food and beverage. Pressure gauges can be essential to keeping pumps up and running. Proper maintenance plays a vital role in keeping your pumps pumping. Here's a quick look at …
Pressure
SDWA-Compliant Pressure Gauges are Now Required by Law
Hardy OrzikowskiOnly WIKA offers a NSF International certified pressure gauge to meet the requirements of the Safe Drinking Water Act (SDWA). Although stainless steel was an option, it is expensive, so WIKA engineers crafted a gauge with wetted parts made from lead-free brass that …
The Best Gauge for High Vibration Conditions
Hardy OrzikowskiBased WIKA Instrument’s analysis of audit data from more than 250 plants, vibration is one of the most common reasons for gauge failure. What are signs of gauge failure? Visible = detached pointer and dust on the inside of the gauge window. Hidden risks = wear …
WIKA Instrumentation Can Help You Comply with Stricter EPA Rules
Robert LukatThe U.S. Environmental Protection Agency (EPA) has proposed new rules that will boost emissions-control requirements for the 150 active refineries in the United States. Proper instrumentation can help these refineries reduce fugitive emissions and the steep price tag …
Learning About the Effect of Temperature on Pressure Sensors
Robert LukatTemperature has a major impact on the function and operating lifetime of most electronic devices. This is especially true for electronic pressure sensors. That's why pressure sensor specifications typically include minimum and maximum values for operating, storage, …