SF6 Gas Solutions

WIKA’s Innovative Dehydrator Removes Moisture from SF6 Gas Without Stopping Operations

Josh Sizemore
Wide shot of a power plant under a blue sky.

Pure SF 6 is an excellent insulator in electric switchgears, but humidity in the gas decreases its insulating ability and can also result in very harmful decomposition products for humans, machinery, and the environment. Created in partnership with a European utility …

Read more

GPU-2000: SF6 Tank for Handling, Replacement, and Cleaning

Josh Sizemore
Transformer substation

The level of humidity in SF 6 -insulated switchgear must be kept below its water saturation point. If the gas is too humid, it loses some of its insulating properties; corrosion and dangerous leaks can also occur. A complete SF 6  handling instrument monitors the …

Read more

How Humidity Affects a SF6 Gas-Insulated Switchgear

Josh Sizemore
Water droplets

Sulfur hexafluoride is the gas most commonly used as insulator in power transmission and distribution switchgear. Water, however, can negatively affect the dielectric capabilities of SF 6  gas. To prevent operational and safety issues, it is important to measure and …

Read more

How Changes in Gas Temperature Affect Gas Density Measurements

Josh Sizemore

Circuit breakers, disconnectors, and switchgear in power transmission and distribution (T&D) operations have been using sulfur hexafluoride (SF 6 ) as insulation for decades. To maintain the excellent thermal conductivity and dielectric strength of SF 6 , …

Read more

How Ambient Conditions Can Compromise Density Measurements in T&D SF6-Insulated Equipment

Josh Sizemore

For decades, the power transmission and distribution (T&D) industry has been using sulfur hexafluoride (SF 6 ) as the insulator in circuit breakers, disconnectors, and switchgear. The heat transfer and dielectric characteristics of this gas are better than those of …

Read more
Welcome to the WIKA blog

In our WIKA US blog you can expect many interesting articles on pressure, temperature, level and flow measurement, and also on the subject of calibration technology. Furthermore, there are various insights into the world of the WIKA group of companies – seen from different angles.

Most-read articles
  • Common SF6 Gas Hazards and How to Avoid Them
  • Case Study: Preventing Moisture in SF6 Switchgear with WIKA’s SF6 Gas Dehydrator
  • WEgrid Services: SF6 Gas Consulting, Training, Maintenance/Repair, Analysis, and More

© 2026 WIKA Alexander Wiegand SE & Co. KG

  • Privacy policy
  • Legal notice