A diaphragm seal makes measuring pressure safer and more reliable – even in extreme working conditions – and is ideal for protecting pressure instrumentation and process transmitters. Discover the basic principle behind diaphragm seals and when to use them.
It often isn’t a problem when the process medium comes into direct contact with pressure gauges, pressure transmitters, or other pressure instruments. However, harsh media and environments can damage a sensor’s internal pressurized parts. In these instances, a diaphragm seal can make all the difference between reliable and unreliable readings.
The purpose of a diaphragm seal is to isolate a pressure measuring instrument from the process media. It is often used for the most difficult measuring tasks, such as when the environment is extremely hot or cold, or when a process connection is difficult to attach to the measuring instrument. Diaphragm seals are also used when the media being measured is corrosive, viscous, sticky, or easily solidified, or when the process isn’t chemically compatible with the instrument material.

A diaphragm seal is a thin, flexible wall that separates the media being measured from the pressure measuring instrument.
What Is a Diaphragm Seal?
Typically connected to a pressure gauge, process transmitter, or pressure switch, a diaphragm seal is a thin, flexible wall that separates the media being measured from the pressure measuring instrument. The space between the diaphragm and the measuring instrument is filled with a system fluid (transmitting fluid), which hydraulically transmits pressure from the flexible diaphragm. The contact surface between the media and the diaphragm is relatively large, which ensures more accurate pressure measurements – especially for very low pressures (< 600 mbar).
By preventing media from contacting the pressure measuring element directly, a diaphragm seal also:
- Eliminates clogging and crystallization in the measuring instrument
- Minimizes corrosion
- Protects the sensing element from extreme temperatures
When using a diaphragm seal, the measuring instrument can be used at temperatures from −130 to +750°F (−90 to +399°C), as well as with aggressive, corrosive, heterogeneous, abrasive, highly viscous, or toxic media. There are diaphragm seal designs, materials, and filling fluids available for many demanding industrial applications, such as bioethanol production, fertilizer production, and wastewater filtration.
Why Use a Diaphragm Seal
A properly engineered diaphragm seal protects while only minimally affecting accuracy. As such, diaphragm seals extend the operating life of pressure measurement instruments – saving users significant time and money in the long run.
Diaphragm seals also enable remote mounting from the pressure port via a capillary that is custom suited for your unique application. And thanks to the wide range of available process connections (flanged, threaded, etc.), they can meet many industry standards.
WIKA’s Expertise and Excellence in Diaphragm Seals
WIKA manufactures a complete line of diaphragm seals for a variety of industries and processes. Some features include:
- Wetted materials in several grades of stainless steel and alloys
- Many accessories, including flushing rings and ports, saddle and block flanges, capillaries, and cooling elements
Many customers have come to appreciate WIKA’s diaphragm seal service, which has gained quite a reputation in the Gulf Coast for returning diaphragm seal repairs in less than 24 hours. The seal repair service is also a great way to save money by repairing or replacing only the damaged pieces rather than buying a completely new transmitter assembly. We make repairs on any make or model of diaphragm seal on any transmitter, regardless of the original manufacturer.
For more information about WIKA’s comprehensive Diaphragm Seal Division, contact our pressure experts.
WIKA’s video explained that Diaphragm Seal including capillary tube may allow users to extend measuring instrument installation location. During installation, the capillary tube may be bent along with the route toward measuring instrument location. Is there any limitation of radius of bending the tube? Is there a possibility of capilary tube damage during installation?
Hello,
The capillary line is a stainless steel flexible tubing covered by a thin, flexible armor. The capillary is flexible, but we recommend a bend radius of 6 inches (152 mm) so it doesn’t restrict the flow of the internal fill to keep your accuracy and response time. The armor is there just to protect the capillary and there is a potential of damaging the armor since it is a thin-walled stainless, it can be cut. However, even if the armor is damaged, the capillary tube inside should still be ok. The capillary tube has enough of a wall to protect it from being accidentally stepped on, but it still has the potential of being kinked or bent beyond repair.
Best Regards,
Chi-Che Ma
You said diaphragm seal, the measuring instrument can be used at temperatures from −130 to +750°F (−90 to +399°C), as well as with aggressive, corrosive, heterogeneous, abrasive, highly viscous, or toxic media. What is its reference?
Hi Ali, thank you for your question. Diaphragm seal system temperature ratings are based on the various system fill fluids we offer. We offer a variety of fill fluid suitable for different applications, such as low temperatures, and high temperatures, and we even offer food safe and inert for oxygen-free applications. For different types of media, different process-wetted materials, such as Hastelloy C-276, Monel 400, and tantalum, just to name a few that will work best with your media and application. We also offer different types of diaphragm seals such as flush diaphragm to prevent clogging and recess diaphragm for small process connections that require a more sensitive sensor for lower pressure ranges. Let me know if you have any other questions.
Very informative! One question I have is about the maintenance of diaphragm seals. What is the typical maintenance schedule, and how can we ensure their longevity in high-pressure systems?
Thank you so much for visiting our blog and posting your question!
Diaphragm Seal System maintenance varies depending on your media. For example, if the media is viscous or prone to clogging, regular cleaning of the system is recommended. We advise against mechanical cleaning methods such as scraping or wiping the diaphragm clean. Instead, we recommend using the lowest pressure possible when cleaning the diaphragm.
For high-pressure applications, the hydraulic back pressure from the system fill is sufficient to maintain the integrity of the diaphragm throughout its service life. Therefore, regularly check for any fill fluid leaks outside of the system. Opting for an all-welded system, such as our M933.D1, adds additional security against leaks.
For corrosion concerns, it is crucial to start with material selection to ensure that process-wetted parts are made of the appropriate materials for your media. Lastly, regularly scheduled calibrations can help ensure that your diaphragm seal is in good working condition. WIKA recommends a yearly calibration of the system, but more frequent calibrations are always better.