In the U.S., pressure measurement is all about pounds per square inch. As such, it’s important to understand what psi means and how it is used.
What is PSI, and where is this unit of measurement used?
Pounds per square inch is the unit of pressure measurement used in the vast majority of U.S. household, commercial, and industrial equipment. Even in countries that have adopted the metric system, such as Canada and the UK, psi is used alongside bar and millibar (mbar) in specific contexts; these contexts include tire pressure, in oil and gas applications, and scuba tanks. For measuring low pressure, the U.S. tends to use inches of water (inH2O).
Most other countries measure pressure in bar and millibar. 1 bar is the average atmospheric pressure at sea level. In scientific contexts like physics labs, pressure is typically measured in much smaller units called pascals. For reference, 14.5 psi equals 1 bar, and 1 psi equals 6,894.76 Pascals (Pa). Confusingly enough, the standard atmospheric pressure at sea level — 1 atmosphere (atm) — is 14.7 psi.
Two frequently used variations of psi are psia (pounds per square inch absolute) and psig (pounds per square inch gauge).
Comparing PSIG and PSIA
PSIA is a term that describes the absolute pressure in psi, including the pressure of the atmosphere. Absolute pressure is also sometimes referred to as total pressure, as it is the sum of the atmospheric pressure and the exerted pressure.
PSIG is the term for pressure specified by a gauge or other pressure measuring instrument. Gauge pressure, also called overpressure, is the pressure of a system above atmospheric pressure. Therefore, gauge pressure is always lower than absolute pressure.
PSIG to PSIA Conversion Table
| Absolute pressure (psia) | Gauge pressure (bar) | Gauge pressure (kPa) | |
|---|---|---|---|
| −14.7 Perfect vacuum (assuming 14.7 psi atmospheric pressure) | 0.0 | −1.0135 | −101.353 |
| 0 | 14.7 | 0.0000 | 0.000 |
| 1 | 15.7 | 0.0689 | 6.895 |
| 10 | 24.7 | 0.6895 | 68.948 |
| 25 | 39.7 | 1.7237 | 172.369 |
| 50 | 64.7 | 3.4474 | 344.738 |
| 100 | 114.7 | 6.8948 | 689.476 |
How to read the table: Read from the psig column to the psia column to convert gauge pressure to absolute pressure. Read in reverse to convert absolute pressure to gauge pressure. The bar and kPa columns express the gauge pressure in different units. Values are rounded.
Conversion formulas:
Absolute pressure (psia) = gauge pressure (psig) + local atmospheric pressure (psi)
Gauge pressure (psig) = absolute pressure (psia) − local atmospheric pressure (psi)
1 psi ≈ 0.06894757 bar ≈ 6.894757 kPa
Altitude and weather: Local atmospheric pressure changes with elevation and weather. Use the actual local atmospheric pressure when accuracy matters, rather than assuming 14.7 psi. A perfect vacuum is always 0 psia; its equivalent gauge pressure depends on local atmospheric pressure.
For more information about units of pressure measurement, pressure gauges in the process industry, and customized pressure instruments, contact WIKA USA.

Why does on Pressure Gauge scale indicate PSI instead of PSI-g? Regards!!!
Hello,
Per the US standard for pressure gauges ASME B40.100 all standard pressure units such as psi, bar, kPa, kg/cm2 etc. indicate gauge pressure or relative pressure until otherwise specified. It is not required to use psi or bar unless required by the customer. For all other scales, absolute or differential pressures are indicated by adding the words “absolute” or “differential”. It is also acceptable to use abbreviations such as abs or diff or to use units such as psia (psi absolute) or psid (psi differential). However, the suffix g is not required when measuring relative or gauge pressure. Almost all manufacturers use psi or bar, kPa etc.
I am having a pressure tank built, for some reason I do not yet understand, upon testing the tank seal at 13 psig one of the securing bolts gave way the threads stripped out and the nut came flying off at a high rate of speed. The tank and securing bolts and nuts are all steel components. Can you explain why this situation occurred at such a low pressure?
Thank you
Sincerely
Bruce Eversole
Hi Bruce. Thank you for your comment. A product manager should be reaching out to you shortly if they have not already.
Hi,
If I had two hoses one being longer than the other, and I ran water from both at the same psi. Would there be less pressure/output from the longer hose?
thanks,
-Will
Hey Will,
The length of the hose should not matter if the output of the hoses are at the same height, and the diameters of the hoses are the same.